Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech: Python + PyGTK + Glade = UI Design
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 21 Aug 2015 11:40 PM Date Created
  • Views 4431 views
  • Likes 7 likes
  • Comments 24 comments
  • interface_design
  • meditech_project
  • python
  • user_interface
  • development_speedup
  • raspberry-pi
  • graphic_libraries
  • glade
  • pygtk
  • graphic_design
  • sci_fi_your_pi
Related
Recommended

Meditech: Python + PyGTK + Glade = UI Design

balearicdynamics
balearicdynamics
21 Aug 2015

Introduction

Definitely the Python language with some content improvements has been adopted to manage the UI, replacing the initial idea to use Qt for two reasons: development optimization and architecture simplification. Unfortunately as many times occur, making things simple it is not so simple.

 

Exploiting the features of the Linux graphic interface

Together with Python there is a very useful  library interfacing the language with the standard features natively available in the Raspbian desktop: PyGTKimage

This library lets create almost any graphical user interface with the Python language using  GTK+. This means that it is possible to create multiplatform visual applications based on the graphic features and performances of the Gnome Desktop.

The resulting program can work easily with good performances without further intermediate graphic components.

Another advantage is that the entire set of UI applications developed in PyGTK inherit the GTK  desktop theme adapting to any supported environment.

 

As occur with all the Python libraries the integration of PyGTK in the Python programs is almost simple:

 

#!/usr/bin/env python

import sys
try:
    import pygtk
    pygtk.require("2.0")
except:
    pass
try:
    import gtk
    import gtk.glade
except:
    print("GTK Not Availible")
    sys.exit(1)

class HellowWorldGTK:
    """This is an Hello World GTK application"""

    def __init__(self):

        #Set the Glade file
        self.gladefile = "HelloWin.glade"
        self.wTree = gtk.glade.XML(self.gladefile)


if __name__ == "__main__":
    hwg = HellowWorldGTK()
    gtk.main()

 

A simple GTK Window with Python

The following scriptlet  shows the creation of a simple windows using PyGTK

#!/usr/bin/env python

# example base.py

import pygtk
pygtk.require('2.0')
import gtk

class Base:
    def __init__(self):
        self.window = gtk.Window(gtk.WINDOW_TOPLEVEL)
        self.window.show()

    def main(self):
        gtk.main()

print __name__
if __name__ == "__main__":
    base = Base()
    base.main()

 

This source is very simple generating a small window on the screen as shown below:

image

Something more complex

Using the PyGTK API - we can try this more complex example

#!/usr/bin/env python

# example table.py

import pygtk
pygtk.require('2.0')
import gtk

class Table:
    # Our callback.
    # The data passed to this method is printed to stdout
    def callback(self, widget, data=None):
        print "Hello again - %s was pressed" % data

    # This callback quits the program
    def delete_event(self, widget, event, data=None):
        gtk.main_quit()
        return False

    def __init__(self):
        # Create a new window
        self.window = gtk.Window(gtk.WINDOW_TOPLEVEL)

        # Set the window title
        self.window.set_title("Table")

        # Set a handler for delete_event that immediately
        # exits GTK.
        self.window.connect("delete_event", self.delete_event)

        # Sets the border width of the window.
        self.window.set_border_width(20)

        # Create a 2x2 table
        table = gtk.Table(2, 2, True)

        # Put the table in the main window
        self.window.add(table)

        # Create first button
        button = gtk.Button("button 1")

        # When the button is clicked, we call the "callback" method
        # with a pointer to "button 1" as its argument
        button.connect("clicked", self.callback, "button 1")


        # Insert button 1 into the upper left quadrant of the table
        table.attach(button, 0, 1, 0, 1)

        button.show()

        # Create second button

        button = gtk.Button("button 2")

        # When the button is clicked, we call the "callback" method
        # with a pointer to "button 2" as its argument
        button.connect("clicked", self.callback, "button 2")
        # Insert button 2 into the upper right quadrant of the table
        table.attach(button, 1, 2, 0, 1)

        button.show()

        # Create "Quit" button
        button = gtk.Button("Quit")

        # When the button is clicked, we call the main_quit function
        # and the program exits
        button.connect("clicked", lambda w: gtk.main_quit())

        # Insert the quit button into the both lower quadrants of the table
        table.attach(button, 0, 2, 1, 2)

        button.show()

        table.show()
        self.window.show()

def main():
    gtk.main()
    return 0      

if __name__ == "__main__":
    Table()
    main()

This code will generate the window shown in the image below

image

Until we press the buttons 1 and 2 we  see on the terminal the button message then pressing the  OK button the program ends.

Hello again - button 1 was pressed
Hello again - button 2 was pressed

 

The PyGTK library includes also the API to set callback functios, associate methods to the buttons and so on. A complete manager of the visual interaction. Unfortunately also for a  simple application (three buttons with their callback  inside a standard window) we should write a lot of code. As a matter of fact every graphic option, button, icon and  detail should be written in Python calling the proper PyGTK API.

 

Separating the design from the code

The solution to make the things easier is to operate a separation between the User Interface design and the code. To reach this goal we should adopt a technique very similar to the Android applications, keeping apart the  objects design in XML format  from the PyGTK Python code.

The Meditech Python controller when start shows the main Meditech logo on the screen while managing the inter-process communication. To reach this result  the background image has been created:

image

Then a special window has been defined in a separate XML file: the MeditechInterface2.glade as shown below

<?xml version="1.0" encoding="UTF-8"?>
<interface>
  <!-- interface-requires gtk+ 3.0 -->
  <object class="GtkWindow" id="MeditechBackground">
    <property name="visible">True</property>
    <property name="sensitive">False</property>
    <property name="can_focus">False</property>
    <property name="halign">center</property>
    <property name="valign">center</property>
    <property name="title" translatable="yes">Meditech 1.0Beta</property>
    <property name="resizable">False</property>
    <property name="modal">True</property>
    <property name="window_position">center-on-parent</property>
    <property name="default_width">1024</property>
    <property name="default_height">1080</property>
    <property name="hide_titlebar_when_maximized">True</property>
    <property name="type_hint">desktop</property>
    <property name="skip_taskbar_hint">True</property>
    <property name="skip_pager_hint">True</property>
    <property name="accept_focus">False</property>
    <property name="focus_on_map">False</property>
    <property name="decorated">False</property>
    <property name="deletable">False</property>
    <property name="gravity">center</property>
    <property name="has_resize_grip">False</property>
    <property name="mnemonics_visible">False</property>
    <property name="focus_visible">False</property>
    <child>
      <object class="GtkImage" id="background">
        <property name="width_request">1024</property>
        <property name="height_request">768</property>
        <property name="visible">True</property>
        <property name="sensitive">False</property>
        <property name="can_focus">False</property>
        <property name="xalign">0</property>
        <property name="yalign">0</property>
        <property name="pixbuf">images/Meditech-1024.jpg</property>
      </object>
    </child>
  </object>
</interface>

This is a window where many parameters are  different than the default: there are no decorations, the window is not resizable, the image is centered and both window and image are expanded over the entire screen and more. Designing the UI apart has created a dramatic simplification in the Python code, where the entire UI definition is reduced to a line of code as shown below.

import sys
try:
    import pygtk
    pygtk.require("2.0")
except:
    pass
try:
    import gtk
    import gtk.glade
except:
    print("GTK Not Availible")
    sys.exit(1)

class MeditechMain:

    wTree = None

    def __init__( self ):
        #  ============================ XML with the UI desgn definition
        builder = gtk.Builder()
        builder.add_from_file("MeditechInterface2.glade")
        # ============================
        builder.connect_signals(self)
        self.window = builder.get_object("MeditechBackground")
        self.window.fullscreen()
        self.window.maximize()
        self.window.set_keep_below(True)
        self.window.set_deletable(False)
        # self.window.show_all()

        # self.image = builder.get_object("Background")
        # self.image.show()

def main():
    gtk.main()

if __name__ == "__main__":
    mainClass = MeditechMain()
    main()

 

What makes the difference is the call add_from_file("MeditechInterface2.glade") incorporating the XML file. Obviously the PyGTK APIs remain available and can be used in the program to make changes and adaptions to the initial UI.

 

Making the design simple

It is almost intuitive that it is not simple to define the UI components in  XML. It is also obvious that this separation between design and code has also another great advantage: we can retouch and adjust some design issues without changing the code.

The reason that the UI design XML file has the glade extension derives from the name of the graphic IDE we are using, just to create the design. Again this strategy is a remembrance of the Android UI design.

image

The Glade IDE makes available all the GTK components to design the UI components seeing them as they appear at runtime; then generates the glade XML file when the design is saved to be used in the PyGTK Python application. Details on the installation and usage of the Glade IDE can be found at glade.gnome.org

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago in reply to balearicdynamics +2
    That's indeed one of the big rewards of the challenge, winner or not, to be able to play, experiment and learn new things on your own and from others
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm +2
    Enjoy ! Enrico
  • fvan
    fvan over 11 years ago +1
    Impressive work, as usual
Parents
  • phoenixcomm
    phoenixcomm over 11 years ago

    Enrico, have you ever thought of using eclipse? there is a python version. ~~ Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm

    Hello Cristina,

     

    not only though, I am using Eclipse for Android, pure java, C++ and Php. Then I have tried to use Eclipse (at least because I already now almost well the features of the IDE, updates and so on). The problem is that the Python plugin is not yet complete and as I read on the last versions of Eclipse supporting this plugin it has some problems. As in this project I already meet more problems than I can imagine, I have "temporarily" opted for the specific Python IDE that works fin on Mac.

     

    Personally I don't like so much this IDE because in a complete open source environment this has a community edition and a payment edition. Unfortunately only the payment edition gives the components for the remote editing and synchronisation so I had to make a couple of external tricks that solve only the 80% of the question.

     

    Another lack of Eclipse (and this is a mess) is the complexity to make the remote compilation with the GNU C++ toolchain that instead it can be set in minutes with NetBeans. So for the C++ development of the Raspberry PI components I definitely adopted this last solution.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 11 years ago in reply to balearicdynamics

    I have a mess here.. I am personally disgusted with the Arduino's IDE. I have a project that I thought I could do with it.. but it needs 3 libraries. ps2keybord, Wire (for port expanders), and the SoftwareSerial. the problem is the Arduino's hack of ANSI C/C++. So I took the bull by the horns and am working on getting working with the GNU-toolchain, and AVR-plugin. nexgen-software-development-arduino-sketch-eclipse-on-linux I think this makes  5 installs of eclipse that I have.. LOL I really like the TI Stellaris launchpad parts..  They have a TON of I/O  and I can use interrupts. I want to be able to use select() and just get it over.

    ~~ Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm

    Cris,

     

    I am a step ahead. I stopped to think that the Arduino IDE is NOT and IDE. Try this exercise and you feel immediately better. It's a storture. And it is not my impression only because it can be demonstrated. But why not, as Arduino is the same ?

     

    I usually develop with the AVR studio 6 but this is not the better choice of the world as it is slow by definition, based on Visual Studio from MS and has a lot of other bad stuff. I agree with you that the better and definitive solution will be the AVR GCC toolchain under Linux (then the Arduino IDE simply is a crap Java editor with the pre-built toolchain call). I tried several times with different Eclipse flavours to manage the AVR toolchain but it seems that despite the several community-driver Eclipse plugins for Arduino it is not the better environment. Maybe the worth to use NetBeans. It is true that this means adding another piece of heavy software on the computer but it seems better to manage the AVR toolchain. What do you think of this possible approach? I am already in the phase to explore the more promising direction.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm

    Cris,

     

    I am a step ahead. I stopped to think that the Arduino IDE is NOT and IDE. Try this exercise and you feel immediately better. It's a storture. And it is not my impression only because it can be demonstrated. But why not, as Arduino is the same ?

     

    I usually develop with the AVR studio 6 but this is not the better choice of the world as it is slow by definition, based on Visual Studio from MS and has a lot of other bad stuff. I agree with you that the better and definitive solution will be the AVR GCC toolchain under Linux (then the Arduino IDE simply is a crap Java editor with the pre-built toolchain call). I tried several times with different Eclipse flavours to manage the AVR toolchain but it seems that despite the several community-driver Eclipse plugins for Arduino it is not the better environment. Maybe the worth to use NetBeans. It is true that this means adding another piece of heavy software on the computer but it seems better to manage the AVR toolchain. What do you think of this possible approach? I am already in the phase to explore the more promising direction.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 11 years ago in reply to balearicdynamics

    I don't know I like your reference to storture!! to me That damn IDE is like an expresso that you get at Starbucks.  Now me personally have a used GAGGIA Syncrony Logic. No, I'm not rich, or well off but I picked it up at a Goodwill store for $5.00 :)) A good can of Medaglia D'Oro (10oz) can last me almost a year...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm

    I will adopt in future this perfect parallel:

     

    That damn IDE is like an expresso that you get at Starbucks


    In this case the correct term of this coffee (and the IDE too IMO) is brodaglia image image image

    I was a couple of months to complete a job in California on January 2014 and I am again finishing to digest the starbuck coffe...

     

    Anyway, after I saw how efficient and simple is the toolchain management and remote compilation (tried both) with the Pi and other Linux in past ( tried with LPC Linux, LTib, OpenWRT) I plan to make a serious test with NetBeans. At least to be able to make a comparison.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 11 years ago in reply to balearicdynamics

    nah, brodaglia tastes better...

    BTW the term brodaglia is what I have always called my pasta e fagioli's brodo..

    • cook a little, shredded pork  in some chicken stock.. (with a *** load of garlic), and if you have a pork bone throw that in too.
    • add diced Roma tomatoes. ( 2 cups or so  )
    • Basil, Oregano
    • open a can of Progresso Kidney Beans and rinse them off with the brodo (the hot broth)
    • wait till the flavors come together and season to taste. then add the beans
    • wait a few minutes and serve over a bowl of al dente Ditalini (the pasta)
    • pile high with shaven Locatelli
    • Fork to mouth image
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 11 years ago in reply to balearicdynamics

    come to Fort Worth, my friend and I will hook you up!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm

    I you were not so far it was the worth, trust me. Then I can invite you here to eat my Chicken-potato-onions at oven with ginger, garlic and indian spices (image available) image