Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog QuadCOP:  Final Summary and Test Flight
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: screamingtiger
  • Date Created: 29 Aug 2015 12:03 AM Date Created
  • Views 3880 views
  • Likes 7 likes
  • Comments 16 comments
  • quadcop_project
  • design_challenge
  • winners
  • sci_fi_your_pi
Related
Recommended

QuadCOP:  Final Summary and Test Flight

screamingtiger
screamingtiger
29 Aug 2015

Well this project was a great challenge and I LOVE my new QuadCOP.  I think I may rename it to DRIOD COP since I made the look akin to Star Wars droids.

 

I have posted some information that I will not repeat in this summary.  A few post that I think are very important:

Some information from my original application

Explanation of the ControlSwitch

Challenges with the ChipKit Pi

Microstack GPS and how I used it

The Sensor Array

I2C Custom Block Protcol

Rasberry Pi Turning on the camera

Autopilot Functionality I am Trying to Implement

QuadCOP Navigiation

The Test Flight Plan

First Loiter Test

Source Code and Software Flowcharts

 

My Favorite posts that are not as important but include my family:

You call that A QuadCopter? (see first video)

QuadCOP final construction pics

 

I want to provide a high level picture of the final hardware:

 

image

 

Here is the final walk around of all the hardware and elements I have used.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Parts Used from Kit:

  • Pi 2
  • Pi b+
  • Raspberry Pi Cam
  • ChipKit Pi
  • Microstack GPS
  • Xtrinsic Mems Board (still under testing)
  • Pi Shim RTC

 

 

Things I added from original design:

  • Custom Protocols
  • Moving Head
  • Use of ChipKit Pi instead of Arduino (huge learning curve)
  • Custom built quad body (instead of buying one)

 

Things I didn't get done in original design:

  • Sound Card
  • Motion Sensor
  • Sending of Text Messages (Logging is still done)

I have yet to test the waypoint navigation as I am out of time, but I will be testing that this weekend, I will add the video to this post.   Currently what I am testing it the "loiter" functionality, that it the QuadCOP attempts to stay at a specific heading and GPS location.

 

 

I am new to this hobby and did not account for the huge learning curve with some of the systems.  I also lost a month for a family vacation and wish I would of taken the project with me!

 

As a final fairwell I went out in high winds and did one last test of the loiter and also flew the quad around a bit.  The winds were very high and I wanted to see how well the quad held.  Unfortunately the camera cut out after 1 minute.  This flight was CRAZY and the QuadCOP was trying hard to holds its place.  I had to take control back a few times.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I attempted a very low loiter and the quad headed towards the ground.  There was a puddle on the ground and I think it messed up the sonic sensor, and it hit the ground!  You can see the puddles.

image

 

Since the head came off, it unplugged the RPi B and the camera, and the video didint record from inside the head.  The repairs seem minor so I am going post more vid tomorrow with a 2nd retry.

 

Conclusion

Thanks Element 14 and EVERYONE for your help and support.  I didn't get as much done as I wanted and my documentation is not as nice as I am capable of.  But rest assured in future projects my abilities and quality will continue to rise!

This project allowed me to use C++, which seems to be a dying language in the everyday workplace.  C++ is dear to my heart and thoroughly enjoyed coding the QuadCOP with a real language.

 

My family participated including holding things, getting tools, painting, and putting up with a grouchy dad!  Time with family is never wasted and as such I am very satisfied with my project.  I will continue it on forever as it will never be considered complete!  I have an awesome new RC toy with unique functionality and I plan to fly this around at my club giving demos.  It is a real show stopper!

 

Edit:  What I feel I accomplished.

 

I read the point of the contest is to push the knowledge of the Raspberry Pi 2.  I feel I did that by using wiringPi and I2C, block protocols, repeated starts, threading (Pi 2 has multiple cores) as well as sorting out the ChipKit Pi as a real time component to the Raspberry Pi.  I showed how to realistically use the Chip Kit Pi do to do real tasks that may not be suitable for a Non Real-Time System such as the Pi2 with Raspbian.

 

I don't like that I didn't get all the functionality I wanted to completed.  I do feel that I solved many issues and if someone wants to do real work with C++ and the Pi as an embedded system I have provided a strong foundation for doing that.  I felt these things were more important than adding more eye candy or videos.  Unfortunately the technical aspects do not get much attention, as is shown by my software flow charts and source code post.  I hope that someone can use my knowledge I have shared.

 

 

A few parting pictures:

image

 

image

 

image

 

image

 

image

image

 

image

 

image

image

 

The Ketteh sez was a good project.

image

We all had fun!

image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger +2
    I also learned how to be more effective going forward. In the end, I got a bunch of free stuff so all the contestants are winners! And those things will help you in the next design challenge, and many…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1 +2
    I Perfectly agree. In my case,just the fact that thanks to the Challenge (element14 etc) Meditech come alive and found its own way is the real winning. Including the option to discuss, discover and support…
  • Jan Cumps
    Jan Cumps over 11 years ago +1
    The first video is private.
Parents
  • mcb1
    mcb1 over 11 years ago

    Nice work Joey.

    Glad the family were supportive ....

     

    I think many contestants underestimate how much time and effort goes into these challenges.

    When you combine it with other family commitments, and normal work, it is a exercise in time management.

     

    While the regular updates take time, if you left it until the end, many great projects would be lacking information.

     

    I'm sure it won;t simply get plonked in the corner, so please take some time and then tackle the list.

    You can usually continue in the same area, or simply edit your post to reference a new location.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to mcb1

    Ehh I am just upset about a couple things I saw.  I also learned how to be more effective going forward.  In the end, I got a bunch of free stuff so all the contestants are winners!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger

    I also learned how to be more effective going forward.  In the end, I got a bunch of free stuff so all the contestants are winners!

    And those things will help you in the next design challenge, and many other projects.

     

    Well done.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger

    I also learned how to be more effective going forward.  In the end, I got a bunch of free stuff so all the contestants are winners!

    And those things will help you in the next design challenge, and many other projects.

     

    Well done.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    I Perfectly agree. In my case,just the fact that thanks to the Challenge (element14 etc) Meditech come alive and found its own way is the real winning. Including the option to discuss, discover and support reciprocally.

     

    Enrico