Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Sci Fi Your Pi: PiDesk - Guide: Controlling NeoPixels with the Raspberry Pi A+/B+
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 20 May 2015 10:46 AM Date Created
  • Views 3353 views
  • Likes 4 likes
  • Comments 15 comments
  • design_challenge
  • touch_motion_controls
  • touch_motion_control
  • sci_fi_your_pi
Related
Recommended

Sci Fi Your Pi: PiDesk - Guide: Controlling NeoPixels with the Raspberry Pi A+/B+

fvan
fvan
20 May 2015

  • Introduction
  • Software
  • Hardware
  • Demo

 

Introduction

 

Addressable LEDs or NeoPixels are typically used in combination with an Arduino or similar microcontroller, due to the timing critical signal required to control them. An SBC such as the Raspberry Pi is not suited for such realtime GPIO activities, as the Linux operating system runs other tasks in parallel. Or at least that was the case until Jeremy Garff found a way to use the DMA (Direct Memory Access) module to transfer bytes of memory between different parts of the processor, without using the CPU and thus not being interrupted by the Pi's OS.

 

image This procedure works for all Raspberry Pi models except version 2!

 

Software

 

Jeremy Garff has written a library called "rpi_ws281x", which can be found on his GitHub page: https://github.com/jgarff/rpi_ws281x. It makes use of the Pi's BCM2835's PWM module to drive the controllable WS281X LEDs found in NeoPixel strips and rings. The folks at Adafruit have created a Python wrapper for the library along with some Python example scripts, making it look and feel like the Arduino NeoPixels library. So if you're familiar with NeoPixels on the Arduino, you should be up and running with this version in no time.

 

To compile and install the library, follow the steps below.

 

First, install the dependencies required to download and install the library:

sudo apt-get update
sudo apt-get install build-essential python-dev git scons swig

 

Next, download the files and build the library:

git clone https://github.com/jgarff/rpi_ws281x.git
cd rpi_ws281x
scons

 

Finally, install the Python wrapper:

cd python
sudo python setup.py install

 

As you can see, these steps are very straightforward.

 

Hardware

 

Hooking up the NeoPixels to the Raspberry Pi is extremely easy, just make sure the power supply used is properly rated for the number of NeoPixels you intend to use. For testing, I used a 5V/4A power supply to power the Pi and the NeoPixels (12 and 60 LEDs).

 

image

Make sure the ground signals of the NeoPixel strip/ring and the Raspberry Pi are connected. If they are not, the LEDs won't function properly and will light up in unpredictable patterns.

 

Even though the LED strip/ring operates at 5V and the Pi's GPIO at 3.3V, it appears that it is possible to drive the LEDs without having to use logic level conversion.

 

 

Demo

 

I tested two components:

  • an Adafruit NeoPixel ring with 12 LEDs
  • an addressable WS2811 60 LED strip from eBay

 

Both performed as expected using the sample script (strandtest.py), which I edited to configure the correct number of LEDs:

 

# LED strip configuration:
LED_COUNT      = 60      # Number of LED pixels.
LED_PIN        = 18      # GPIO pin connected to the pixels (must support PWM!).
LED_FREQ_HZ    = 800000  # LED signal frequency in hertz (usually 800khz)
LED_DMA        = 5       # DMA channel to use for generating signal (try 5)
LED_BRIGHTNESS = 255     # Set to 0 for darkest and 255 for brightest
LED_INVERT     = False   # True to invert the signal (when using NPN transistor level shift)

 

As you can see, it is also possible to edit other parameters to match the LEDs used, but also parameters such as brightness.

imageimage

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 11 years ago +1
    Great work!
  • DAB
    DAB over 11 years ago +1
    Great blog. You have given me some ideas for a project I have. Thanks DAB
  • fvan
    fvan over 11 years ago in reply to balearicdynamics +1
    Hi Enrico, I believe I bought this one from Pimoroni in the UK: http://shop.pimoroni.com/products/adafruit-neopixel-ring-24-x-rgb-led-w-integrated-drivers You can choose between 24, 16 and 12 LEDs. They…
Parents
  • screamingtiger
    screamingtiger over 11 years ago

    Couple questions:

    Where did you get the strip of LEDs that can be controlled like that?  I have a tape of LEDS but they are all on or all off at once.  The addressable strip I assume is neat and I would like to maybe try some for my arcade I built.  I just purchased a bunch of mosfets to power some LEDs I have but this may provide a shortcut for some parts.

     

    In your picture, you have an external power and then you also have the raspberry pi power connected in parallel to that power.  Are you also powering up the pi through the 5V input pin?  If so I'm sorry if you know this, but this bypasses power and fuse protection.  I looked into powering it this way for my quadcopter and its not safe.   Just FYI and if you are aware of that my apologies.  Any short will blow up the Pi.  Would hate to see a good pi go to waste image

     


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to screamingtiger

    Hi Joey,

     

    the strip was bought on eBay a little more than a year ago. Search for WS2811/WS2812 LED strips, you'll find plenty variants with 30, 60 or more LEDs/meter.

     

    I know my setup bypasses the fuses and that's also why I didn't put it like that in the drawing. It's just something I quickly do when I don't have my microUSB power supply at hand. Thanks for looking out though image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fvan
    fvan over 11 years ago in reply to screamingtiger

    Hi Joey,

     

    the strip was bought on eBay a little more than a year ago. Search for WS2811/WS2812 LED strips, you'll find plenty variants with 30, 60 or more LEDs/meter.

     

    I know my setup bypasses the fuses and that's also why I didn't put it like that in the drawing. It's just something I quickly do when I don't have my microUSB power supply at hand. Thanks for looking out though image