Shift it! Warehouse Automation Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Shift it! Warehouse Automation Design Challenge
  • More
  • Cancel
Shift it! Warehouse Automation Design Challenge
Forum Reuse the stepper and frame of DVD Player
  • News
  • Forum
  • Projects
  • Leaderboard
  • Files
  • Members
  • Mentions
  • More
  • Cancel
  • New
Join Shift it! Warehouse Automation Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 46 subscribers
  • Views 1450 views
  • Users 0 members are here
Related

Reuse the stepper and frame of DVD Player

fyaocn
fyaocn over 1 year ago

1 Introduction

With previous g-code and grbl library, it is good for one CNC proto design with some handy parts .

Two dvd Player and ADI TM5272 shall be used in this case.

2 Stepper driver with ADI TM5272

Controlling with MKR wifi 1010 and driving stepper with ADI TM5272

image

The TMC5272 Evaluation Board (TMC5272-EVAL-KIT) is designed to assess the capabilities of the TMC5272, a compact, intelligent, and high-performance dual-axis stepper motor controller and driver IC. It features serial communication interfaces (SPI and UART) and comprehensive diagnostic functions, making it suitable for precise motion control applications.

Key Features & Advantages

  • Wide Power Supply Range: Operates from 2.1V to 20V DC, adapting to diverse power environments.
  • High Integration:
    • Includes four 20V H-bridges with low Rds(on) (0.31Ω typ. at TA=+25°C) for reduced power loss and heat.
    • Supports peak current per H-bridge: Imax=1.5A max, with full-scale current Ifs=0.8A rms (1.12A sinusoidal peak).
  • Silent & Smart Control Modes:
    • StealthChop 2: Enables noiseless PWM operation for quiet environments.
    • StallGuard 4: Sensorless load detection to monitor motor status in real time.
    • Tricoder: Sensorless stall detection and full-step encoder functionality for reliability.
  • High-Resolution Motion Control:
    • 8-point motion controller with minimum jerk (snap) control for smooth trajectories.
    • Auto 2D linear trajectory and axis interpolation; step/direction interface with MicroPlyerTm interpolator (up to 256 microsteps per full step).
  • Flexible Communication: SPI/UART interfaces for easy integration with microcontrollers. Includes two quadrature encoder interfaces and reference switch inputs for precise feedback.

3 Parts from Old DVD Player

Here is the frame got from two DVD players

image

Core Idea

DVD players contain high-precision stepper motors (for disc rotation and laser tracking) and linear guides (for moving the laser assembly). These components can be salvaged and adapted to build a low-cost CNC machine, in this case a 3-axis  plotter as the starter. It can be revised to router or mill.

Key Components to Salvage

  1. Stepper Motors:
    • DVD players typically use 2-phase hybrid stepper motors (e.g., for tray loading, spindle rotation, and laser positioning).
    • These motors offer fine resolution (e.g., 200 steps per revolution) and precise control, suitable for small-scale CNC movements.
  2. Linear Rails/Guides:
    • The laser assembly’s sliding mechanism often includes smooth linear guides or lead screws, which can act as CNC axis rails.
  3. Gears/Belts:
    • Gears or timing belts from the DVD drive can be used for mechanical coupling between motors and axes (e.g., for X/Y/Z motion).
      But I remove them for now.

Benefits of This Approach

  • Low Cost: Reuses discarded electronics, minimizing hardware expenses.
  • Compact: Suitable for small-scale projects (e.g., PCB milling, 3D printing, or drawing).

Challenges & Limitations

  • Power and Torque:
    • DVD stepper motors are small and low-power (often rated for <1A current). They may struggle with heavy loads or large CNC beds.

4 Next to do

This is proto type design for miniature plotter, including TE Connectors  to fit for the design.

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 1 year ago +1
    Nice project. I will be following your progress. I have a number of these old devices that I would like to repurpose.
  • phoenixcomm
    phoenixcomm over 1 year ago +1
    fyaocn This thing has been around for most likely a decade! I built a long time ago. But I used the Laser in a writer to cut and engrave plastic. Problem: It has a very small workspace! ~~ Cris BTW look…
Parents
  • phoenixcomm
    phoenixcomm over 1 year ago

     fyaocn This thing has been around for most likely a decade! I built a long time ago.  But I used the Laser in a writer to cut and engrave plastic. Problem: It has a very small workspace!  ~~ Cris 

    BTW look in your Goodwill for older sewing machines or something that does embroidery you get nice stuff with that also old printers with scanners are great for salvage of parts. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 1 year ago

     fyaocn This thing has been around for most likely a decade! I built a long time ago.  But I used the Laser in a writer to cut and engrave plastic. Problem: It has a very small workspace!  ~~ Cris 

    BTW look in your Goodwill for older sewing machines or something that does embroidery you get nice stuff with that also old printers with scanners are great for salvage of parts. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fyaocn
    fyaocn over 1 year ago in reply to phoenixcomm

    This would be best for laser engraver and I would start from small plotter.

    Thera are still many modification for the design to make it work.