Sixth Sense Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sixth Sense Design Challenge
  • More
  • Cancel
Sixth Sense Design Challenge
Documents Sixth Sense Design Challenge: The Kit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: randogless
  • Date Created: 4 Sep 2018 12:11 AM Date Created
  • Last Updated Last Updated: 18 Mar 2019 10:19 PM
  • Views 3579 views
  • Likes 11 likes
  • Comments 5 comments
Related
Recommended

Sixth Sense Design Challenge: The Kit

image
Sixth Sense Design Challenge

About this Challenge | The Kit | The Prizes | Intro Video | Technical Documents | The Judges | Example Application | Terms & Conditions | The Challengers

 

All 20 of the sponsored Challengers for the Sixth Sense Design Challenge will receive for FREE the kit detailed in the table below. 

Our judges will choose 20 applicants to become sponsored challengers, and they will receive the kit free of charge.

If you are not a sponsored challenger, you can still compete as a non-sponsored or independent challenger.  See note below.*

 

Featured Products

From STMicroelectronics:

image SensorTile Development KitSensorTile Development Kit

image STM32 Nucleo-64STM32 Nucleo-64

 

From TE Connectivity:

image KMT32BKMT32B or KMT36H

image FX19FX19

image PTF Series RTD Sensor

 

Once the sponsored Challengers receive their kit, they will then embark on their journey of designing an exciting and original project that uses the  STMicroelectronics Sensor Tile and TE Connectivity Component PackSTMicroelectronics Sensor Tile and TE Connectivity Component Pack to give a Sixth Sense to a small remotely operated or autonomous vehicle, such as a drone, robot, or tunnel exploration device.

 

*NOTE: Even if you aren't a sponsored challenger, you can still participate in the Design Challenge as long as you integrate the STMicroelectronics Sensor Tile and TE Connectivity Component Pack into your design.

 

The deadline for project application submissions is 19th November 2018.

 

 

The Kit Buy Kit*Buy Kit*
image

SensorTile Development Kit  STEVAL-STLKT01V1STEVAL-STLKT01V1

The  STEVAL-STLKT01V1STEVAL-STLKT01V1 is a comprehensive development kit designed to support and expand the capabilities of the SensorTile It is complemented with software firmware libraries and tools including a dedicated mobile app The SensorTile is a tiny square-shaped IoT module with powerful processing capabilities to leverage a high-performance Arm Cortex-M4 32-bit RISC core 80 MHz STM32L476JGY microcontroller It has on-board Bluetooth low energy connectivity based on BlueNRG-MS network processor as well as a wide spectrum of motion and environmental MEMS sensors including a digital microphone

 

image 32Bit MCU

image 3D Accelerometer

image 3D Gyroscope

image Microphone

image Bluetooth LE

image Li-Ion Battery

image
Buy NowBuy Now
image

STM32 Nucleo-64, STM32F411RE

The  NUCLEO-F411RENUCLEO-F411RE is an STM32 Nucleo development board with an STM32F411RET6 microcontroller that allows users to build their own prototypes for embedded applications The Arduino connectivity support and ST Morpho headers make it easy to expand the functionality of the STM32 Nucleo open development platform with specialized shields The STM32 Nucleo board does not require any separate probe as it integrates the ST-LINK/V2-1 debugger/programmer

 

imageSTM32F411RET6 microcontroller

imageArduino Uno Revision 3 connectivity and STMicroelectronics Morpho extension resources supported

imageOnboard ST-LINK/V2-1 debugger/programmer with SWD connector

image
Buy NowBuy Now
image

KMT32B or KMT36H Magnetic Angle Sensor

The KMT32B is a magnetic field sensor based on the anisotropic magneto resistance effect, i.e. it senses the magnetic field direction independently of the magnetic field strength for applied field strengths H>25 kA/m. The sensor contains two parallel supplied Wheatstone bridges, which enclose a sensitive angle of 45 degrees.

 

imageContactless angular position, ideal for harsh environments

imageSelf-diagnosis feature

imageHigh accuracy, extended operating temperature range

image
Buy NowBuy Now
image

FX1901 Compression Load Cell

The FX1901 is a 1% load cell device with full scale ranges of 10, 25, 50 or 100 and 200lbf compression. This technology enables force sensing in a whole new class of "smart" consumer and medical products. Operating at very low strains, MicrofusedTm technology provides an essentially unlimited cycle life expectancy, superior resolution, high over-range capabilities, and a ratiometric span of 20mV/V.

 

image10 - 200lbf ranges

imageCompact coin cell package, anti-rotation mounting features

imageLow noise, high reliability, low deflection

image
Buy NowBuy Now
image

PTF Series RTD Sensor

The PTF-sensor family combines a group of resistance temperature detectors (RTD) using a Platinum resistor in thin film technology as sensing element. The usage of platinum as resistive material guarantees high long term stability. Due to a small outline and low mass this RTD has a low time constant; therefore, it is a suitable solution for fast and precise feedback control systems.

 

image Sensing Temperature Min: -50°C to 600°C

image Low drift over lifetime

image Fast response time because of low thermal mass

image
Buy NowBuy Now

 

Interested in joining the Challengers? You can do it as a non-sponsored Challenger! Here's how:

Simply purchase the low-cost STMicroelectronics Sensor Tile and TE Connectivity Component PackSTMicroelectronics Sensor Tile and TE Connectivity Component Pack, integrate it into your project, and post 10 blogs about your design journey in the Sixth Sense space, tagging your blogs 'Sixth Sense.'  Then you'll be eligible to win the awesome prizes!

  • stm nucleo
  • sixth_sense
  • te connectivity
  • sensortile
  • design_challenge_kit
  • sixth sense design challenge
  • nucleo
  • stmicroelectonics
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 8 years ago +2
    This looks like a very interesting kit. I have a few STM boards already but not the STEVAL-STLKT01V1 which looks pretty cool. Once note though, the link for STEVAL-STLKT01V1 in the "SensorTile Development…
  • carmelito
    carmelito over 8 years ago +2
    Very interesting kit, and should be challenging challenge .. Hoping to see a quadcopter build, using the kit..
  • danzima
    danzima over 8 years ago in reply to jomoenginer +1
    Hi Jon! Thanks for the heads up. That is the JIVE platform's attempt to make a product link automatically based on text, which happens sometimes. I've removed it, because clearly it didn't link up right…
Parents
  • jomoenginer
    jomoenginer over 8 years ago

    This looks like a very interesting kit.  I have a few STM boards already but not the STEVAL-STLKT01V1 which looks pretty cool.

     

    Once note though, the link for STEVAL-STLKT01V1 in the "SensorTile Development Kit" block shows:

    "Sorry, the product link wasn't applicable for your country."

     

    I'm in the US.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jomoenginer
    jomoenginer over 8 years ago

    This looks like a very interesting kit.  I have a few STM boards already but not the STEVAL-STLKT01V1 which looks pretty cool.

     

    Once note though, the link for STEVAL-STLKT01V1 in the "SensorTile Development Kit" block shows:

    "Sorry, the product link wasn't applicable for your country."

     

    I'm in the US.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • danzima
    danzima over 8 years ago in reply to jomoenginer

    Hi Jon! Thanks for the heads up. That is the JIVE platform's attempt to make a product link automatically based on text, which happens sometimes. I've removed it, because clearly it didn't link up right! The orange "buy now" button on the right should work, that's something we created manually.