• Products and Partners
    Products and Partners
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
Sixth Sense Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sixth Sense Design Challenge
  • More
  • Cancel
Sixth Sense Design Challenge
Documents Sixth Sense Design Challenge: Technical Documents
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: randogless
  • Date Created: 4 Sep 2018 12:15 AM Date Created
  • Last Updated Last Updated: 18 Mar 2019 8:57 PM
  • Views 2379 views
  • Likes 6 likes
  • Comments 10 comments
Related
Recommended

Sixth Sense Design Challenge: Technical Documents

image
Sixth Sense Design Challenge

About this Challenge | The Kit | The Prizes | Intro Video | Technical Documents | The Judges | Example Application | Terms & Conditions | The Challengers


Check out the following technical documentation for the Sixth Sense Design Challenge

 

STMicroelectronics Sensor Tile and TE Connectivity Component Pack

 

Documentation

SensorTile Development Kit  STEVAL-STLKT01V1

STM32 Nucleo-64, STM32F411RE

G-MRCO-016 -  Angle Sensor, Magnetic, KMT32B, 180°, TDFN-8, 10 V, 4 mA

FX1901-0001-0025-L. -  COMPRESSION LOAD CELL, 25LB, 5VDC

NB-PTCO-032 -  RTD Sensor, -50 °C, 600 °C, 100 ohm, MEAS PTF Series

 

Software

SensorTile Software

 

Support

SensorTile Support
STM32 Nucleo-64 Support

  • sixth_sense
  • technical_documentation
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 7 years ago +2
    Dear E14 Community and fellow challengers, Something else I don't quite understand and I've been going around in circles is how to start my own project using the SensorTile. I could do one of two things…
  • e14phil
    e14phil over 7 years ago in reply to 14rhb +2
    Hey Rod, I will see who I can summon!
  • e14phil
    e14phil over 7 years ago +2
    Hello Challengers I have been in touch with ST direct and they have recommended emailing them here: AMS-support-EMEA@st.com If you get stuck with this support email we can try kick it up a notch after…
Parents
  • 14rhb
    14rhb over 7 years ago

    Hopefully someone could help me with a basic understanding on the SensorTile and associated boards. My understanding is that the small SensorTile board contains a STM32L476JG MCU along with other parts and it is this that I need to program. I can:

     

    (1) use the SensorTile directly in a design, soldering to the side pins

    (2) solder the SensorTile into the Cradle and use the 5-pin header to program it or

    (3) plug the SensorTile into the Cradle Expansion board

     

    I think when it was delivered there was some firmware already on the SensorTile as I was able to download an app called ST Blu Node and as I moved the Sensor Cradle around I could see a cube rotating about my phone screen plus many other really cool functions.....sometime later I managed to upload my own code and lost all that.....but have finally got back to that position. I'm using Atollic TrueStudio as my IDE.

     

    Does anyone know if that cool data is also pushed out to the SensorTile Cradle pins, maybe as UART data, and therefore if I plug that into the Nucleo F4 board I could read them? Currently when I plug the SensorTile cradle into my laptop via USB it doesn't show up so there is no way of pulling that data out via PUTTY or the like. The data is obviously getting generated as I can see it in my phone app (ST BLU )

     

    [if any of that doesn't make sense it is because I am not really sure still about the whole setup - please ask and I'll try and explain my problem more clearly.]

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to 14rhb

    I hope to be digging into the software next weekend. I expect we will have to program both the Sensor Tile MCU and the Nucleo MCU, although the Sensor Tile is pretty capable by itself so you may not need the Nucleo. There may be an example on the ST web site of the Sensor Tile sending data via the UART - I think I saw a mention of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to dougw

    Thanks Douglas,

     

    I've currently programmed my SensorTile (clicked into the SensorTile Cradle Extension) with STLKT01-Datalog and it pushes out the data I need to the USB port. I need to check that it also goes to the boards pins as then I can plug it into the Nucleo board and use that for my robot....I'd leave the SensorTile running the STLKT01-Datalog software.

     

    I modified the latter code to proove to myself I could and it now outputs the following for example:

                   
    TimeStamp: 19338
    
    
    
     Acc_X: 16, Acc_Y: -22, Acc_Z :987
     Gyro_X:-1750, Gyro_Y:-1610, Gyro_Z:560
     Magn_X:-211, Magn_Y:-90, Magn_Z:-672
     Press:996.25, Temp: 0.00, Hum: 0.0
    Rodders Data Node.
    
                   
    TimeStamp: 19358
    
    
    
     Acc_X: 16, Acc_Y: -22, Acc_Z :987
     Gyro_X:-1680, Gyro_Y:-1680, Gyro_Z:490
     Magn_X:-210, Magn_Y:-85, Magn_Z:-678
     Press:996.26, Temp: 0.00, Hum: 0.0
    Rodders Data Node.

     

    I'll have a look for the UART example, thanks.

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 7 years ago in reply to dougw

    Thanks Douglas,

     

    I've currently programmed my SensorTile (clicked into the SensorTile Cradle Extension) with STLKT01-Datalog and it pushes out the data I need to the USB port. I need to check that it also goes to the boards pins as then I can plug it into the Nucleo board and use that for my robot....I'd leave the SensorTile running the STLKT01-Datalog software.

     

    I modified the latter code to proove to myself I could and it now outputs the following for example:

                   
    TimeStamp: 19338
    
    
    
     Acc_X: 16, Acc_Y: -22, Acc_Z :987
     Gyro_X:-1750, Gyro_Y:-1610, Gyro_Z:560
     Magn_X:-211, Magn_Y:-90, Magn_Z:-672
     Press:996.25, Temp: 0.00, Hum: 0.0
    Rodders Data Node.
    
                   
    TimeStamp: 19358
    
    
    
     Acc_X: 16, Acc_Y: -22, Acc_Z :987
     Gyro_X:-1680, Gyro_Y:-1680, Gyro_Z:490
     Magn_X:-210, Magn_Y:-85, Magn_Z:-678
     Press:996.26, Temp: 0.00, Hum: 0.0
    Rodders Data Node.

     

    I'll have a look for the UART example, thanks.

     

    Rod