Smart Security and Surveillance
  • Challenges & Projects
  • Design Challenges
  • Smart Security and Surveillance
  • More
  • Cancel
Smart Security and Surveillance
Projects Sentinel Box - consensus based lock box
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Security and Surveillance to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: saramic
  • Date Created: 23 May 2026 6:36 AM Date Created
  • Views 194 views
  • Likes 2 likes
  • Comments 2 comments
  • max32630fthr
  • rust
  • LPSDK
  • design-challenge
  • vault
Related
Recommended

Sentinel Box - consensus based lock box

saramic
saramic
23 May 2026
Sentinel Box - consensus based lock box

TL;DR

A lock box that opens only when multiple parties agree — whether guarding digitally addictive devices or just the good chocolate, an unlock requires consensus from enough family members via a biometric fingerprint reader. The end result is unfortunately nothing more than a stepper motor controlled via a Bluetooth console in a browser, oh and a big a-r-s-e round box.


Introduction & Objective

Digital addiction is real — family members cannot go a few minutes before pulling out their smart device and checking on their social status or just trying to prove a point with Wikipedia or AI. We need to learn to STOP Octagonal sign. But it ain’t just digital: sugar, sweets and chocolate can unfairly be disposed of by teenagers around the house. Standard lock boxes are too small and often go to the other extreme of having no override at all.

The idea of Sentinel Box was to have consensus in the family to open the box. Be it 2 parents, a parent and a kid, or all the kids conspiring together. Consensus authorisation — the same idea behind nuclear launch codes or dual-control bank vaults — shrunk into a handy box that requires deliberate, multi-party action authenticated via a biometric fingerprint reader.

I did not make the cut in my first ever element14 Smart Security and Surveillance Design Challenge to be selected to receive the hardware for the challenge, but given there was a control board involved — the MAX32630FTHR, a compact ARM Cortex-M4F with a TI CC2564B Bluetooth module — I thought I would buy one, strap myself in and take part anyway.

What started as a brainstorm of 18 possible unlock mechanisms — from wake-word recognition to geofenced GPS checks to two-phone proximity — was focused down to what could actually be shipped: a fingerprint reader for biometrics, a stepper-motor vault bolt, and BLE for remote configuration and override. (The astronomical time lock — where the unlock window is calculated from that day’s sunset — remains on the ideas list. It is genuinely achievable. It just did not make the deadline.)

The initial concept — a simple timer lock box that inspired the final design. The perspex structure and stepper-based bolt mechanism evolved from here.


System Architecture

┌──────────────────────────────────────────────────────────┐
│                    MAX32630FTHR (96 MHz ARM M4F)         │
│                                                          │
│  UART0 (P0.0/P0.1) ──── PAN1326B ─────── BLE (CC2564B)   │
│  UART2             ──── AS608/R307 ────── Fingerprint    │
│  GPIO (P2.4/5/6)   ──── RGB LED                          │
│  GPIO (P4-5)       ──── ULN2003 ──────── 28BYJ-48 Stepper│
└──────────────────────────────────────────────────────────┘
         │
         │ BLE GATT (Web Bluetooth API)
         ▼
┌────────────────────────────────────┐
│  Chrome / sentinel-console         │
│  Vite + React + Lit web components │
│  Connect · Setup · Debug tabs      │
└────────────────────────────────────┘

Key hardware choices:

Component Role Why
MAX32630FTHR MCU + brain Challenge board. 512 KB RAM, 2 MB flash, onboard BLE
PAN1326B / CC2564B BLE radio Soldered onto the FTHR board — no extra wiring
AS608 / R307 optical fingerprint Biometric auth UART interface with onboard template matching (5 slots)
28BYJ-48 + ULN2003 Vault mechanism Cheap, geared, precise — 4096 half-steps per revolution
Perspex sheet Enclosure Cut, filed and polished by hand

The software stack is equally lean: bare-metal C on LPSDK, with BTstack as the BLE layer. I did look at a hermetic build using Rust from scratch but got stuck on the complexities of the power-on procedure of the MAX32630FTHR.


Development Process

The project evolved through five published posts and a fair amount of dead ends.

Part I — The Plan

The challenge specification landed and I dug through my junk box to find some related items: RFID readers, cameras, and mmWave proximity detectors.

image

Immediately the scope wanted to be enormous. Eighteen unlock mechanisms were sketched out — everything from morse-code tap patterns on a piezo to two-phone proximity checks.

The Rust Detour

Before committing to C, the project spent time exploring Rust on the MAX32630. A working 6-axis accelerometer attitude meter was built — the onboard BMI160 driving an external MAX7219 LED matrix to display a tilting artificial horizon.

Play this video

The attitude meter: tilt left, the bar tilts left. Tilt forward and the bar scrolls. Built entirely in Rust with raw register access.

This was real progress — cold-boot issues were traced and fixed (the 96 MHz ring oscillator needs calibration constants copied from the INFO block on every POR; the MAX7219 needs 100 ms after LDO3 comes up). But the real obstacle was the peripherals. No Rust HAL exists for the MAX32630, which means UART, I2C, and SPI would all require writing drivers from register access up. Fingerprint reader, BLE module — everything needed for the actual lock box — would each be weeks of work before the application code could start.

C and LPSDK it was.

Part II — Back to C

Switching to LPSDK unlocked the fingerprint reader immediately. The AS608 optical sensor connects via UART2 and handles template capture, merging, and matching entirely onboard. A rotary encoder selects fingerprint slots (0–F displayed on a debug terminal), a button triggers enrol or wipe, and the state machine covers five states: Startup, Idle (scan mode), Enrol, SensorError, and SlotsFull.

image

Finger placed on sensor → Letter to match the finger and a red X if the finger print has no match

Part III — Stepper Motor and Vault Lock Mechanism

The 28BYJ-48 geared stepper motor — the cheap five-wire motor that comes in every Arduino starter kit — turns out to be well-suited for a vault mechanism. 4096 half-steps per revolution, a gear ratio of roughly 64:1, and the ULN2003 Darlington array driver keeps the MAX32630’s GPIO pins well clear of the motor’s current draw.

The vault door design took several iterations. A central rotating cam pushes four separate bolts outward when locked, and the stepper drives the cam.

image

The vault mechanism design: a stepper drives a central disc which in turn drives 5 cams, the bolts extend and retract. Lock and unlock in one motion.

image

More of a reality of a single cam drive, and no idea how to attach the stepper motor.

The perspex construction revealed its own learning curve and difficulties. Cutting in a straight line is not that easy and then it takes a bit of work to file and sand pieces to spec.

Part IV — Bluetooth and BTstack

Getting BLE working on the MAX32630FTHR is more involved than the datasheet suggests. Just to get a HCI layer bare bones demo to work, required a proprietary TI vendor-specific CC256XB service pack to be uploaded — ~150 TI vendor-specific HCI commands that load the LE firmware subsystem.

Fortunately the forum posts of other element14 design challenge battlers directed me towards BTstack to replace all my hand-rolled HCI with a full BLE stack — L2CAP, ATT, SM, GATT. The GATT database is compiled from a .gatt file into a C byte array using BTstack’s Python tool. The ATT read and write handlers are straightforward callbacks.

Although I still ran into a number of advertising issues between the device and a console running in a Chrome browser, I did manage to get full read/write capabilities at full speed.

image

The first successful BLE demo: connecting from Chrome, writing 01/02/03 to the LED characteristic, watching the RGB LED change colour remotely.


The Web Console — sentinel-console

Rather than a native phone app, the control interface is a web app served from localhost using the Web Bluetooth API. Chrome and Edge support Web Bluetooth natively — any nearby BLE peripheral is reachable from a browser tab without installation.

The stack: Vite + React + TypeScript for the shell, shadcn/ui components for the UI, and Lit (Google’s 5KB web components library) for the two pieces that need genuine encapsulation — the BLE hardware abstraction layer and the debug terminal.

sentinel-console/
├── src/ble/
│   ├── SentinelBleManager.ts   ← Lit web component, owns Web Bluetooth API
│   ├── useSentinelBle.ts       ← React hook wrapping BLE events as state
│   └── gatt.ts                 ← UUID constants, command byte enums
└── src/components/
    ├── terminal/SentinelTerminal.ts  ← Lit terminal web component
    └── LedOverrideCard.tsx           ← shadcn colour buttons → 0xF002

The <sentinel-ble-manager> Lit element owns all Web Bluetooth API calls and fires typed custom events (sentinel-connected, sentinel-state-change, sentinel-gatt-notify). React hooks listen to those events and expose typed state to the rest of the tree. The <sentinel-terminal> Lit element renders a colour-coded scrolling log (tx/rx/ok/warn/error) with auto-scroll and a clear button.

image

Clicking colour buttons in the sentinel-console web app: the physical RGB LED on the board switches through red, green, and blue in real time over BLE.


Final Build

The final src/main.c build had a plan to bring everything above together. As time was running out and hardware is not as simple as software, I found myself hand filing 100s of teeth in perspex - all I could do was hope the teeth would mesh with a wheel on the stepper motor. I did get a last day success in that the gears mostly worked!!! but the reality of how long a build would take started to kick in.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In the end, I had to cut it short, I had all the electronics mounted, which I now wish I had done a month ago, but I only got around to having the stepper motor going.

imageimage

image

All in all I had a great time, even if all I got was a Bluetooth, browser controlled stepper motor controlling a cam

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Lessons Learned

The Rust exploration was worth it. Writing bare-metal Rust on hardware with no HAL forces a deep understanding of the peripherals — the POR vs SWD reset distinction, the factory calibration constants in the INFO block, the power sequencer registers. Although the knowledge was deeper than needed for my switch to C, it did give me a bigger appreciation for development boards and all that goes into their design, as well as the benefit of reading all the manuals and specifications.

BTstack is excellent. I have never successfully worked with Bluetooth and although I had some hiccups, it works!

Web Bluetooth is genuinely useful for hardware debugging. The ble_debug.html page served from localhost was the fastest way to verify BLE behaviour — no app install, no pairing ceremony, just a browser tab that reads and writes characteristics directly. Chrome’s chrome://bluetooth-internals/#devices panel shows connected device GATT tables in real time.

Hardware takes time. Although I was lucky to get a bunch of pieces working throughout the competition, and I had deferred a lot of things to software, there was still a need for hardware and that takes a lot of meticulous preparation and time.


Future Completion

  • I have committed to a big a-r-s-e box so I need to do something with it.
  • I am pretty sure the perspex I went for is a little too thin for the vault door mechanism but I do hope to build that out.
  • I am not sure I will be going back to the MAX32630FTHR anytime soon, opting for a Nano, ESP32 or STM32 instead, but the learnings have been invaluable

Source & Links

Resource Link
GitHub saramic/sentinel-box
Design challenge Smart Security and Surveillance
Project page Sentinel Box — Consensus-based Lock Box
Part I — The Plan element14 forum
Part II — Back to C element14 forum
Part III — Stepper Motor element14 forum
Part IV — Bluetooth and BTstack element14 forum
Part V — Concept vs Perfect Build  element 14 forum
  • Sign in to reply

Top Comments

  • friendlyantz
    friendlyantz 3 months ago +1
    Nice one! Not only is this clever, it’s the kind of clever that makes other projects quietly reevaluate their life choices. The consensus-based approach is giving “no single point of failure, no single…
Parents
  • skruglewicz
    skruglewicz 3 months ago

    saramic , Brilliant work! It's incredibly impressive to see you take second place in your very first element14 challenge. Way to go! Competing as a new member and delivering a project of this caliber entirely on your own dime shows real dedication. Congrats on a well-deserved win!

    Working with the sponsor kit hardware definitely gave me a run for my money too. I hit a few walls and couldn't get everything fully integrated before the deadline, but it was an awesome learning experience and I'm glad to wrap things up with a finisher prize. I'm planning to reuse my design for the "On The Line" challenge next, so here's hoping the learning curve with the Analog Devices MAX33041ESHLD# Shield is a smooth one!

    I see that you also are competing in the and were awarded the sponsor kit also. Looking for to seeing what you build.

    #skruglewicz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • skruglewicz
    skruglewicz 3 months ago

    saramic , Brilliant work! It's incredibly impressive to see you take second place in your very first element14 challenge. Way to go! Competing as a new member and delivering a project of this caliber entirely on your own dime shows real dedication. Congrats on a well-deserved win!

    Working with the sponsor kit hardware definitely gave me a run for my money too. I hit a few walls and couldn't get everything fully integrated before the deadline, but it was an awesome learning experience and I'm glad to wrap things up with a finisher prize. I'm planning to reuse my design for the "On The Line" challenge next, so here's hoping the learning curve with the Analog Devices MAX33041ESHLD# Shield is a smooth one!

    I see that you also are competing in the and were awarded the sponsor kit also. Looking for to seeing what you build.

    #skruglewicz