Smart Security and Surveillance
  • Challenges & Projects
  • Design Challenges
  • Smart Security and Surveillance
  • More
  • Cancel
Smart Security and Surveillance
Forum Sentinel Box - Part IV - Bluetooth and BTStack
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Security and Surveillance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 48 subscribers
  • Views 402 views
  • Users 0 members are here
  • ble
  • btstack
  • security-challenge
  • design-challenge
  • MAX32630FTHR#
Related

Sentinel Box - Part IV - Bluetooth and BTStack

saramic
saramic 5 months ago

As the competition end Checkered flag is nearing, I am hoping to connect to some Bluetooth to help speed up some of the configuration options of my Lock Closed lock with key Box Package — Sentinel Box.

Recap

The idea is to build a smart lock box for digital devices to help control digital addiction, more on the idea can be found in part I and coding with LPSDK and accessing a fingerprint scanner in part II, and mechanical stepper motors and vault lock mechanisms in part III:

  • Sentinel Box - Part I - the plan
  • Sentinel Box - Part II - back to C
  • Sentinel Box - Part III - Stepper Motor and Vault lock mechanism

Getting over my fears

I have a somewhat scarred history in some parts of microprocessor hobbyist programming. I recall back in the early 2000s making some relatively expensive development board unresponsive, I think it may have been running some version of J2ME Java ¯_(ツ)_/¯, I shoved it under the house and gave up for some 5 years. I thought with the advent of PIC microcontrollers , and when I got around to looking at them around 2005, I would give it a try, but after a few different approaches I failed and gave up again. By the time Arduino came around I was a little hesitant and didn’t really think much of it. Finally, at a coding hackathon in Melbourne Australia, I was lucky enough to get a Particle board — one you had to program through a web browser and by default it was internet connected by WiFi when the implications of an internet connected device sparked something in me. Noting that most Arduinos do not support wireless communications, I quickly switched to ESP32 as my go-to and was relatively happy ever since. This was until a few years ago when I wanted to connect via Bluetooth — and I failed, the project went into a box.

So with this background I got myself into this competition, where all of a sudden I would need a DAP link programmer to connect to a device, and the only wireless comms that it came with was Bluetooth. Numerous times when my device was unresponsive, I thought I had fried it somehow and it was time to put it in a box under the house. Numerous times I would touch and check voltages just in case something was heating up, or I had mixed up a wire or a voltage. This was exacerbated by my reliance on AI guiding me in a bunch of ideas like hermetic builds in a new Rust Crab tool chain only to work out I had not thought about setting up the PMIC (power management) and pins were at random voltages. I got this far, touch wood, I can finish this off.

When it came to Bluetooth  and not really understanding the communications protocol and GATT (Generic Attribute Profile) vs ATT (Bluetooth Attribute Protocol) and what is Bluetooth vs BLE (Bluetooth Low Energy) and all the write ups on bluetooth that came before me in this competition:

  • Guardian Sentinel <Part 3> — Ethernet & BLE  meera_hussien 
  • BLE scanning and CC256X firmware uploading  Alistair 
  • Identity Protocol - Part 9 - BLE GATT Challenge/Response with BTstack arvindsa 
  • Accessing the PAN1326B Bluetooth module with the Arduino IDE (Don’t Forget to Set) Alistair 
  • Accessing the PAN1326B Bluetooth module on the MAX32630fTHR Alistair 
  • Identity Protocol - Part 4 - BLE using PAN1326B and BTstack arvindsa 
    • github:arvindsa ble_beacon test using LPSDK

With things like:

CC256X firmware uploading … returned 0x01 (Unknown HCI Command), and that shown new firmware needs uploading. Has anyone done this?

and

GATT Service Definition … BTstack generates an ATT database at plaintext .gatt file. Refer: tool/compile_gatt.py … If you are new to GATT - I recommend to watch this video …

and

The first thing I do is to pull the reset pin low (aka active) white we set up some other things. There is an obscure hardware bug in the module design that at times prevents the reset from functioning as it should later

#define BT_RST P1_6
digitalWrite(BT_RST, LOW);

and

I figured since BTStack was kind enough to share the LPSDK I thought they would also include the TI’s Init Script for the CC2564B.

and

AI  no longer having access to reading artilces on Element 14 - seems like that block came in recently?

I was scared Grimacing — was I going to fry my device? Was this ever going to work? Was my reliance on AI  going to just burn tokens and not get me anywhere?

here goes nothing …

Random paths with AI

The Element 14 apparent block of AI  hit me day one. Given all the great resources of other people’s findings, I thought I would point AI at these articles and have it give me a strategy to go forward. Not paying too much attention, I just kept agreeing to the prompt to come up with a plan; only after hours of going around in circles I worked out it was actually having trouble accessing the articles and nothing to do with coming up with a plan of how to get things going. I was triggered when I saw it trying to install and set up Jina AI Reader.

Jina AI is a specialized tool designed to scrape website data and convert it into clean, LLM-friendly text or Markdown format. It is particularly useful for RAG (Retrieval-Augmented Generation) systems, AI agents, and content extraction by removing HTML clutter.

A bunch of tokens burnt and the long way round to getting Bluetooth working, as we will see shortly.

HCI (Host Control Interface)

The MAX32630FTHR has a PAN1326B Bluetooth module soldered directly on it — no external module or extra wiring needed. Inside the PAN1326B is a TI CC2564B dual-mode BT/BLE chip. It talks to the MAX32630 via UART0, via P0.0 and P0.1, simple enough, at least I couldn’t get the wiring wrong.

As I had somehow gone down the direct HCI (Host Control Interface) method, I seemed to have to start to do a lot of low-level stuff like setting up the 32kHz reference clock on P1.7 needed by the BLE module. So this required starting the crystal oscillator and enabling it

MXC_RTCCFG->clk_ctrl |= MXC_F_RTC_CLK_CTRL_NANO_EN;
MXC_RTCCFG->osc_ctrl |= MXC_F_RTC_OSC_CTRL_OSC_WARMUP_ENABLE;
MXC_PWRSEQ->reg4     |= MXC_F_PWRSEQ_REG4_PWR_PSEQ_32K_EN;
TMR_Delay(MXC_TMR0, MSEC(50));

Skipping the first two lines gives you a valid GPIO voltage on P1.7 — just no clock signal. The module boots but never initialises its HCI UART properly.

Next there was a CTS trap. The module relies on hardware flow control — specifically RTS (Ready to Send) and CTS (Clear to Send) — to manage data transmission.

With hardware flow control enabled (.cts = 1 in uart_cfg_t), the UART peripheral refuses to transmit while the CTS input (P0.2) is HIGH. During boot, the PAN1326B holds its RTS output HIGH — which feeds directly into P0.2. Result: every HCI command sits in the transmit buffer and never goes out. The fix is to disable hardware CTS checking and let the MCU transmit freely:

const uart_cfg_t ble_cfg = {
    .parity = UART_PARITY_DISABLE, .size = UART_DATA_SIZE_8_BITS,
    .extra_stop = 0, .cts = 0, .rts = 0, .baud = 115200,
};

Finally, to run BLE (Bluetooth Low Energy), the CC256XB requires a service pack???

The CC2564B chip ships without any LE (Bluetooth Low Energy) subsystem firmware. After a plain HCI Reset, standard BLE commands like HCI_LE_Set_Advertising_Parameters (opcode 0x2006) come back as “Unknown HCI Command”. Before BLE works, a service pack of ~150 TI vendor-specific HCI commands must be uploaded.

TI distributes this as CC256XB-BT-SP. The Bluetopia variant (CC256XB.h) packages all the commands as two C arrays — BasePatch[] and LowEnergyPatch[] — each a flat stream of raw HCI packets. Uploading is straightforward iteration:

while (p + 4 <= end) {
    unsigned int cmd_len = 4 + p[3];
    hci_send(p, cmd_len);
    hci_drain_event(200);
    p += cmd_len;
}

The last command in LowEnergyPatch is 0xFD5B (LE enable). It takes noticeably longer than the others and its Command Complete event can still be sitting in the UART buffer when you send the follow-up HCI Reset. The symptom: hci_reset() receives 04 0E 04 01 5B FD 00 — a valid response, but for the wrong command. The fix is to loop in hci_reset() and skip any Command Complete that isn’t for the Reset opcode 0x0C03.

The file is TI proprietary (TSPA licence)

TI TSPA License TECHNOLOGY AND SOFTWARE PUBLICLY AVAILABLE

so it lives in reference/CC256XB_BT_SP/ which is gitignored.

The license to get it reminds me of distributing encryption back in the 90s

I certify that the following is true: (a) I understand that this Software/Tool/Document is subject to export controls under the U.S. Commerce Department’s Export Administration Regulations (“EAR”).

(b) I am NOT located in Cuba, Iran, North Korea, Sudan or Syria. I understand these are prohibited destination countries under the EAR or U.S. sanctions regulations.

(c) I am NOT listed on the Commerce Department’s Denied Persons List, the Commerce Department’s Entity List, the Commerce Department’s General Order No. 3 (in Supp. 1 t o EAR Part 736), or the Treasury Department’s Lists of Specially Designated Nationals.

(d) I WILL NOT EXPORT, re-EXPORT or TRANSFER this Software/Tool/Document to any prohibited destination, entity, or individual without the necessary export license(s) or authorization(s) from the U.S. Government.

(e) I will NOT USE or TRANSFER this Software/Tool/Document for use in any sensitive NUCLEAR, CHEMICAL or BIOLOGICAL WEAPONS, or MISSILE TECHNOLOGY end-uses unless authorized by the U.S. Government by regulation or specific license. …

something was working, so now to connect

Chrome Web Bluetooth scanner

Chrome (and Edge) support the Web Bluetooth API — a page served from localhost can scan for and connect to nearby BLE peripherals without any native app. The device picker shows all advertising BLE devices:

const device = await navigator.bluetooth.requestDevice({
  acceptAllDevices: true,
  optionalServices: ["generic_access"],
});
const server = await device.gatt.connect();
const services = await server.getPrimaryServices();

The MAX32630FTHR was advertising and I had connectivity Tada

but what now? …

BTStack is the way

Seems I had gone a roundabout way to try to manually install packages and set oscillators as well as use HCI, but this was a lot of code and was not going to scale well to actually having 2-way comms between a configuration browser page and the BLE device. I re-read some of the above mentioned resources and it seemed BTStack was the way.

AI still seemed to take me down some custom “polling” method it claimed

src/btstack_port.c uses the same cooperative polling approach — not interrupt-driven DMA — but with a “simpler” single-pass structure: RX drain → TX drain → run loop tick.

but I finally corrected it to pretty much use the code from  arvindsa 

Switching from the raw HCI to BTstack — a proper BLE stack — meant the code was simpler, faster and more robust.

Following adding BTstack as a git submodule

git submodule add https://github.com/bluekitchen/btstack.git third_party/btstack

I could now compile a human-readable GATT database — .gatt → .h file into a C byte array. The service definition is trivial:

PRIMARY_SERVICE, 0000F001-0000-1000-8000-00805F9B34FB
    CHARACTERISTIC, 0000F002-..., DYNAMIC | WRITE | WRITE_WITHOUT_RESPONSE,

And I could now access this from the browser and by writing data, see changes on the board.

LED Red/Green/Blue controll via Web Bluetooth control

shows that changes on the Chrome page change the LED colour: 01 — RED Red circle, 02 — GREEN , 03 — BLUE Large blue circle.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Next

Ok, I have some Bluetooth, a dash of stepper and a finger scan or two. I am away down the coast at the moment so I cannot attempt the build of the vault mechanism till I have access to my limited tools. I am feeling bullish and maybe I should also get access to writing some things to the SD card, but maybe it is time to start to bring these things together in a final design of a Bluetooth-controlled setup for capturing fingerprints, locking and unlocking once the required family members have scanned their fingers.

Source

https://github.com/saramic/sentinel-box

  • Sign in to reply
  • Cancel

Top Replies

  • meera_hussien
    meera_hussien 5 months ago +1
    great progress...
  • meera_hussien
    meera_hussien 5 months ago

    great progress...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo 5 months ago

    Great post.  Good job on getting the Bluetooth going.