Smart Spaces Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Smart Spaces Design Challenge
  • More
  • Cancel
Smart Spaces Design Challenge
Forum PROBLEMS - Using MCUXpresso IDE with MCXA153 and MCXN236 on the same PC
  • Forum
  • Projects
  • Info
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Spaces Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 38 subscribers
  • Views 1298 views
  • Users 0 members are here
  • NXP FRDM MCX A
  • NXP FRDM MCX A & MCX N development kit.
  • nxp
  • NXP FRDM MCX N
Related

PROBLEMS - Using MCUXpresso IDE with MCXA153 and MCXN236 on the same PC

skruglewicz
skruglewicz over 1 year ago

I'm currently working to run example code on both the MCXA153 and MCXN236 boards from the same instance of MCUXpresso IDE on a single PC. I wanted to share my experiences here, in case anyone else is attempting this during the challenge, Also, to offer a solution I found for one of the issues I encountered after struggling with the IDE for some time. There’s still another issue described at the end of this post that I’m having difficulty understanding.

I followed the instructions on the MCXA153 Build and Run  page. On this page I learned:

  • To import an SDK example (like hello world) into MCUXpresso IDE.
  • The guide walks you through selecting the FRDM MCX board, expanding the demo_apps category, and choosing hello_world.
  • You’ll build the demo and set the debug console to UART for serial output.
  • Steps include connecting the board via USB MCU-LINK port, flashing the application, and selecting the MCU-Link CMSIS-DAP debug probe. NOTE – Be sure to include the 
  • Instructions for opening a serial terminal (settings: 115200 baud, 8 data bits, no parity, 1 stop bit) are provided.
  • Finally, you will run the demo and see terminal output.

 I tried the “hello world example” on both devices to get a feel for developing on two devices from the same IDE on the same PC. I followed the instructions from the “Build and Run Page” outlined above. I was able to get the example to run on the MCXA153 the first time, but unable to successfully run again after getting the following problem, trying to run it on the MCXN236 

Problem:1:  “no Terminal output” 

  1. Build 
  2. Debug 
  3. The following dialog appears to select a probe
    1. I selected the MCU-Link CMSIS-DAP debug probe for the MCXN236: 

image

I selected the MCU-Link CMSIS-DAP debug probe for the MCXN236:

image

Hint: the next time you run the code, this screen does not show. to allow it to show up again , simply delete the file "frdmmcxn236_hello_world LinkServer Debug.launch", in this case for the MCXN236. Now the dialog should come up on the debug session.

Open up a serial terminal to be able to see the application's output.

       Problem: empty terminal?

image

What could be wrong?

Solution : I had the wrong Serial COM port selected. It needs to be the com port that the MCXN236 is connected to . In my case it is COM4. 

Select the “Terminal” window and press the “new terminal” icon. Choose a “Serial Terminal” and then set the UART settings to 115200 baudrate, 8 bit data size, no parity and 1 stop bit. Press OK.

 image

Oh now the mcxa153 project is also working . I need to select the correct SDK, debug probe port and set the serial port at the proper COM port, in ny case COM3.

Now the debugger is running but it hangs the code here after pressing a character on the screen?

image

NOW I’m stuck and pondering this second Problem:

Why is it printing 2 lines of “Hello World”?
Why is it paused at the line ch = GETCHAR();
What is it expecting from the function call GETCHAR()


I was wondering If any of the challengers have this problem or have an answer? For now I’ll be continuing to run other coding examples to keep experimenting with the IDE using 2 devices.

Happy coding

  • Sign in to reply
  • Cancel

Top Replies

  • skruglewicz
    skruglewicz 10 months ago +3
    wrong comment see: NO connection to chips debug port on the MCXN236?
  • balajivan1995
    balajivan1995 over 1 year ago +2
    I'm also facing the same issue when using two boards at the same time. 1. The reason you are getting two "Hello world" is, after the firmware was flashed, it immediately starts running in application…
  • Jan Cumps
    Jan Cumps 11 months ago in reply to skruglewicz +1
    skruglewicz said: Regarding your number 2 and 3 answers, that's what I thought initially, but when I started typing in the terminal, I didn't notice anything happening on the screen. I'll give it another…
Parents
  • balajivan1995
    balajivan1995 over 1 year ago

    I'm also facing the same issue when using two boards at the same time. 

    1. The reason you are getting two "Hello world" is, after the firmware was flashed, it immediately starts running in application mode before switching to debug mode. 

    2. GETCHAR() is a blocking UART receive function that requires you to type a character in the serial terminal.

    3. Once you provide an input, it'll be printed automatically on the screen using PUTCHAR(ch);

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • skruglewicz
    skruglewicz 11 months ago in reply to balajivan1995
    balajivan1995 said:

    I'm also facing the same issue when using two boards at the same time. 

    1. The reason you are getting two "Hello world" is, after the firmware was flashed, it immediately starts running in application mode before switching to debug mode. 

    2. GETCHAR() is a blocking UART receive function that requires you to type a character in the serial terminal.

    3. Once you provide an input, it'll be printed automatically on the screen using PUTCHAR(ch);

    Thank you for responding, balajivan1995 ! I really appreciate you taking the time to answer my questions. It's great to know that you are also using the same IDE for 2 boards as I am.

    Your number 1 answer about the double print messages really clears things up for me - that makes perfect sense now!

    Regarding your number 2 and 3 answers, that's what I thought initially, but when I started typing in the terminal, I didn't notice anything happening on the screen. I'll give it another try when I get a chance.

    Thanks again for your reply!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps 11 months ago in reply to skruglewicz
    skruglewicz said:
    Regarding your number 2 and 3 answers, that's what I thought initially, but when I started typing in the terminal, I didn't notice anything happening on the screen. I'll give it another try when I get a chance.

    in the eclipse terminal, you have to put your cursor in a little (somewhat bland) input box at the bottom of that terminal window. It's not obvious until you saw it once.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balajivan1995
    balajivan1995 11 months ago in reply to skruglewicz
    skruglewicz said:

    Regarding your number 2 and 3 answers, that's what I thought initially, but when I started typing in the terminal, I didn't notice anything happening on the screen. I'll give it another try when I get a chance.

    I don't like the serial terminal that usually comes with eclipse IDE.  I use a separate application called HTERM to monitor my UART data.
    If you want to see how I send and receive UART data, you can follow this video. I have also provided subtitles in case it's hard to listen to my voice.


    community.element14.com/.../dds-elevator---hello-world

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balajivan1995
    balajivan1995 11 months ago in reply to skruglewicz
    skruglewicz said:

    Regarding your number 2 and 3 answers, that's what I thought initially, but when I started typing in the terminal, I didn't notice anything happening on the screen. I'll give it another try when I get a chance.

    I don't like the serial terminal that usually comes with eclipse IDE.  I use a separate application called HTERM to monitor my UART data.
    If you want to see how I send and receive UART data, you can follow this video. I have also provided subtitles in case it's hard to listen to my voice.


    community.element14.com/.../dds-elevator---hello-world