Smart Spaces Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Smart Spaces Design Challenge
  • More
  • Cancel
Smart Spaces Design Challenge
Forum PROBLEMS - Using MCUXpresso IDE with MCXA153 and MCXN236 on the same PC
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Spaces Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 40 subscribers
  • Views 272 views
  • Users 0 members are here
  • NXP FRDM MCX A
  • NXP FRDM MCX A & MCX N development kit.
  • nxp
  • NXP FRDM MCX N
Related

PROBLEMS - Using MCUXpresso IDE with MCXA153 and MCXN236 on the same PC

skruglewicz
skruglewicz 1 month ago

I'm currently working to run example code on both the MCXA153 and MCXN236 boards from the same instance of MCUXpresso IDE on a single PC. I wanted to share my experiences here, in case anyone else is attempting this during the challenge, Also, to offer a solution I found for one of the issues I encountered after struggling with the IDE for some time. There’s still another issue described at the end of this post that I’m having difficulty understanding.

I followed the instructions on the MCXA153 Build and Run  page. On this page I learned:

  • To import an SDK example (like hello world) into MCUXpresso IDE.
  • The guide walks you through selecting the FRDM MCX board, expanding the demo_apps category, and choosing hello_world.
  • You’ll build the demo and set the debug console to UART for serial output.
  • Steps include connecting the board via USB MCU-LINK port, flashing the application, and selecting the MCU-Link CMSIS-DAP debug probe. NOTE – Be sure to include the 
  • Instructions for opening a serial terminal (settings: 115200 baud, 8 data bits, no parity, 1 stop bit) are provided.
  • Finally, you will run the demo and see terminal output.

 I tried the “hello world example” on both devices to get a feel for developing on two devices from the same IDE on the same PC. I followed the instructions from the “Build and Run Page” outlined above. I was able to get the example to run on the MCXA153 the first time, but unable to successfully run again after getting the following problem, trying to run it on the MCXN236 

Problem:1:  “no Terminal output” 

  1. Build 
  2. Debug 
  3. The following dialog appears to select a probe
    1. I selected the MCU-Link CMSIS-DAP debug probe for the MCXN236: 

image

I selected the MCU-Link CMSIS-DAP debug probe for the MCXN236:

image

Hint: the next time you run the code, this screen does not show. to allow it to show up again , simply delete the file "frdmmcxn236_hello_world LinkServer Debug.launch", in this case for the MCXN236. Now the dialog should come up on the debug session.

Open up a serial terminal to be able to see the application's output.

       Problem: empty terminal?

image

What could be wrong?

Solution : I had the wrong Serial COM port selected. It needs to be the com port that the MCXN236 is connected to . In my case it is COM4. 

Select the “Terminal” window and press the “new terminal” icon. Choose a “Serial Terminal” and then set the UART settings to 115200 baudrate, 8 bit data size, no parity and 1 stop bit. Press OK.

 image

Oh now the mcxa153 project is also working . I need to select the correct SDK, debug probe port and set the serial port at the proper COM port, in ny case COM3.

Now the debugger is running but it hangs the code here after pressing a character on the screen?

image

NOW I’m stuck and pondering this second Problem:

Why is it printing 2 lines of “Hello World”?
Why is it paused at the line ch = GETCHAR();
What is it expecting from the function call GETCHAR()


I was wondering If any of the challengers have this problem or have an answer? For now I’ll be continuing to run other coding examples to keep experimenting with the IDE using 2 devices.

Happy coding

  • Sign in to reply
  • Cancel

Top Replies

  • skruglewicz
    skruglewicz 7 days ago +3
    UPDATE STATUS on this problem It works on the new PC with a clean MCUXpresso + SDK install, so the board and probe are fine, and the root cause is almost certainly something broken or conflicting on…
  • balajivan1995
    balajivan1995 1 month ago +2
    I'm also facing the same issue when using two boards at the same time. 1. The reason you are getting two "Hello world" is, after the firmware was flashed, it immediately starts running in application…
  • Jan Cumps
    Jan Cumps 1 month ago in reply to skruglewicz +1
    skruglewicz said: Regarding your number 2 and 3 answers, that's what I thought initially, but when I started typing in the terminal, I didn't notice anything happening on the screen. I'll give it another…
Parents
  • skruglewicz
    skruglewicz 7 days ago

    UPDATE STATUS on this problem

    It works on the new PC with a clean MCUXpresso + SDK install, so the board and probe are fine, and the root cause is almost certainly something broken or conflicting on the original PC’s toolchain/driver side rather than the hardware.

    Brief summary

    On a new PC I installed MCUXpresso (24.12) and the SDK (24.12.00), connected the FRDM‑MCXN236, built an example, and debug worked immediately. On the original PC I have MCUXpresso 25.6 with SDK 25.09.00, and despite reinstalling, updating LinkServer, trying LinkFlash, firmware updates, and ISP/bootloader mode, you still get Ee(42). Could not connect to core / No connection to chip's debug port.That confirms the FRDM‑MCXN236 and MCU‑Link firmware are good and isolates the problem to the original  Windows environment.

    Likely causes on the original  PC

    Most probable categories, given that the exact same board works elsewhere:

    • Corrupted or conflicting USB/debug drivers (MCU‑Link / CMSIS‑DAP / WinUSB) on the   original  PC, possibly from prior NXP, SEGGER, PE Micro, or other probe installs.

    • A stale or mismatched LinkServer instance or config on the   original  PC that the IDE keeps reusing, so the probe enumerates but SWD never actually connects to the target core.

    • Security/IT software (AV, endpoint protection, USB control) on the   original  PC interfering with USB enumeration or blocking the debug interface, while the new laptop is more “clean.

    • Leftover MCUXpresso or SDK fragments from original versions in different paths, causing the IDE to point at the wrong debug driver or XML/config for MCXN236 even though the latest SDK is installed.

    I have researched a few things I could try which I will and update this post. so stay tuned

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • skruglewicz
    skruglewicz 7 days ago

    UPDATE STATUS on this problem

    It works on the new PC with a clean MCUXpresso + SDK install, so the board and probe are fine, and the root cause is almost certainly something broken or conflicting on the original PC’s toolchain/driver side rather than the hardware.

    Brief summary

    On a new PC I installed MCUXpresso (24.12) and the SDK (24.12.00), connected the FRDM‑MCXN236, built an example, and debug worked immediately. On the original PC I have MCUXpresso 25.6 with SDK 25.09.00, and despite reinstalling, updating LinkServer, trying LinkFlash, firmware updates, and ISP/bootloader mode, you still get Ee(42). Could not connect to core / No connection to chip's debug port.That confirms the FRDM‑MCXN236 and MCU‑Link firmware are good and isolates the problem to the original  Windows environment.

    Likely causes on the original  PC

    Most probable categories, given that the exact same board works elsewhere:

    • Corrupted or conflicting USB/debug drivers (MCU‑Link / CMSIS‑DAP / WinUSB) on the   original  PC, possibly from prior NXP, SEGGER, PE Micro, or other probe installs.

    • A stale or mismatched LinkServer instance or config on the   original  PC that the IDE keeps reusing, so the probe enumerates but SWD never actually connects to the target core.

    • Security/IT software (AV, endpoint protection, USB control) on the   original  PC interfering with USB enumeration or blocking the debug interface, while the new laptop is more “clean.

    • Leftover MCUXpresso or SDK fragments from original versions in different paths, causing the IDE to point at the wrong debug driver or XML/config for MCXN236 even though the latest SDK is installed.

    I have researched a few things I could try which I will and update this post. so stay tuned

    • Cancel
    • Vote Up +3 Vote Down