Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 010
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 10 Nov 2013 8:49 PM Date Created
  • Views 615 views
  • Likes 0 likes
  • Comments 2 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 010

COMPACT
COMPACT
10 Nov 2013

SPI - DERs!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here is the result of driving two MCP23S17 16-bit GPIO drivers using a PSoC 4.

The PSoC4 SPI Master component has a hardware driven SS (Slave Select) signal and it not always appropriate to use it.

For these cases the SS needs to be driven under firmware control.

One such beast is the Microchip MCP23S17 where the its version of SS called -CS needs to be asserted (held low) for a varying number of bytes according to the circumstance.

Since there is a FIFO used for the SPI Master component, the SPI Master's status register must be monitored to ensure that the control of the SS occurs correctly.

 

The MCP23S17 has a special addressing mode that allows up to 8 MCP23S17s to be driven from the same SPI bus.

This is disabled by default and can be enabled by setting a device configuration bit and tying 3 address pins to the desired value.

  • Sign in to reply

Top Comments

  • COMPACT
    COMPACT over 12 years ago in reply to DAB +1
    Hi Don, The answer is yes. The memory adds absolutely no timing issues with my display idea. Although it seems counter intuitive I have configured my design so that the SPI SRAMs add NO DELAYs when displaying…
Parents
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Have you measured the delay introduced by the MCP23S17 devices from the PSOC to the SPI device?

    I wonder if the delay might add some timing issues with your display idea.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 12 years ago in reply to DAB

    Hi Don,

    The answer is yes.

    The memory adds absolutely no timing issues with my display idea.

    Although it seems counter intuitive I have configured my design so that the SPI SRAMs add NO DELAYs when displaying data.

    I have tested it thoroughly and confirmed that it works perfectly .

     

    Cheers

    Very Compact

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 12 years ago in reply to DAB

    Hi Don,

    The answer is yes.

    The memory adds absolutely no timing issues with my display idea.

    Although it seems counter intuitive I have configured my design so that the SPI SRAMs add NO DELAYs when displaying data.

    I have tested it thoroughly and confirmed that it works perfectly .

     

    Cheers

    Very Compact