Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 016
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 18 Nov 2013 10:55 AM Date Created
  • Views 456 views
  • Likes 1 like
  • Comments 1 comment
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 016

COMPACT
COMPACT
18 Nov 2013

Captured on Film!

image

The Timer (2.5) component also has a capture input.

It's options are identical to the timer's trigger options:

  • None
  • Rising Edge
  • Falling Edge
  • Either Edge
  • Software Controlled

With the Capture Counter checkbox unchecked, the Capture pin is similar to a Lap time button of a stopwatch but works for a down counter rather than an up counter.

The Capture causes the value of the timer to be captured for use for another process.

The Capture doesn't cause the timer to stop counting down so you can capture many moments during a single countdown cycle until the TC (Terminal Count) is reached in single shot mode.

 

When the Capture Counter checkbox is checked, the capture pin acts a bit like a Swedish power switch and will only capture the countdown value after the specified number of capture events.

For example, when the Capture counter is set to 2, only every second valid capture event is captures the value of the countdown timer. This is equivalent to the double clicks required on some Swedish power switches to toggle the state the switch.

Likewise when set to 3, only every third capture event captures the value of the countdown timer.

 

I know that you can use Capture in combination with One Shot Run Mode and Triggers to measure the duration of a digital pulse signal.

In the next article I'll demonstrate it.

 

BTW - The photo above has nothing to do with the timer component except to show the backside of the Pioneer Kit and its very useful annotations.

I wonder if you captured that furphy?

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Good post.  I had not looked at the capture timer option, but I have several applications where I need that capability.

     

    Thanks for bringing it to my attention.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Good post.  I had not looked at the capture timer option, but I have several applications where I need that capability.

     

    Thanks for bringing it to my attention.

     

    DAB