Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 035
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 17 Dec 2013 10:37 AM Date Created
  • Views 460 views
  • Likes 0 likes
  • Comments 1 comment
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 035

COMPACT
COMPACT
17 Dec 2013

Proof Of Life

image

 

Another boring photo but it shows 9 panels (2,304 LEDS) being driven by a single PSoC 4 and my one of my secret circuits.

Anyone for TV tennis as a side project?

I could have used colour but decided of a low brightness white.

 

Each panel has a unique pattern displayed to prove that it that is individually driven.

The only reason for 9 and not 12 panels is that I only have a 3A power supply attached.

With no LEDs lit the quiescent current is 2.13A. It sounds a lot but it works out to be about 1mA per LED.

 

One remarkable aspect of the WS2812B LEDs is that they are static so once a value has been assigned to a LED it will remain in that state indefinitely until the value is changed, the power removed or the device is broken.

Yes, sure enough each LED has 3 bytes of RAM.

The caveat is that it is only optically readable.

 

Technology, what'll they think of next?

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Good update.

    It looks like you have the setup to do some awesome displays with that level of control.

    I like the idea that the LED will hold its last state until it receives an update.

    May have to look into those LEDs for one of my projects.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Good update.

    It looks like you have the setup to do some awesome displays with that level of control.

    I like the idea that the LED will hold its last state until it receives an update.

    May have to look into those LEDs for one of my projects.

    DAB