Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog PSoC 4 Tricopter (Smarter Life Challenge) part #5
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yuritikhonov
  • Date Created: 24 Nov 2013 7:10 PM Date Created
  • Views 1438 views
  • Likes 1 like
  • Comments 2 comments
  • RoadTest
  • tricopter
  • psoc4
  • Multiwii
  • smarter_life_challenge
  • smarter_life
  • smart_tricopter
  • smart_control_and_diagnostics
  • arduino
  • quadcopter
Related
Recommended

PSoC 4 Tricopter (Smarter Life Challenge) part #5

yuritikhonov
yuritikhonov
24 Nov 2013

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

 

Good day comrades!

Let's talk today about the next stage on the road to success, namely about the EEPROM emulation.

 

You're probably thinking, why is this guy spending so much time working on software changing almost nothing in the hardware?

The answer is simple: I still have not received a parcel from HobbyKing and not only that, they even didn't give me the track number!

But we will not dwell on this, because I believe that tricopter will be built in time image

 

So let's go! An important part of the software for a tri or quadcopters is the non-volatile memory for storage of configuration. In the AVR-based MultiWii we use EEPROM as the most suitab.PSoC has the ability to emulate EEPROM memory, for this purpose there is a special unit which is a nothing else but the API to access the flash memory of the controller, which, like the EEPROM is non-volatile.

 

Today PSoC's schematics look like this:

image

 

Like the last time, here is a piece of code that I use to work with virtual EEPROM:

 

1. Copying data from one memory area to another (I wrote this function with the use of "volatile uint8", as recommended by Cypress):

void toMem(void *des, const void *src, uint8_t size)
{
    uint8_t i;
    uint8_t *cdes = (uint8_t *) des;
    for (i=0; i<size; i++) *cdes++ = *((volatile uint8_t *) src + i);
}

 

2. Read data from EEPROM to RAM (for more details see original MultiWii source code).  "static const uint8_t eep_array[64]" variable locate in flash memory (it's a virtual EEPROM):

void readEEPROM(void)
{
  uint8_t i, _address = eep_entry[0].size;
  for(i=1; i<EEBLOCK_SIZE; i++)
  {
    toMem(eep_entry[i].var, &eep_array[_address], eep_entry[i].size);
    _address += eep_entry[i].size;
  }
  for(i=0;i<7;i++) lookupRX[i] = (2500+rcExpo8*(i*i-25))*i*(int32_t)rcRate8/1250;
}

 

3. Write data from RAM to EERPOM:

void writeParams(void)
{
    uint8_t d = EEBLOCK_SIZE;
    uint8_t i, _address = 0, data_array[64];
    for(i=0; i<EEBLOCK_SIZE; i++)
    {
        toMem(&data_array[_address], eep_entry[i].var, eep_entry[i].size);
        _address += eep_entry[i].size;
    }

    d = sizeof(data_array);
    vEEPROM_Write(data_array,eep_array,sizeof(data_array));
    readEEPROM();
}

 

4. "after first turn on" function:

void checkFirstTime(void)
{
    uint8_t i, test_val = *(volatile uint8_t *) eep_array;
    if (test_val == checkNewConf) return;

    P8[ROLL]      = 40; I8[ROLL]    = 30; D8[ROLL]    = 23;
    P8[PITCH]    = 40; I8[PITCH]    = 30; D8[PITCH]    = 23;
    P8[YAW]      = 85; I8[YAW]      =  0;  D8[YAW]    =  0;
    P8[PIDALT]    = 16; I8[PIDALT]  = 15;  D8[PIDALT]  =  7;
    P8[PIDGPS]    = 50; I8[PIDGPS]  =  0;  D8[PIDGPS]  = 15;
    P8[PIDVEL]    =  0; I8[PIDVEL]  =  0;  D8[PIDVEL]  =  0;
    P8[PIDLEVEL]  = 90; I8[PIDLEVEL] = 45; D8[PIDLEVEL] = 100;
    P8[PIDMAG]    = 40; rcRate8      = 45; rcExpo8      = 65;
    rollPitchRate =  0; yawRate      =  0; dynThrPID    =  0;
    for(i=0;i<CHECKBOXITEMS;i++)
    {
        activate1[i] = 0;
        activate2[i] = 0;
    }
    accTrim[0] = 0; accTrim[1] = 0; powerTrigger1 = 0;
    writeParams();
}

 

And lastly, the main function (for a better understanding of each of it's functions, I recommend you read my previous posts in this blog):

 

void main()
{
    tikInit();
    eepromInit();
    checkFirstTime();
    SerialOpen(0,115200);
    readEEPROM();
    configureReceiver();
    CyGlobalIntEnable;

    for(;;)
    {
        computeRC();
        serialCom();
    }
}

 

So, let us examine the steps, how our software is working at the moment:

  1. The configuration of all the systems (UpTime, EEPROM, Serial, RX);
  2. After initialization of the EEPROM we test the "is it a first running of the system?" if Yes, the defaulte date is recorded in the EEPROM;
  3. After configuration we turn on the global interrupts;
  4. In the main loop we read the data from RX and trying to communicate PSoC with PC-program;
  5. If PC-program requests the data - we try to transmitt it via UART;
  6. If PC-program suggests to write the data to EEPROM, the PSoC tryint to get it and write it to EEPROM via writeParams() function

 

Below you can see the animation of the work with EEPROM you can review the content of every slide:

  1. Loading firmware to PSoC;
  2. Launching the PC-program;
  3. Connecting to the PSoC via UART
  4. Correction of the data (RC RATE and EXPO by this example)
  5. Writing data to the EEPROM (WRITE button)
  6. Turning off the PSoC development board (COM7 is escaped)
  7. Turning on the PSoC back (COM7 is come back)
  8. Connecting to PSoC...
  9. ...and reading the data

image

 

As you can see, the data was successfully wrote to EEPROM and read back again after voltage brownout!

Next week I plan to realise motor's control function and this means that the moment of the first field trials is coming soon!

 

See you next week!

                                                                                                                                              

#linkdescription
1PSoC 4 Tricopter Part #1Introduction
2PSoC 4 Tricopter Part #2Purchase of components from Farnell and HobbyKing
3PSoC 4 Tricopter Part #3PSoC firmware: upTime & Rx
4PSoC 4 Tricopter Part #4PSoC firmware: UART & MultiWii GUI
5PSoC 4 Tricopter Part #5PSoC firmware: EEPROM emulation
6PSoC 4 Tricopter Part #6PSoC firmware: Servo & ESC control
7PSoC 4 Tricopter Part #7PSoC firmware: IMU, LED's & PID
8PSoC 4 Tricopter Part #8Hardware: PCB
9PSoC 4 Tricopter Part #9Hardware: tricopter's frame
10PSoC 4 Tricopter Part #10Hardware: YAW mechanics & motors
11PSoC 4 Tricopter Part #11Hardware: ESC's, wires & misc
12PSoC 4 Tricopter Part #12Final: The first fly

 

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Good update.

     

    I agree with your decision to work out as many details as you can before you get the rest of your components.

    Most of the interface issues need to be worked one at a time and then integrated.  Using a simulation to test out the transfer and protocol issues is standard procedure.

     

    Look forward to your next post.

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to DAB

    Thanks DAB! I'm starting to worry about the components, you know, I can't even try to test the motor control system without ESC's and motors...

    Now the minimum plan is as follows: fly to the sky image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to DAB

    Thanks DAB! I'm starting to worry about the components, you know, I can't even try to test the motor control system without ESC's and motors...

    Now the minimum plan is as follows: fly to the sky image