Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog PSoC 4 Tricopter (Smarter Life Challenge) part #8
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yuritikhonov
  • Date Created: 15 Dec 2013 3:23 PM Date Created
  • Views 1646 views
  • Likes 1 like
  • Comments 6 comments
  • RoadTest
  • tricopter
  • psoc4
  • Multiwii
  • smarter_life_challenge
  • smarter_life
  • smart_tricopter
  • smart_control_and_diagnostics
  • arduino
  • quadcopter
Related
Recommended

PSoC 4 Tricopter (Smarter Life Challenge) part #8

yuritikhonov
yuritikhonov
15 Dec 2013

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

 

Good day comrades!

This week, the last before the beginning of voting, I still haven't received the parcel from HobbyKing. Nevertheless, Russia is still in game!

 

This week we begin a new stage: "hardware", but I must save a bit of material on the case, if the parcel with spare parts will not come.

Already done:

  • Schematics were developed;
  • PCB layout was made;
  • PCB was made in the old-school style image
  • Pioner Kit was turned into a convenient programmer for external PSoC chips.

 

1. Initially I wanted to use PSoC at 3.3v, thus the following diagram was born, I used CAD-System DipTrace to draw it (schematics developed according to Russian standards, however, they differ a little from the western ones):

image

 

But after reading the datasheet, I found that in contrast to all "Cortex M" family MCU's, with which I worked earlier, the PSoC is able to operate at 5v! Circuitry was seriously simplified:

image

 

2. The next step was making the PCB, then I looked posts of other participants and saw that the level of performance was good enough! I decided to go the other way: to run the old-school tracing and to use a parallelepiped-shaped PCB. After all, we are having a creativity contest image

 

For tracing I used CAD-System TopoR (if you knew a little Russian, this name will make you smile). However the TopoR, Russian version of the DipTrace, and the OS Windows 7 Professional x64 have been refusing to be friends for a long time. But I wanted so much to make an unusual PCB that I managed to overcome this problem!

image

 

3. Captain Obvious reminds: December is the last month of the year! I am a PhD-student and I have a huge amount of work on the thesis. My printer worked in emergency mode and the day when I decided to make a printed-circuit-board, the printer suddenly broke down image

 

However, I found an activity: I understood that I need to flash the PSoC, and it will require the programmer. However, at the time of ordering components I forgot the programmer... I want to use the Pioneer Kit to program an external controllers. For this, I downloaded the firmware source code and decided to give it a little change, overriding SWDCLK and SWDIO lines thus to have access from outside:

 

image

However, this week gave me another surprise: the PSoC refused flatly being flashed! After long hours of torment, I found a solution!

 

In the original: SWDCLK = P2.1 and SWDIO = P2.0. I decided to override them on P0.0 and P0.1 respectively. Guess why? Exactly! At the end, after making SWDCLK = P0.1, SWDIO = P0.0 I was surprised to find that the programmer worked, Bingo!!!

image

image

 

4. Meanwhile, I fixed my printer. PCB was made (the photo was made before drilling and final grinding):

image

 

Next I bought  all the necessary components at a local store and soldered everything together:

image

 

Finaly, tricopter control system looks as follows:

image

 

I yet did not drill the mounting holes, because I still don't have the frame...

Did you notice the location of the LEDs? Yes-Yes, this is also an echo of unusual design image

 

5. So, let's summary the work today:

  • Was written firmware for PSoC. Although the  MultiWii 2.0 was taken as basis, I did a great job on revision of the code was studied every line of the program, significant structural changes were made, in general I am very pleased with the work done!
  • Were manufactured and tested the control system PCB.
  • Were ordered and paid all necessary parts, but the fault of HobbyKing, the majority of them is still on the way. Small details I bought in local shops, no problem with them.

 

Next week, if the components do not come, I'll make all the remaining details "blindly", without a clear understanding of the dimensions of the basic units of the machine + I have a stock of cool stuff image This copter is not first for me, so I must  successfully cope!

 

See you next week!

                                                                                                                                              

#linkdescription
1PSoC 4 Tricopter Part #1Introduction
2PSoC 4 Tricopter Part #2Purchase of components from Farnell and HobbyKing
3PSoC 4 Tricopter Part #3PSoC firmware: upTime & Rx
4PSoC 4 Tricopter Part #4PSoC firmware: UART & MultiWii GUI
5PSoC 4 Tricopter Part #5PSoC firmware: EEPROM emulation
6PSoC 4 Tricopter Part #6PSoC firmware: Servo & ESC control
7PSoC 4 Tricopter Part #7PSoC firmware: IMU, LED's & PID
8PSoC 4 Tricopter Part #8Hardware: PCB
9PSoC 4 Tricopter Part #9Hardware: tricopter's frame
10PSoC 4 Tricopter Part #10Hardware: YAW mechanics & motors
11PSoC 4 Tricopter Part #11Hardware: ESC's, wires & misc
12PSoC 4 Tricopter Part #12Final: The first fly

 

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Yuri,

     

    Great update, but you should have read my post on the PSOC.  One of the things I highlighted was its extreme versatility between various voltage levels.

     

    Other than that, it looks like you are making great progress.  I look forward to seeing it fly.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Yuri,

     

    Great update, but you should have read my post on the PSOC.  One of the things I highlighted was its extreme versatility between various voltage levels.

     

    Other than that, it looks like you are making great progress.  I look forward to seeing it fly.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to DAB

    Hello DAB.

    1. The design of this site is little strange for me and sometimes I can't find necessary information... Now I read your post, thanks!

    2. After I received the Pioneer Kit I tried to connect PSoC directly to 5v. But it is strongly warmed up and I was scared of fire! Now I know what the voltage is selectable by software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to DAB

    DAB, can you link to that post? Navigation is quite hard sometimes, so an extra link would be beneficial for those searching for PSOC voltage levels / 5V tolerant parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to vsluiter

    Hi Victor,

     

    Sadly, I am very web ignorant and have no idea on how to do that.

    Hopefully Dave or someone at Element 14 will do the deed for us.

     

    DAB4