Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog PSoC 4 Tricopter (Smarter Life Challenge) part #9
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yuritikhonov
  • Date Created: 21 Dec 2013 10:22 AM Date Created
  • Views 1190 views
  • Likes 1 like
  • Comments 2 comments
  • RoadTest
  • tricopter
  • psoc4
  • Multiwii
  • smarter_life_challenge
  • smarter_life
  • smart_tricopter
  • smart_control_and_diagnostics
  • arduino
  • quadcopter
Related
Recommended

PSoC 4 Tricopter (Smarter Life Challenge) part #9

yuritikhonov
yuritikhonov
21 Dec 2013

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

 

Good day comrades!

1. Let's start with the current situation on the construction of the tricopter's frame. In my case it consists of the following components:

  • aluminum square tubes: 15x15x600mm and 15x15x500mm;
  • two plates made of fiberglass;
  • landing legs made of wooden ruler;
  • M3 screws, M3 washers, M3 nuts;
  • plastic clamps.

 

Tricopter's features are already emerging:

image

image

 

Originally, I planned to use an Y-type design, but afer making the T-type I really liked it! The frame seems to be strong and light.

To help you understand it better, here is an example of Y-type tricopter, which inspired me to build:

image

reference to the original source.

 

2. During the construction of our apparatus I'd forgotten a very important thing: charger for LiPo batteries. As its basis, I took the following scheme: link. Ultimately, of the materials I had on hand I built such a device:

image

Note: 'HP zenner-diode' is an electronic unit, which volt-ampere characteristic is similar to the high power zenner-diode (HP = High Power). In my charger are used three blocks of this type.

 

3. Plans: next week I am going to build a YAW-mechanics. I have one "plastic gear analog 9g servo", I may use it as a sample.

Programming part is moving as well, this week I've corrected a little bit the file "output.c", after these changes, the servo started to work not only in theory but also in practice image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The next in turn before the installation of the BLDC, ESC, etc. will be only wiring and different small things. Unfortunately, the details from HobbyKing are still in transit image But the good news is that I have got now a track number to track the parcel!

See you next week!

                                                                                                                                              

#linkdescription
1PSoC 4 Tricopter Part #1Introduction
2PSoC 4 Tricopter Part #2Purchase of components from Farnell and HobbyKing
3PSoC 4 Tricopter Part #3PSoC firmware: upTime & Rx
4PSoC 4 Tricopter Part #4PSoC firmware: UART & MultiWii GUI
5PSoC 4 Tricopter Part #5PSoC firmware: EEPROM emulation
6PSoC 4 Tricopter Part #6PSoC firmware: Servo & ESC control
7PSoC 4 Tricopter Part #7PSoC firmware: IMU, LED's & PID
8PSoC 4 Tricopter Part #8Hardware: PCB
9PSoC 4 Tricopter Part #9Hardware: tricopter's frame
10PSoC 4 Tricopter Part #10Hardware: YAW mechanics & motors
11PSoC 4 Tricopter Part #11Hardware: ESC's, wires & misc
12PSoC 4 Tricopter Part #12Final: The first fly

 

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Yuri,

     

    The aluminum pieces look a little too heavy to me.  Plus your configuration will change the balance equations for a tricopter to stabilize the airframe.

     

    I will defer to your experience, and look forward to your first test flight.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to DAB

    Thanks for you comment DAB!

    1. I agree, these stuff looks a bit heavy, but in real it is lightweight! Such tubes are now very popular in quadcopter's and I think they are suitable for tricopter.

    2. About balance: the balance will be good, because in addition to the front, I have a heavy battery and YAW mechanics. Moreover, the motors are arranged at equal distances from each other.

    3. The total mass of the device will be 700-850 grams, so I have a field for experiments image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to DAB

    Thanks for you comment DAB!

    1. I agree, these stuff looks a bit heavy, but in real it is lightweight! Such tubes are now very popular in quadcopter's and I think they are suitable for tricopter.

    2. About balance: the balance will be good, because in addition to the front, I have a heavy battery and YAW mechanics. Moreover, the motors are arranged at equal distances from each other.

    3. The total mass of the device will be 700-850 grams, so I have a field for experiments image