Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog PSoC Challange "Smart reflow oven"
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Kilohercas
  • Date Created: 1 Nov 2013 10:02 AM Date Created
  • Views 2128 views
  • Likes 3 likes
  • Comments 15 comments
  • stm32f429i-disco
  • smps
  • pwm
  • uart
  • smarter_life
  • amoled
  • pid
  • reflow_oven
  • psoc
Related
Recommended

PSoC Challange "Smart reflow oven"

Kilohercas
Kilohercas
1 Nov 2013

Hello, i would like to present my Smart Life challenge idea.

 

I am thinking about making reflow oven. It will have 3.7 inch capacitive touchscreen with 800x480 AMOLED or SLCD screen for user interace as well as encoder for setting up time and temperatures of each reflow process steps. (maybe i will going to use unipolar stepper for this function, since it has very positive feedback, and very long life span )

 

 

PSoC4/5 will run control algorithms for heating, and so on. I will use two K type thermocouples for temperature measurement ( maybe one will be glued to small pcb with only copper and solder mask to get idea about this arrangement temperature, and also maybe second thermocouple will be glued to small FR4 board, to get idea about pcb temperature without any copper around.So i could guess temperature of pcb. It will get all commands for GUI controller ( for now i am thinking about STM32F429isince i need lot of power to drive large 800x480 screen and at the same time get information from touchscreen

 

And third large part will be SMPS for heating. Since i want to get precise temperature control, i will use PWM control for heaters.  I don't want to use SCR , or even relay, since it can produce high temperature fluctuations.

 

Ok so first job was to reverse engineer HTC desire screen. that take me some time, but i finally get it working, so now i can produce similar user experience as any high end smartphone can give for users. I will share code and pin-out, so others can try this out  ( as well as where to get connectors, since it nonstandard 10 pin 0,4mm pitch small size board to board  connector)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Still have many problems with AMOLED screen. It has not only RGB565 interface but also SPI interface for seting up screen, and at this time i don't know exact registers and data. but at least, i getit display something. This part will be hardest in this project

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Now comes easy part, making 2000-3000W PWM controller for heater. For now i am thinking about PWM controller driving high power IGBT transistor, and all data will come via Analog ISO digital I2C or simple isolator, since i don't want to have common ground that is directly connected to heater ground. So i will have to separate power supply, one for driver electronics, one for heater control electronics, simple .

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

YES, get AMOLED panel working with my user interface controller. That was very very hard, but result is superb. I guess that would be oven with best display in the market image
Only problem is that screen is 800x480, i will try to get resolution cut by half of each axis (240x400 would be tip top but i will have to add small fpga fr it, bummer )

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

wow, quality compared to other screens are just mind boggling

 

Fullscreen contentimage_45769.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

mini IR oven for my project. Its 800W and it has nice flat side for touchscreen mounting. Problem is, it will "just fit" with not much place around.

image

Also, all markings will be removed, and if all goes well, i have access to laser engraver for some custom markings ( in university we have laser marking machine ). Biggest problem is that i have very little room for my PWM controller, 12v power supply and my driver. I bet i have to integrate all electronics on single pcb and also send it to OHS Park for manufacturing, so not much time to spear image

 

Heater power control

 

As you might know,i will use PWM control, so i can adjust heating power , and by doing that i should get better temperature control ( low temperature "ringing" with flat temperature profile )

Idea is this. PSoC 5 will generate PWM signal by measuring temperature from sensors, and adjusting pulse width according to PID controller state. Set point will be controlled by STM32F429 via UART. At start-up, PSoC will check if driver has ULVO, if yes, displays error, since i can't run power mosfet with gate voltage below 10V. Temperature fault will not be used, since i have 100mOhms MOSFET and rms current is just 5A, that is very little of heat. ( maybe i will add more heaters to get faster heating curve, but for now original heaters will work just fine.

 

Simple schematic:

image

 

User interface

image

Hrr, is is very hard to make nice looking front panel. I have no room for any mountings, also very little room for AMOLED itself.
Plan is to use FR4 sheets, cut it with cnc, and glue them . For now it's my only option

 

If some one still has a question, do i really need stm32f429i, here is the answer : (still, it's only for basic functions, more pins will be used in this design )

 

image

 

 

 

 

 

 

 

 

 

Still lot of work to be done.

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Hello Linas,

    Wouldn't it be possible to drive the display with the PSOC4 / PSOC5? I mean, the other task (temperature control) is so slow that you can probably just do it on interrupt / DMA basis so your display updates will hardly suffer. I'm not at home in display control, but I can't see yet why you would need a very powerful processor; frame rate only needs to be 20Hz, if not lower....

    Please convince me image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago

    Hello Linas,

    Wouldn't it be possible to drive the display with the PSOC4 / PSOC5? I mean, the other task (temperature control) is so slow that you can probably just do it on interrupt / DMA basis so your display updates will hardly suffer. I'm not at home in display control, but I can't see yet why you would need a very powerful processor; frame rate only needs to be 20Hz, if not lower....

    Please convince me image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Kilohercas
    Kilohercas over 12 years ago in reply to vsluiter

    well, when i need to get LCD controller, S1D13517 should do the job. But here is the thing, it cost nearly the same as STM32F429, and i need 16b high speed interface. More to that i need on-board memory for graphics. That is ok, i could use SPI flash, but again, problems to load files for spi. STM32F429 has 2MB flash, memory controllers  and even i2c for touchscreen. So i can run Segger UI with RTOS or write my own UI

     

    So in short, i can use only PSoC for this task, it will be very slow, and will  i spend more time to get it working again with new controller. What would be waste of time, and will cost much more i guess .
    Note that screen takes up to 750KB for frame, (5.9Mbit) . so i have to do some clever programing on new platform, and i just don't see it working as i want to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to Kilohercas

    Very good, you convinced me image that it's a sh..load of work to get going from the PSOC, and indeed, you don't have much time. Wouldh have been nice though...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to vsluiter

    I don't like idea that i use other part for this project. I could do simple reflow oven, with 16x2 character by using only Cypress parts without any problem ( i would use PSoC 5 ), but it's not a challenge then. This project is not cost orientated, it's more lets do what i wanted to do and see how it turns out.

    This would be the first oven capable of running precision temperature control for cooking, and at the same time fractal calculation on screen ( Mandelbrot or Julia series )

     

    And where is no question if i going to use 800x480 AMOLED screen, i have to use high end mcu. In other forum ( my.ST.com ) i get lot of pounding that my STM32F429i is too weak for large AMOLED panel like mine, i should switch to Arm Cortex A8/9/15 for that.