Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Smart Life Challenge: geoCar PSoC meets Android sample
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: camuyano
  • Date Created: 20 Nov 2013 2:27 AM Date Created
  • Views 930 views
  • Likes 1 like
  • Comments 3 comments
  • android
  • bluetooth
  • psoc4
  • smarter_life_challenge
  • gecar
  • smarter_life
  • psoc
Related
Recommended

Smart Life Challenge: geoCar PSoC meets Android sample

camuyano
camuyano
20 Nov 2013

A few posts ago I posted about the bluetooth and the PSoC and was asked to post some code for it. So here it is some sample code to write from Android via Bluetooth to the PSoC. This is nothing close to what my project be but it is a test of the different components and others might found it useful so why not share it.

 

Hardware

PSoC Pioneer Kit

Bluetooth to Serial TTL adapter (cheap adapter close to $10 ebay/amazon .... )

 

Software

PWM

UART

Android application (https://github.com/soynerdito/AndroidPSoCBluetooth)

 

Overview

I copied the PWM from the PSoC capacitance sample. Then added an UART control with 9600 baud rate. Wrote a simple Android app to send a character via Bluetooth.

The bluetooth device is called "linvor" with passcode 1234. If you use a different one, may need to change the code to use the one you needed. Before using the app the bluetooth device should be paired with the phone (the same way you pair a headset) with it's corresponding pin code. The app will try to connect to an already paired device named linvor, please note that this is a simple sample code without any error checking. Original code gotten from the android developer site sample and modified a little bit.

On the PSoC when receiving a character (integer value) I did the exact same thing as the demo (shift the bits) and write to the PWM control. I control the range of the values like the example, from 1 to 127 (I skipped the 0).

image

image

It is pretty straight forward. On the demo the PWM is written when an interrupt is generated, here is when a character from 1 to 127 arrives.

image

 

Testing the app with the PSoC

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
BlueSoc.zip
  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Good demo.

     

    It looks like the Bluetooth HW and SW worked well.

    Did you encounter any unexpected issues when you put the two together?

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • camuyano
    camuyano over 12 years ago in reply to DAB

    Actually no. It is scary easy on how to use the UART on the PSoC. The code of the PWM is not something that I understand very well, but it was just as easy as taking the code from the interrupt of the Cap demo out and then set it up on the receiving of the character that comes from the UART interface. On the android it was just getting the correct documentation from the Android site.

    I hope somebody sees this and help'em achieve what ever he/she wants.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • camuyano
    camuyano over 12 years ago in reply to DAB

    Actually no. It is scary easy on how to use the UART on the PSoC. The code of the PWM is not something that I understand very well, but it was just as easy as taking the code from the interrupt of the Cap demo out and then set it up on the receiving of the character that comes from the UART interface. On the android it was just getting the correct documentation from the Android site.

    I hope somebody sees this and help'em achieve what ever he/she wants.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vsluiter
    vsluiter over 12 years ago in reply to camuyano

    Nice demo. Simple and effective.

    It's always impressive when paired with a smart phone. Just like a few years ago when the first 'tinkerer' devices started to feature USB. Makes you feel grown up image