Browse By Tags

  • Can Someone Review my Schematic for Android GPIO?

    Okay, so I want to access Arduino GPIO pins via Android. My plan is to access them via a serial connection using an MCP2200. I can read / write to the serial port on Android, which can then interact with the Arduino. The problem is I also want to be…
  • Is it possible to access GPIO on Android?

    I'm designing my next project, and was wondering if it's possible to access GPIO on an Android tablet. I know you can do this on a PC using a breakout board like the Adafruit FT232H. Is there something similar I can use with an Android tablet?
  • U-boot booting error: "Error" handler, esr 0xbf000002

    Hi Everyone, I am working on u boot configuration for the maaxboard (imx8mq) to port to Android. So, I built u boot successfully with maaxboard_defconfig with some additional configs however, I am getting this error, any one has any idea? here is…
  • fsl_avbkey.c:314: undefined reference to `blob_decap' | Porting u-boot-imx to android 13

    I am trying to port u-boot from origin/maaxboard_lf-5.15.71-2.2.0' to Android 13. So I am comparing all the files here and in the uboot-imx for imx8mq-evk board and if something is missing or different, creating a new file considering maaxboard configs…
  • Android - System crash and reboot when wifi connection is established

    Hi there. I am trying to figure out a wifi issue on Android which causes the system to be crashed and rebooted. When I have a wifi connection or even search for available networks, suddenly the system is restarted due to some reason. Is there anyone who…
  • Arduino with GSM sends data to Phone App

    Hello, community of element14, Long time since I last been here and I need your help once more. Am working on a project (a DIY remote control system for cars) using a phone app (not everyone can buy a new car with these cool features) :). This comes…
  • Using an Android logic board to connect to display

    I am wanting to prototype a system that uses an existing logic board like from a Samsung or another Android, and connect that to a 3rd party flexible AMOLED display. I'm curious on the engineering side of this, cause I can get the system running on a…
  • Hacking a Hotel POS Tablet - How Hard Can it Be? -- Episode 556

    You don't have permission to edit metadata of this video. Edit media Dimensions x Small Medium Large Custom Subject (required) Brief Description…
  • Tablet / ChromeBook / laptop for tech hobby?

    Hi all, I’m thinking of getting a new tablet so that I’m not tied to my desk for hobby type projects. I have a Mac as my main computer that I can use when I really need power and screen size, but for hobby things I’d rather work from the couch or table…
  • Smart Air Quality Monitor #6 - Wireless Air Quality Monitor - CY8CKIT-062S2-43012 Plus ZMOD4510 - The Outdoor Test

    My new findings on ZMOD4510 Air Quality Sensor ZMOD4510 Air Quality Sensor is focused on the outdoor air quality measurement based on ozone and NOx concentration. Ozone concentration indoor is very low. I was able to detect it after a long period of time…
  • RIoTboard: Developing for Android with Python (Kivy) and Java

    I recently got my hands on a new RIoTboard and wanted to start developing on it as soon as I could. The first thing I did was check if any guides existed, and sure enough there was this guide from element14 . However, it uses Windows and I am primarily…
  • How to Install Netflix Streaming on the RIoTBoard

    Fullscreen contentimage_30363.html Download <html><head><title>Jive SBS</title></head> <body><font face="arial,helvetica,sans-serif"> <b>Error</b><br><font size="-1"> An general error occurred while processing your request. </font></font></body…
  • Open Source EMDR Machine #11. An update on Software Application

    Open Source EMDR Machine. The Whole Blog. Where to get it The Workflow. A Short Tutorial The First Screen The Second Screen The Third Screen An update on Software Application Where to get it Update: I…