Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Smart solder reflow oven exterior
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Kilohercas
  • Date Created: 30 Jan 2014 4:05 PM Date Created
  • Views 2419 views
  • Likes 1 like
  • Comments 10 comments
  • smarter_life
  • reflow_oven
Related
Recommended

Smart solder reflow oven exterior

Kilohercas
Kilohercas
30 Jan 2014

2 days work on exterior and today i can say, it turns out better than i expected . Now only UI programming is left, RTC, PID,PWM are working and i can do reflow soldering even today, but i need to make clean UI.

Still don't know how can this project be completely ignored by in this contest, but where is other contest on STM32F429 that needs to explore DMA2D peripheral and what is exactly what i need for my user interface, alpha blending for 2 temperature graphics, also transparency for on screen keyboard and so on.( but i am running low on SRAM, so it could be a challenge )

image

Attachments:
image
  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Linus,

     

    Good looking build.

    You should be able to make a nice usable UI with the tools you have.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to DAB

    intel inside, idiot outside , so no, it will take lot of time to do that. and i am not good at programming

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Kilohercas
    Kilohercas over 12 years ago in reply to DAB

    intel inside, idiot outside , so no, it will take lot of time to do that. and i am not good at programming

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 12 years ago in reply to Kilohercas

    We learn by doing.

    Look upon it as an opportunity to explore new territory.

    Sit down and plan out what you want to do and define a control sequence that is simple and easy to follow.

    Then you just draft out the command/control structure and identify the information you need at each step.

    That way you can keep the flow simple and easy to program.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to DAB

    problem is not that i don't know how to program, problem is i am low on resources. Now look, it is easy to make mathlab program, calculate matrix multiplication and so on. but it consumes lot of memorycare, i can make 6GB dynamic array on my notebook, without any problem . Because i have huge screen, (800x480) i need lot of resources to make it work,since only DMA send around 0.786MB/frame at 60FPS. At the same time i have to change GRAM buffer data, that cause tearing and all other visual problems. Not only that i have problems with flash loader, half of STM32F429 memory is damaged somehow... so only uploading 400x400 picture will cause flash loader crash image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to Kilohercas

    Hi Linus,

     

    Think about using sprites.  They are very low on memory use and you can set them up with counters to paint them at the right location on the screen.

    Good resolution displays are both a blessing and a curse.  I used an 8085 to drive a 400 by 400 pixel display back in the early 1980's.  We used a memory board with one bit display resolution for each pixel and then just dumped the array to the display.  Crude but it worked for real time updates.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to DAB

    i don't know how to do gradient fillings , and also color mapping by only using c code. It would be easy to make it look like window 98, but i am going for windows 8 look if you know what i mean

    right now i have concerns about:
    making temperature graph that looks good, and still is informative, not just plain line, but something more, like blend two graphs from T1 and T2 with color map by suing alpha blending.

    Second how to write keyboard application that can return data in right format, and jump between windows (text box). I am also have problems with double interrupts, like how to understand that i pressed button only one time, and not 20.

     

    Third, graphical layout of all settings, check boxes, and so on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to Kilohercas

    Hi Linus,

     

    Have you used the de-bounce capability of the PSOC?

    Its a quick way to isolate a single touch and ignore multiple detection interrupts.

    I am not sure which display functions are supported by the PSOC.  I used to do brute force pixel drawing for my project many years ago.  Hopefully you have better software tools to do this than I did.

     

    Unless you have a good visual graphic support, you can always do a paper layout and count pixels for your layout.

    I am hoping you have access to some drawing tools to simplify the task.

     

    DAB