Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Forum Any ideas on how to count pulses and shut off a PWM
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 1 answer
  • Subscribers 8 subscribers
  • Views 7837 views
  • Users 0 members are here
  • timers
  • pwm
  • counter
  • smarter_life
  • psoc
Related

Any ideas on how to count pulses and shut off a PWM

PaulMakesThings
PaulMakesThings over 12 years ago

TL;DR version: How do I count pulses with programmable digital and use the count to shut off 5 PWMs. The count to shut off and the frequency of the PWMs would have to be set in software for each iteration.

 

I'm trying to figure out a good way to use programmable digital of the PSoC 4 on the pioneer kit to do coordinated stepper moves. Setting up a PWM module was pretty easy, I just need something to shut it off after a set number of pulses. The black box description is this, the software sets the pulse frequency for several modules, 5 in this case, with the timing already calculated so that they will finish their pulses in the same amount of time, then it starts them at the same time, then they all shut off when they're done and signal (probably via interrupt) back to the software that the move is done and they are ready for the next. I'm thinking the architecture would use one PWM module as the master, if there are not timing glitches they would all finish together, it would stop them, and interrupt that the move was done.

 

So far I have found that I can easily set a PWM module for a certain frequency from the software, but I'm not sure how to make a counter shut it off. The algorithm is pretty simple for these moves, you have a known speed in pulses at which each axis can move given the electrical and mechanical limitations of the system, given the number of steps required for a move on each axis and that speed you can find which one will take the longest, and divide the number of pulses for all the others to make them happen in that amount of time. At that point most controllers just use timers to generate and count those pulses, I'd like to figure out a nice efficient way to do it in programmable digital. I think it should be pretty simple if I can just figure out how to count pulses with a counter, then I would have it trigger an interrupt and stop the PWMs when the target is reached, can someone show me how to do that? I'd also be interested in other hardware architectures that can do this.

 

As a note, this is for the smarter life challenge, I'm not really worrying about my competitors seeing my code. If I win I want it to be by making the coolest project, not because they got stuck.

 

Thanks for reading

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +2 verified
    My solution was to use a lower frequency clock to drive a PWM(acting as a counter) just to generate a time-base during which the other 4 PWMs could generate the required number of pulses. We then use a…
  • DAB
    DAB over 12 years ago +1
    Hi Paul, I believe that you can set up counters and status registers inside the PSOC. I think that you can turn the PWM outputs on and off by using a status/control register from the software side. Inside…
Parents
  • PaulMakesThings
    0 PaulMakesThings over 12 years ago

    I'm going to finish the project for the contest this way, but a interesting idea occurred to me. It seems like feedback servo control could also be done in hardware, the encoder can be read by a decoder or a counter and that can be fed into a comparison. I haven't worked out the details, but it has potential. I'm not just talking about basic potentiometer feedback servos like an RC car, but high speed precision ones like you would use in an industrial robot, the kind with 1024 or more counts per rev. I wonder how fast you could go, the ones we buy at my job usually cost about $700 because they can update the torque command at 4 MHz. It almost seems like a PSoC could do that, though getting the curve just right would be tricky and of course it would still need the power amplification stage. It can't handle 10A to 50A, but then you can't blame them for that, some good size high frequency Mosfets in an H-bridge could take care of it. Just food for thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to PaulMakesThings

    Hi Paul,

    We've used the incremental encoders from Pololu for a student's project, they were quite OK, but sometimes we lost track (encoder error, or missed pulses? i don't know...).

    There are a lot of nice and cheap magnetic encoders, for example by Agilent, or RLS or ic-haus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago in reply to PaulMakesThings

    Hi Paul,

    We've used the incremental encoders from Pololu for a student's project, they were quite OK, but sometimes we lost track (encoder error, or missed pulses? i don't know...).

    There are a lot of nice and cheap magnetic encoders, for example by Agilent, or RLS or ic-haus.