Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Documents PSoC4 Smarter Life Challenge - DAS Project :Example 3 LED Dimming (PWM based)
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: bose
  • Date Created: 4 Nov 2013 12:31 PM Date Created
  • Last Updated Last Updated: 17 Dec 2014 3:55 AM
  • Views 655 views
  • Likes 2 likes
  • Comments 1 comment
Related
Recommended

PSoC4 Smarter Life Challenge - DAS Project :Example 3 LED Dimming (PWM based)

This example show how to perform LED dimming using PWM module for Cypress PSoC 4 Pioneer Kit.

 

Here is the Application Schematics:

image

image

This example uses the PWM block in a timed configuration to produce the dimming effect on the LED.

 

The PWM module { PWM (TCPWM mode) [v1.0] }configuration is as shown below:

image

In the code one needs to vary the Compare factor for the PWM to generate a DC average output that would lead to dimming of the led.

Ideally a capacitor is needed to produce the DC averge but since the LED load is not significant, its possible to directly generate the dimming on the pin connected LED.

Here is the code for this example:

#include <project.h>
int main()
{
     uint32 i = 0; //Used as a Counter
     uint32 op = 0; //Used to define which operation is being currently performed : 0-additions 1-subtractions
     // Start the PWM generation
     PWM_1_Start();
     for(;;)
     {
          CyDelay(5); //Cycle Delay
          // Process the Counter Operation
          if(op == 0)
               i += 10;       
          else
               i -= 10;
          // Change the PWM duty cycle value as per the Counter
          PWM_1_WriteCompare(i);
          // Handle Counter overflow
          if(i>=1000)
          {
               op = 1; // Start Decrementing as max value has already reached
          }
          else if(i<=1)
          {
               op = 0; // Start Incrementing as Min value has already reached
               CyDelay(800); // Delay to keep the LED off for more time
          }
     }
}

 

After building and loading this code the Green LED on the Pioneer Kit would show the dimming effect.

Its important to note here that this dimming would show up some visible blink and may also cause EMI/EMC or RFI issues in case the output is used to control LED drivers.

The better solution would be use the PrISM module to generate precise dimming without flicker or emission issues.

  • psoc4
  • examples
  • smarter
  • das_project
  • smarter_life
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • mcb1
    mcb1 over 11 years ago

    Nice clear instruction.

     

    Thanks for adding it. (not sure how i missed it earlier)

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    Nice clear instruction.

     

    Thanks for adding it. (not sure how i missed it earlier)

    Mark