Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Blog Part4.1 - ADT7320 Temperature Sensor [Central Hub]
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
  • Author Author: sunnyiut
  • Date Created: 7 May 2015 12:05 PM Date Created
  • Views 1108 views
  • Likes 2 likes
  • Comments 1 comment
  • sudden_impact
  • adt7320
  • total_player
Related
Recommended

Part4.1 - ADT7320 Temperature Sensor [Central Hub]

sunnyiut
sunnyiut
7 May 2015

Title: Total Player Monitoring

By: Md. Kamrul Hussain

Project Category: Design Challenge

Project Name: Sudden Impact Wearables Design Challenge

Blog post: 09

 

Intro:

It's an update on the temperature sensor ADT7320. It's a part of the module 04 [central hub]. This sensor will be placed on the back of the wrist and will be mounted along with the central hub. In this blog post I'll demonstrate the outputs of the sensor with different configuration and simulate a visual indication of crossing the temperature limits.

But before that I would like to recall my proposal on the basic structure of the 'central hub' and the other modules belong to it.

 

Central Hub:

According to my proposal, the central hub will communicate with all the modules through Bluetooth and it will maintain a long range communication bridge [Using BlueGiga WT41] with the remote device held by the trainer. The hub itself will accommodate a few other modules and will be placed on the back of the wrist.

image

Sub-modules:

  • Temperature Sensor
  • Impedance measurement for detecting Dehydration
  • Photoplethysmograph for SPO2

 

proposed model for mounting the module 04 hardware in a wrist band ->

image


Today I am presenting the first part of this module -> Temperature Sensor. I have done some hardware work and preliminary design of other two parts. But none of them are completed yet. However, I'll carry on according to my plan step by step, but shall try to post updates on the other two parts [impedance and plethysmograph] within the deadline of the submission. So, that I'll be able to give a generous idea of how much work has been done or partially done by me so far.

 

ADT7320 Temperature Sensor:


Range -> -20'C to 105'C at 3.3vimage

Resolution -> 0.0078'C at 16bit

Communication -> SPI mode3

Benefits ->

          • different mode selection for lower power operation
          • wide operating range
          • easy implementation as no calibration is needed
          • hardware capability of generating interrupts

 

Protocol structure:


ADT7320 operates in Mode3, where the idle state = clk high and data sampled at active to inactive [low to high rising] state.imageimage

ADT7320 has both 8bit and 16 bit reading and writing structure depending on the size of the target register. But for every read or write operation, 8-bit command byte has to be written at first.

I have shown the writing and reading structure from the datasheet at the end of the blog.

 

Configuration:


I have experimented with both the 13-bit and 16-bit data structure with continuous and 1SPS operating mode and also changed the temperature limits from default value to get the desired interrupts. Finally I have chosen the following configuration for my design ->

  • resolution -> both 13 and 16-bit depending on the demand
  • fault queue -> 4 consecutive faults to generate an interrupt
  • operation mode -> 1SPS, one sample per second to save the power. It takes only 46uA at 3.3v for 60msec and stays at stand by for 940msec. The captured data can be read any time  from the buffer even in stand by mode. So, it saves a lot of power consumption as the body temperature does not change at once suddenly and we don't need the continuous data conversion.
  • interrupts -> just for demonstration purpose
        • critical value = 34'C
        • high limit = 33'C
        • low limit = 32'C

 

Calculation of Temperature:

image

image

Steps:

image

 


Hardware:


I am using Mikromedia board for demonstration. Unlike previous cases, this time I am going to use the dsPIC33EP microcontroller of Mikromedia board for this module. Because, I have other sub-modules like impedance measurement and plethysmograph, where the DSP will be needed to process the signals.

 

Step 01 - Reset:


After powering up the first step is to reset the SPI interface and reset all the register contents which ensures that the sensor is ready for stable performance.

To do that logic high [1] has been sent into DIN line of the sensor for 32 times.

 

         device setup                                                                                               reset ADT7320

imageimage

 

Step 02 - Read Configuration:


After resetting the sensor it's better to read the configuration  to see whether the operation mode is in expected form.image

 

First to check the device ID.

      

command byte frame for reading the device id :  

 

01011000             ->            0x58 hex

 

C7

C6

C5

C4

C3

C2

C1

C1

0

R/*W

Register address

0

0

0

0

1

0

1

1

0

0

0

 

IDT7320 responded with 195 = 0xC3 hex, which was expected.

 

 

 

  image

Then the 'Configuration' register gives the operation mode for ADT7320.

 

command byte frame for reading the configuration :

 

01001000             ->            0x48 hex

 

C7

C6

C5

C4

C3

C2

C1

C1

0

R/W

Register address

0

0

0

0

1

0

0

1

0

0

0

 

The ADT3720 was running in default mode with 'continuous' data conversion at 13-bit resolution.

The Fault Queue was single fault to generate interrupt.

image

 

 

 

image

 

After that, the Temperature limits for interrupt generation were verified.

 

command byte for reading the interrupts :

 

T(critical) = 0x60 hex

 

T(high) = 0x 70 hex

 

T(low) = 0x78 hex

 

IDT3720 gave the default value of 147'C, 64'C and 10'C respectively

 

The right side image represents an example of reading temperature at default operating mode.

 

 

Step 03 - Set Configuration:


By reading the configuration I came to know that the sensor is running in 'Continuous' mode with 13-bit resolution. Now as I want to use the sensor in 16-bit 1sample per second for more precise output and less power consumption, I need to change the configuration register. I would like to change the temperature interrupt limits as well for demonstration purpose.

image

 

frames for new configuration register ->

     command byte  =  00001000 = 0x08 hex

C7

C6

C5

C4

C3

C2

C1

C1

0

R/W

Register address

0

0

0

0

0

0

0

1

0

0

0

 

     write to configuration register = 11000011 = 0xC3 hex

C7

C6

C5

C4

C3

C2

C1

C1

1

1

0

0

0

0

1

1

 

For Interrupts ->               command byte                    register value to write            value

 

T(critical)                               0x20 hex                              0x1100 hex                    34'C

T(high)                                   0x30 hex                              0x1080  hex                   33'C

T(low)                                    0x38 hex                              0x1000  hex                   32'C

 

 

 

 

Step 04 - Read Temperature:

 

frames for reading temperature ->

     command byte  =  01010000 = 0x50 hex

C7

C6

C5

C4

C3

C2

C1

C1

0

R/W

Register address

0

0

0

0

1

0

1

0

0

0

0

 

Outputs at different temperatures:

 

For demonstration purpose I have used a very small range of temperature limits.

 

Normal Temperature [32 -33 'C] ->     The thermometer ICON stays green to indicate normal temperature.

imageimage

 

Low Temperature [ < 32 'C] ->     The thermometer ICON becomes blue to indicate low temperature.

imageimage

 

High Temperature [ 33 - 34 'C] -> The thermometer ICON becomes orange to indicate higher temperature.

imageimage

 

Critically High Temperature [ > 34 'C ] ->      The thermometer ICON becomes red.

imageimage

So, this is the Temperature Sensor part of Module 04 - central hub. On my next blog I'll post about 'Detection of Dehydration using Impedance Measurement' [partial work - whatever I have done so far].

 

**these are the writing and reading structure of IDT7320 SPI protocol for both 8 and 16 bits taken from the datasheet.

Writing structure ->

                                                       8 bit

image

                                                       16 bit

image

Reading Structure ->

                                                          8 bit

image

                                                            16 bit

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Nice detailed post. Providing the formats and timing details is a nice touch. I like how you track the raw data and the calculated result. Access to raw data is essential in verifying the system operation…
Parents
  • DAB
    DAB over 11 years ago

    Nice detailed post.

     

    Providing the formats and timing details is a nice touch.

     

    I like how you track the raw data and the calculated result.  Access to raw data is essential in verifying the system operation.  The raw data also allows you to hand check the calculations as well.

     

    Good job,

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Nice detailed post.

     

    Providing the formats and timing details is a nice touch.

     

    I like how you track the raw data and the calculated result.  Access to raw data is essential in verifying the system operation.  The raw data also allows you to hand check the calculations as well.

     

    Good job,

    DAB