Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Blog Pictures from evaluation
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
  • Author Author: e14 Contributor
  • Date Created: 26 Jun 2015 10:45 PM Date Created
  • Views 1342 views
  • Likes 3 likes
  • Comments 4 comments
Related
Recommended

Pictures from evaluation

e14 Contributor
e14 Contributor
26 Jun 2015

Dear all,

 

here are a few pictures from the evaluation so far. The boxes had all arrived at Leeds Beckett University by 17 June 2015.

 

image

 

Now the opening could start.

Here are a few "inhabitants" of the Biomechanics Lab in the School of Sports of the Carnegie Faculty at Leeds Beckett University:

image

 

The evaluation team, the film team, and the still unopened boxes:

image

 

Julian Old is opening the boxes with Cosmin's device:

image

 

Athanassios Bissas shows Ravi's device:

image

 

Here Joanne Hudson is showing Austin's device:

image

 

Mike Gray shows Douglas' helmet mount device:

image

 

Here is Hendrik's device being charged:

image


Charging Dragan's device:


image



And the testing continues...

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to DAB +3
    Hi, we will publish the evaluation criteria together with the results. No point in giving them out earlier, as the devices and the software are now here and are not being modified. The main criteria have…
  • mcb1
    mcb1 over 11 years ago +1
    Looks like the poor fella on the left in the second picture could have used one a bit earlier ... Nice to see the opening of the packages. Mark
Parents
  • mcb1
    mcb1 over 11 years ago

    Looks like the poor fella on the left in the second picture could have used one a bit earlier ...

     

    Nice to see the opening of the packages.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    Looks like the poor fella on the left in the second picture could have used one a bit earlier ...

     

    Nice to see the opening of the packages.

     

    Mark