Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Blog SFH: Week 6 - First looks at the app
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
  • Author Author: hawkeyethehacker
  • Date Created: 1 Feb 2015 11:48 AM Date Created
  • Views 562 views
  • Likes 0 likes
  • Comments 2 comments
  • safe_field_hockey
  • sudden_impact
Related
Recommended

SFH: Week 6 - First looks at the app

hawkeyethehacker
hawkeyethehacker
1 Feb 2015

Yes, it says Week 6, no, we did not time travel - I am just making up for some missed updates.

 

We have hit another roadblock - my Velleman K8200 does not work, so no more printed enclosure.

Anyway, while we wait for some of the last parts to arrive, I have been working like mad on the app for SFH. I finally have something to show you.

imageimage

I am aware that the app is only laid out to support one uniform node - I plan to implement multiple nodes later.

Note the values on the "Overview" sceenshot. These are not hardcoded into the app - but are actually being read from the SFH server as the final version would.

Of course, the server has to get those values from somewhere, which is a JSON file that in the final version will be constantly updated with each node's values.

 

The source code for both the Server and Client is available at https://github.com/element14-SFH.

 

Any suggestions as to what you would like to see in the app? Comment away!

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    So this is the ... Tesco Shoppers frenzy sudden impact by cart detector Having seen the rushes in Tesco sometimes, I can understand why it would be needed along with padding and special bumpers on the…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    So this is the ...

     

    Tesco Shoppers frenzy sudden impact by cart detector image

     

    Having seen the rushes in Tesco sometimes, I can understand why it would be needed along with padding and special bumpers on the carts, its a dangerous place at rush hour, especially near the jamy dodgers

     

    But on a more serious note, looks like a nice UI, I did not know Tesco was in the phone business (Hense the joke image )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 11 years ago in reply to Robert Peter Oakes

    Yes, it is a fully integrated system that will push updates to "Scan as you Shop", which then communicates with a base station that can call first aid staff when necessary. It has saved many lives over the years, and the number of jammy dodgers being thrown away has decreased dramatically in a study performed by the "Jammy Dodger Damage Prevention Society (JDDPS).

     

    --

     

    In all seriousness, thank you - and yes, they are, but it's more of a piggyback on O2 image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hawkeyethehacker
    hawkeyethehacker over 11 years ago in reply to Robert Peter Oakes

    Yes, it is a fully integrated system that will push updates to "Scan as you Shop", which then communicates with a base station that can call first aid staff when necessary. It has saved many lives over the years, and the number of jammy dodgers being thrown away has decreased dramatically in a study performed by the "Jammy Dodger Damage Prevention Society (JDDPS).

     

    --

     

    In all seriousness, thank you - and yes, they are, but it's more of a piggyback on O2 image