Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Blog Wearable Sudden Impact and Health Monitor - Update 8
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
  • Author Author: ciorga
  • Date Created: 23 Mar 2015 4:00 AM Date Created
  • Views 814 views
  • Likes 1 like
  • Comments 4 comments
  • sudden_impact
  • wearable_sudden
Related
Recommended

Wearable Sudden Impact and Health Monitor - Update 8

ciorga
ciorga
23 Mar 2015

Hello Everyone, this is another update on my "Wearable Sudden Impact and Health Monitor" project.

 

In my previous update I showed how I connected the Analog Devices EVAL-ADXL375Z module to an Arduino nano and how I measured a physical impact using a small app that I wrote in Android Studio.  This app received the acceleration x, y, and z axis recordings of the ADXL375 accelerometer and it converts them into G units and displays them the screen.

 

Interestingly, as it has been mentioned by hlipka in the comments, my measured values exceeded the ADXL375 spec of maximum 200g.  So I have spent some time to verify how I converted the raw data into g units, and I came to the conclusion that my calculations are correct.  So I came to the hypothesis that maybe my ADXL-375 measures more than 200g.  To test my hypothesis I plugged in the other evaluation kit for ADXL-375 that I have, EVAL-ADXL3745Z-M, which runs trough a GUI provided by Analog Devices, so I exclude any potential calculation errors that I could make.  Also, this kit uses a different ADXL-375 sensor chip than I used in my previous experiments.  Here is a picture of that setup:

 

image

 

On this experimental setup I then applied the same impact force that I applied on my previous experiment.  I then looked at the impact recording on the GUI and indeed it looks like the measured value exceeds the maximum range of 200g on the y-axix of the GUI graph.  Here is a screenshot of this measurement.

 

image

I then looked at the datasheet; here is a screenshot of the section describing the maximum range:

 

image

So the typical range is +/-200g, there is a minimum range shown there of +/-180g, but there is no maximum range value, so the specifications allow the possibility that the ADXL-375 sensor may be able to measure accelerations larger then 200g.

 

After clarifying that I did not make any error in converting the measured data into g values, I continued with improving my Android app by adding a graph that will display the real time ECG measurement.   This was not an easy task, so I spend quite a significant time to get it to work.  Here is a picture of the app running on my phone, which has the graph displayed at the bottom.

 

image

And here is a video (I don’t know why the resolution is so bad; I need to look for a different camera for future videos).  The video shows a square wave signal plotted on the graph, since so far I haven’t connected yet the AD8232 ECG eval kit.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is where I got so far with my wearable impact and health monitor system.  I will come back with other updates as I get more work done.

 

 

Best Wishes,

Cosmin

  • Sign in to reply
Parents
  • clem57
    clem57 over 11 years ago

    Sometimes the software does not improve as fast as the hardware will! Good Jobciorga

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago

    Sometimes the software does not improve as fast as the hardware will! Good Jobciorga

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ciorga
    ciorga over 11 years ago in reply to clem57

    Thank you for the comment Clem; yes, I agree with you.

    Cosmin