Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Blog #10 - The Final Push
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
  • Author Author: dang74
  • Date Created: 6 Oct 2020 2:29 AM Date Created
  • Views 1732 views
  • Likes 7 likes
  • Comments 9 comments
Related
Recommended

Blog #10 - The Final Push

dang74
dang74
6 Oct 2020

Wow, where did all the time go.  It seemed to evaporate.  I tried to stay disciplined with my time management but sometimes life gets in the way.

 

I woke up on Saturday morning with the realization that a whole lot of work still needed to be done.

 

After my coffee I crouched over my kitchen table to solder the remaining components on the carrier board.

 

image

 

 

The first module installed on the carrier was the PROFET 2+ Shield.

image

 

 

Then I installed the DPS368 Pressure2Go module.  He's a cute little guy... smaller than a stick of gum.

image

 

 

And finally, on top of the stack, we have the XMC4700 Relax Kit board.

Wow, I was so impressed with how everything looked together.

image

 

 

So although I was very pleased with the electronic integration there was some disappointment ahead.

 

I was completely defeated by the plumbing. LOL.

 

This is one area that I totally underestimated.  I had a lot of difficulty sourcing the appropriate adapters and plumbing fixtures so I used rubber tubing to attach the solenoid valve.

Unfortunately the smallest amount of pressure would cause the rubber tubing to fail, in turn sending the solenoid into the puddle that was quickly forming in my garden.

 

Things weren't looking too safe so I had to abandon this goal.  For the sake of posterity I've included an image capturing this failed attempt.

 

Please do not try at home:

image

 

I had greater success with the data logging function.  On Sunday night, I 'left the Relax Kit to its own devices'.

After 3 hours or so I checked to see what data was logged.  The results are shown below:

image

 

So, yeah, its kind of cool that it can run autonomously, record data and make decisions based on that data.

And once I befriend a qualified plumber I have no doubt that it will be able to control a water valve. image

 

For the time being my project sits on my TV stand.  He runs autonomously collecting data.

image

 

 

And he's in good company too, being watched over by two of the best friends I ever had.

 

I want to thank Newark Element14 and Infineon for putting together this design challenge.  It provided a good introduction to technologies I wasn't too familiar with like ARM Cortex M4, the XMC series of microcontrollers and the DAVE IDE.  More importantly though, it provided that rare opportunity in life, where you are challenged and given an opportunity to solve problems in creative ways.  For this I am truly grateful.

  • Sign in to reply

Top Comments

  • dang74
    dang74 over 6 years ago in reply to jw0752 +1
    Thanks for the kind words as well as the advice. Once water started spraying on the wires and the valve kept falling into the puddle I kind of lost my nerve.
  • ralphjy
    ralphjy over 5 years ago +1
    I did a similar project a few years ago and used a similar solenoid valve from Adafruit that has 1/2" pipe fittings. The Sparkfun solenoid says that it is 3/4" but the spec and picture look like it is…
  • ralphjy
    ralphjy over 5 years ago in reply to dang74 +1
    Here is the link to Amazon https://www.amazon.com/gp/product/B00K0TKJCU/ref=ppx_yo_dt_b_search_asin_title?ie=UTF8&psc=1 I think that you can get it directly from Adafruit but I was in a hurry. The product…
Parents
  • rati89
    rati89 over 5 years ago

    The whole design looks quite nice in red. Really elegant.

    I am interested, in how well your prototype will predict the weather and how it will work. A really interesting approach.

     

    Another way, of how you could solve the problem, is like a colleague of mine. He uses the real time data of the forecasts to decide if he will adjust his blinds or protect his solar panels from bad weather.

    But still, I like your idea! Also really cute dog pictures, which are always a plus image

     

    Wish you all the best!

    BR

    Brew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dang74
    dang74 over 5 years ago in reply to rati89

    I'll be honest, there were a number of times when it rained and the barometric measurements didn't predict it in advance.

     

    So I am definitely leaning towards your friend's concept of using actual data from weather forecasts.  I imagine there would be a way to tap into this data by means of some IoT method.

    Time permitting, I would definitely like to look into this as I believe that water conservation is a worth while goal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dang74
    dang74 over 5 years ago in reply to rati89

    I'll be honest, there were a number of times when it rained and the barometric measurements didn't predict it in advance.

     

    So I am definitely leaning towards your friend's concept of using actual data from weather forecasts.  I imagine there would be a way to tap into this data by means of some IoT method.

    Time permitting, I would definitely like to look into this as I believe that water conservation is a worth while goal.