Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Waste Food Management Blog #9   Machine Assembly #2
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
  • Author Author: wtos03
  • Date Created: 28 Sep 2020 5:11 PM Date Created
  • Views 760 views
  • Likes 2 likes
  • Comments 1 comment
  • sustain the world
Related
Recommended

Waste Food Management Blog #9   Machine Assembly #2

wtos03
wtos03
28 Sep 2020

This week I had finished assembly all parts together which are

1) Put belt for Grinder’s Motor.

2) Assembly EM Container and Values.

3) Assembly Control Box, On/Off Switch, and 12 V adapter.

4) Wiring all motors and servo.

5) Cover Screw for Stirring rod.

Here is the picture for each view of the machine.

imageimageimageimageimage

After finished assembly. I had tested with dry leaves first.  I want to make sure everything works fine before test on waste food, because of

waste food more moisture. I want to test in dry environment first.  Here is my test video, I need to take many shots and mix together so you can

see machine operation in details.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

https://youtu.be/dxwrPx1bPRs

 

From my testing, I found that the belt is too loose and motor may need more power for crush hard and rigid material like fruits with hard shell.

I need to find a bigger motor and this may take more power and current than the Motor shield can support.  I will try to change the bigger motor if available.

But EM valve works well and the stirring motor should be OK. I also need to cover all the grinder machine as the material are spread all over the place.

 

Next, I will try to find bigger motor, test more and wrap up for the whole project.

  • Sign in to reply
Parents
  • dang74
    dang74 over 5 years ago

    Very impressive. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dang74
    dang74 over 5 years ago

    Very impressive. image