Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog XMC4200 with PROFET+2_12V SHIELD (Blog4)
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
  • Author Author: asokfair
  • Date Created: 12 Sep 2020 5:40 AM Date Created
  • Views 616 views
  • Likes 2 likes
  • Comments 0 comments
  • high current
  • high switches
  • switch
  • infienon
Related
Recommended

XMC4200 with PROFET+2_12V SHIELD (Blog4)

asokfair
asokfair
12 Sep 2020

Hi All,

In the previous blog3 i have explained about interfacing of the H-bridge shield board with XMC2000 Kit to drive DC Motor. In this blog we going to

interface the infineon High Switches (PROFET+2_12V SHIELD)

 

The High current Profit boards have 4 high side Outputs which is capable of driving 20A current. Datasheet is here

In my case I have stacked this shield on top of the TLE94112L shield. the setup looks like below

image

 

Control the Outputs:

Its very simple to control the OUT of BTS7002 by setting high (3.3v) on the IN Pin. In my case i have choosed

IN1 & IN4 to control the OU1 and OUT4.

 

Schematic:

image

 

configured the XMC4200 Pins P0_11 & P2_2 as output

  XMC_GPIO_Init(LOAD_IN4,&config);
  XMC_GPIO_Init(LOAD_IN1,&config);

and toggle the pin inside the SysTick Handler

    XMC_GPIO_ToggleOutput(LED1);
    XMC_GPIO_ToggleOutput(LOAD_IN4);
    XMC_GPIO_ToggleOutput(LOAD_IN1);

 

Make sure that BAT+ is supplied with 12V , I have used 12V 7.5Amps solar battery.

I used 12V LED strips/lights as load for my use case. And finally I could control my lights with a high current profit shield.

The working video is here.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

In the next blog5 we are going to add wireless connectivity.