Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound - Winter Survival Suit Post #1 (Introduction)
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
  • Author Author: dwinhold
  • Date Created: 20 Feb 2017 1:26 AM Date Created
  • Views 1553 views
  • Likes 8 likes
  • Comments 8 comments
  • winter
  • safe and sound design challenge
  • dwinhold
  • survival
Related
Recommended

Safe and Sound - Winter Survival Suit Post #1 (Introduction)

dwinhold
dwinhold
20 Feb 2017

Safe and Sound – Cold Weather Survival Suit Post #1

 

Reason why:

This is a news report from January 11th, 2017:

 

On Tuesday, the warnings covered northeastern Alberta, almost all of Saskatchewan and much of western Manitoba. All people
in those regions are being warned of extreme conditions into Wednesday morning that feel like -45 to -52 with the wind.

 

Attached is another Alberta winter weather report from 2 weeks ago.

 

image

 

As you can see, we get severe cold weather and like it or not we still go out. Either going to work, shopping or recreational the weather
doesn’t get in our way. When I get up to go to work in this cold time of year I always wish there was a better way to stay warm.

 

This is how I came up with the Cold Weather Survival Suit.

 

Explanation of my project

I will take full body thermal underwear and have it computer controlled to:

  • Monitor body temperature at 7 points and outside
    temperature
  • Display information on the LCD screen
  • Display warnings when your temperature drops
    below a set amount
  • Warm the part of you that is getting to cold

 

How this will work

The TI  MSP-EXP432P401RMSP-EXP432P401R will monitor the sensors and control the heat The  430BOOST-SHARP96430BOOST-SHARP96 will display the information to the person
wearing the suit. I will also be using the BOOSTXL-SENSORS to pick-up other important information about the environment.

 

Heating of the suit

I have purchased (and now waiting to arrive) 8 meters of 15mm wide Carbon Fiber Tape. Carbon fiber tape is soft like silk and is 100%
washable. When electricity is put to it, it heats up like a heating blanket. The more electricity, the hotter it gets. Therefore the computer controlling
the carbon fiber will be very efficient for keeping the wearer warm.

 

Below are the carbon fiber specifications:

 

Specifications:

Material:

Carbon
  fiber 100%

Type:

Heating element

Resistance:

18±2
  Ohm/m ( 5.5±0.5 Ohm/ft )

Weight

5±0.5
  g/m (1.5±0.15 g/ft)

Width:

17±2 mm
  (0.67±0.08 in)

Thickness:

0.6±0.1
  mm (0.024±0.004 in)

Tensile
  strength
:

50±10 kg

 

 

image

 

Diagram of the suit

 

image

There will be sensors and carbon fiber elements in the back as well the head

 

 

 

Final Thoughts

 

This is a project I have wanted to make for a few years, now is a great opportunity to make create my idea. Something I will definitely use as well !!

 

Dale Winhold

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +1
    Hot idea. We have had a couple of cold snaps this winter....Maybe it is because we are in a solar sunspot minima. We even had a couple of instances of no sun spots last summer:
  • dwinhold
    dwinhold over 9 years ago in reply to dougw +1
    The weather has been a bit strange this past year. This past week we had +15c weather, this week we are to get to -16c.
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to dwinhold +1
    Dale Winhold wrote: .. this week we are to get to -16c. Switch to °f. It sounds warmer.
Parents
  • dougw
    dougw over 9 years ago

    Hot idea. We have had a couple of cold snaps this winter....Maybe it is because we are in a solar sunspot minima.

    We even had a couple of instances of no sun spots last summer:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 9 years ago in reply to dougw

    The weather has been a bit strange this past year. This past week we had +15c weather, this week we are to get to -16c. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to dwinhold

    Dale Winhold wrote:

     

    .. this week we are to get to -16c.

    Switch to °f. It sounds warmer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 9 years ago in reply to Jan Cumps

    Ok

    3.2°F

     

    It does sound warmer!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dwinhold
    dwinhold over 9 years ago in reply to Jan Cumps

    Ok

    3.2°F

     

    It does sound warmer!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 9 years ago in reply to dwinhold

    On the other hand your -55 C above would be -67 F.