Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound - TELEMETRY SYSTEM FOR SMART CLOTHES #3: The Kit
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
  • Author Author: amolnar
  • Date Created: 14 Apr 2017 8:21 AM Date Created
  • Views 718 views
  • Likes 2 likes
  • Comments 2 comments
Related
Recommended

Safe & Sound - TELEMETRY SYSTEM FOR SMART CLOTHES #3: The Kit

amolnar
amolnar
14 Apr 2017

Hooray!

 

Finally I received the purchased modules, which I need for the participation in this contest !!!

 

It is unfortunate that element14 could not find an opportunity to send me the promised modules, as to all the other participants! I had to buy them for my own money. But the main thing is that I can continue to participate in the contest!

image

Since the mandatory condition for participation is the module  MSP-EXP432P401RMSP-EXP432P401R firstly I ordered it

image

The second module I ordered is 430430BOOST-SHARP96! With remote access to my system, it is basically not needed (and the display is too small), but I wanted to try it out in my work.

image

Unfortunately our local dealer did not have the BOOSTXL-SENSORS module so I bought Sensor Hub BoosterPack It's not quite compatible with the  MSP-EXP432P401RMSP-EXP432P401R but since all the sensors of this board are connected via the I2C interface I'll make an adapter for it

image

Sensors BoosterPack Plug-In ModuleSensor Hub BoosterPack
imageimage
TI OPT3001 Ambient light sensorIntersil ISL29023 ambient and infrared light sensor
TI TMP007 Infrared temperature sensorTI TMP006 non-contact infrared temperature sensor

Bosch BMI160 Inertial Measurement Unit (IMU) sensor –

accelerometer and gyroscope

InvenSense MPU-9150: 9-axis MEMS motion tracking

3-axis gyro

3-axis accelerometer

3-axis compass

Bosch BMM150 Magnetometer

Bosch BME280 Environmental sensor -

pressure, ambient temperature and humidity

Bosch Sensortec BMP180 pressure sensor
Sensirion SHT21 humidity and ambient temperature sensor

 

From my previous project I already had a module  CC3100MODBOOSTCC3100MODBOOST so I did not need to buy it separately

image

Most sorry for the  BQ25570EVM-206BQ25570EVM-206 Power Management module Unfortunately it's too expensive for me so I'll have to give it up I wanted to use it in the power system of my project for using with alternative energy sources(flexible solar panels and piezoelements Well my dream was the development of a combined triboelectric-piezoelectric nanogenerator But without such a module it will be hard but I'll try it all the same

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    It looks like you have the tools to begin the job. DAB
  • amolnar
    amolnar over 9 years ago in reply to DAB +1
    Oh yeah, I'm very happy!!!
Parents
  • DAB
    DAB over 9 years ago

    It looks like you have the tools to begin the job.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amolnar
    amolnar over 9 years ago in reply to DAB

    Oh yeah, I'm very happy!!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • amolnar
    amolnar over 9 years ago in reply to DAB

    Oh yeah, I'm very happy!!!