Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe&Sound:Wearable Tracking Device for Miners - 03: KIT review [MSP-EXP432P401R]
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
  • Author Author: sunnyiut
  • Date Created: 29 Mar 2017 5:41 AM Date Created
  • Views 1045 views
  • Likes 2 likes
  • Comments 1 comment
  • msp432_launchpad
  • safe and sound design challenge
  • msp432p401r
Related
Recommended

Safe&Sound:Wearable Tracking Device for Miners - 03: KIT review [MSP-EXP432P401R]

sunnyiut
sunnyiut
29 Mar 2017

Title: Wearable Tracking Device for Miners                                      

By: sunnyiut                                                                                        

Previous Blogs
01: Introduction02: The Kit

 

Design Challenge: Safe and Sound Wearables

Blog number: 03

 

Intro:image

The heart of this project is the TI  MSP-EXP432P401RMSP-EXP432P401R

In this blog I am presenting my first experience with this chip and Launchpad.

I have demonstrated couple of example codes provided in the tool-chain of MSP432 support.

 

     example codes:          1. out of box experience

                                      2. gpio interrupt

                                      3. PWM controlled LED brightness

 

     IDE:                          Code Composer Studio v7.1.0

     Resource:                  Resource Explorer [dev.ti.com/tirex]

 

 

 

Launchpad Features:

There is no need to mention the features for this project blog post. But still I am highlighting some....

image

  • MCU: MSP431P401R ARM Cortex M4F microcontroller
  • 48MHz
  • 40 pin booster pack plug in module connector
  • Access to unused MCU pins
  • two input button switches
  • two user LEDs [red and RGB]
  • Backchannel UART to PC communication
  • both 5v and 3.3v power
  • JTAG ports and emulator terminals are isolated and connected with jumpers
  • onboard XDS110 emulator for programming, debugging and power supply
  • EnergyTrace technology for real-time power consumption reading through GUI

 

image taken from TI MSP432 Launchpad User Guide

Example Code:

01 - Out of Box Experience

 

Description -

 

This example code comes pre-programmed. It turns the RGB LED on and off with default 60 pulse per minute.

Initially it's RED, but color can be selected by pressing the S2 switch.

S1 button switch can be used to blink the LED at different speed.

imageimageimageimage

by pressing S2 different colors can be selected - green, blue, white, red

 

GUI - [could not connect in CCS v7.1.0]

 

This example code comes with a GUI that communicates with the Launchpad through serial COM port. Blinking speed and color can be selected from the GUI.

However, I could program and debug this example code from CCS v7.1.0 and the GUI gets started, but could not connect to the launchpad.

So, I tried to check out the online resource explorer and found that the GUI runs smoothly on both Chrome and Mozilla after installing the TI Cloud Agent addon.

 

imageimage

CCS v7.1.0 shows 'connecting' but could not connect to Launchpad   Resource Explorer runs the GUI on Chrome and asks for TI Cloud Agent Installation

 

imageimage

GUI can connect to the device after installing TI Cloud Agent on Chrome   GUI runs smoothly on Chrome to change blinking speed and color

 

Later on, I tried another approach to run the GUI offline from my desktop. I installed the 'software example' bundle from the product page of TI and found a standalone executable file for the GUI. This time it runs without any problem. However, I'll try to figure out whats wrong with CCS v7.1.0 later on.

image

 

Example code:

02 - gpio interrupt

 

Description -

 

This example code takes input from button switches S1 and S2 and generates interrupt to toggle LED1 and LED2 [red] respectively.

 

imageimageimage

LED1 turns on by default, LED2 turns off                by pressing S1, LED1 toggles and turns off               by pressing S2, LED2 toggles and turns on

 

Example code:

03 - PWMLED

 

Description -

 

This example code generates a PWM on the P2.0 pin where the RGB LED [red] is connected. The duty cycle of the PWM signal gradually increase and decrease within a time period.

With respect to that the brightness of the LED also increases and decreases gradually.

My aim for trying this code was to check out the EnergyTrace Technology of the Launchpad and CCS.

 

imageimageimage

Brightness of the LED changes with the duty cycle of the PWM signal

 

Energy Trace:

 

MSP-EXP432P401RMSP-EXP432P401Rlaunchpad supports Real-time power consumption reading and the CCCS v7.1.0 has nice GUI to view those traces I tried PWMLED example code mentioned above to check out this function As the brightness of the LED increases and decreases the power traces follow a gradual increment and decrements This tool generates an assumption of battery life based on the energy consumption too

 

imageimage

overview on energy consumption [10sec]                                       Power trace - real time

image

energy trace - 10 sec long

 

MikroC Pro for ARM and UNI FLASH:

 

I am a big fan of Mikroelektronika MikroC compilers. They have recently added support for MSP432 microcontrollers in their MikroC Pro for ARM compiler.

Therefore, I liked to go for a test drive with this compiler. To download the hex into the MSP432P401R through the launchpad programmer, I used TI's web based programmer UNI FLASH.

My experience is pretty good. I made a simple program to blink both LED1 and LED2 with 300ms delay. UNI FLASH connects to the launchpad smoothly and load the hex with a very simple GUI.

 

void main() {
  GPIO_Digital_Output(&DIO_P1IN, _GPIO_PINMASK_0 | _GPIO_PINMASK_1);
  GPIO_Digital_Output(&DIO_P2IN, _GPIO_PINMASK_0 | _GPIO_PINMASK_1);

  DIO_P1OUT = 0;
  DIO_P2OUT = 0;
  DIO_P1OUT.B0 = 0;
  DIO_P2OUT.B0 = 0;
  
  while (1) {
    DIO_P1OUT.B0 = 1;
    Delay_ms(300);
    DIO_P2OUT.B0 = 1;
    Delay_ms(300);
    DIO_P1OUT.B0 = 0;
    Delay_ms(300);
    DIO_P2OUT.B0 = 0;
    Delay_ms(300);
  }
}

 

 

image

 

This is what I experienced with the MSP432 launchpad so far. In my next blog I'll post a review on the Sharp96 memory LCD booster Pack.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +2
    Very good detailed blog. Thanks DAB
Parents
  • DAB
    DAB over 9 years ago

    Very good detailed blog.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Very good detailed blog.

     

    Thanks

    DAB