Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Documents Safe & Sound Design Challenge: The Kit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 23 Nov 2016 3:36 PM Date Created
  • Last Updated Last Updated: 23 Feb 2017 3:04 PM
  • Views 4800 views
  • Likes 12 likes
  • Comments 27 comments
Related
Recommended

Safe & Sound Design Challenge: The Kit

image
Safe & Sound Design Challenge
About the ChallengeThe KitThe PrizesThe Judges
Intro VideoExample ApplicationTerms and ConditionsTechnical Documents
The Challengers

 

Fifteen Challengers will be selected to enter the Safe & Sound Wearables Design Challenge. Each Challenger will receive the following kit - sponsored by Texas Instruments - for FREE (worth almost $300).

 

The lucky 15 will then embark on building an inspired and inventive project that protects you and your personal property anywhere you go. Note other members may still enter at any point as long as they comply with the main terms of the conditions integrating  MSP-EXP432P401RMSP-EXP432P401R in a project.

 

Complete your project and at least 10 blog posts, and you’ll also be in the running for one of these awesome prizes, including a DJI Phantom quadcopter!

 

 

The Kit

For Texas Instruments Product Disclaimer

Texas Instruments Main Application MCU - MSP-EXP432P401RMSP-EXP432P401R


The MSP-EXP432P401RMSP-EXP432P401R LaunchPad enables you to develop high performance applications that benefit from low power operation. It features the MSP432P401R, which includes a 48MHz ARM Cortex M4F, 95μA/MHz active power and 850nA RTC operation, 14-bit 1MSPS differential SAR ADC and AES256 accelerator.This LaunchPad includes an on-board emulator with EnergyTrace+ Technology,which means you can program and debug your projects without the need for additional tools, while also measuring total system energy consumption. All pins of the  MSP-EXP432P401RMSP-EXP432P401R device are fanned out for easy access These pins make it easy to plug in 20-pin and 40-pin BoosterPacks that add additional functionality like wireless, capacitive touch and more (worth $12.92).

image
Buy NowBuy Now

Texas Instruments  CC3100MODBOOSTCC3100MODBOOST Wi-Fi Network Processor


The  CC3100MODBOOSTCC3100MODBOOST is a SimpleLink Wi-Fi CC3100 module BoosterPack The SimpleLink Wi-Fi CC3100 module BoosterPack can be used to connect to TI LaunchPad evaluation kits. With the advanced emulation BoosterPack (CC31XXEMUBOOST) CC3100BOOSTCC3100BOOSTcan connect to a PC for MCU emulation and software development using SimpleLink Studio for CC3100. This kit can also be connected to other platforms through pins use the programming guide for instructions on porting driver and sample code to any microcontroller. The SimpleLink Wi-Fi CC3100 solution gives the flexibility to add Wi-Fi to any microcontroller (MCU). This internet-on-a-chip solution contains all user need to easily create IoT solutions for security, quick connection (worth $24.86).

Please Note: This part is currently only available for purchase inside North America, Canada and Brazil. CC3200MODLAUNCHXL and CC3200AUDBOOST are available  alternatives for purchase inside Europe and APAC.

image
Buy NowBuy Now

Texas Instruments  DLP-7970ABPDLP-7970ABP NFC Transceiver


The  DLP-7970ABPDLP-7970ABP is a NFC transceiver BoosterPack The DLP design NFC/RFID BoosterPack  DLP-7970ABPDLP-7970ABP is an add-on board designed to fit all of TI’s MCU LaunchPads. This BoosterPack allows the software application developer to get familiar with the functionalities of TRF7970A multi-protocol fully integrated 13.56MHz NFC/ HF RFID IC on their Texas Instruments Embedded microcontroller platform of choice without developing the RF section (worth $38.22).

      image
Buy NowBuy Now

Texas Instruments BOOSTXL-CC2650MABOOSTXL-CC2650MA BLE Network Processor


The SimpleLinkTm BluetoothRegistered low energy CC2650 Module BoosterPack plug-in module is the quick and easy way to add Bluetooth low energy to your LaunchPadTm development kit. Simply plug the CC2650 module BoosterPack kit into the MSP432Tm microcontroller (MCU) LaunchPad kit to get started! The CC2650 module BoosterPack kit is programmed with a wireless network processor software that allows you to add Bluetooth low energy connectivity to any application using simple UART interface. The module BoosterPack kit also includes a JTAG connection for programming and debugging the CC2650 module. This allows you to develop any Bluetooth low energy application on the CC2650 module (worth $53).

      image
Buy NowBuy Now

Texas Instruments  BOOSTXL-SENSORSBOOSTXL-SENSORS Sensors Booster Pack


This Texas Instruments Booster Pack contains the following sensors: TI OPT3001 Ambient light sensor; TI TMP007 Infrared temperature sensor; Bosch BMI160 Inertial Measurement Unit (IMU) sensor – accelerometer and gyroscope; Bosch BMM150 Magnetometer; Bosch BME280 Environmental sensor - pressure, ambient temperature and humidity (worth $12.92).

      image
Buy NowBuy Now

Texas Instruments BQ25570EVM-206 BQ25570EVM-206 Power Management Bat


EVM for Ultra Low Power Harvester Power Management IC with Boost Charger, and Nanopower Buck Converter - the BQ25570 Ultra-low power boost charger with integrated DC/DC conversion used for battery management for wearable devices, the BQ25570 is an integrated energy harvesting Nano-Power management solution that is well suited for meeting the special needs of ultra-low power applications BQ25570's EVM is the BQ25570EVM-206 (worth $111.42).

      image
Buy NowBuy Now

Texas Instruments 430BOOST-SENSE1430BOOST-SENSE1 Capacitive Touch Booster Pack


Capacitive Touch Booster Pack - Capacitive sensing is common (if not standard in wearable devices. Hence, This Boosterpack is an easy way to add capacitive touch sensing to a prototype design. The TI site says this cap touch BoosterPack is compatible with the MSP-EXP432P401R MSP-EXP432P401R (worth $10.30).

      image
Buy NowBuy Now

Texas Instruments 430BOOST-SHARP96430BOOST-SHARP96 Memory LCD Booster Pack


The SharpRegistered Memory LCD BoosterPack Plug-in Module is based on the LS013B4DN04 display from Sharp Electronics and features capacitive touch sliders. MCU LaunchPad Evaluation Kit developers can use this BoosterPack to display sensor readings, time & other information using the displays 96x96 pixels as well as to provide touch based input!  (In lieu of Cap Touch Booster Pack) (worth $20.58).

      image
Buy NowBuy Now
  • competition
  • design challenge
  • safe and sound
  • challenger kit
  • contest
  • Wearable tech
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 9 years ago +3
    Is there any information on the physical dimensions of the msp432? Ive had a look through the user guide and cant seem to find any mention of it, maybe I just missed it! This is important with a wearables…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to e14 Contributor +3
    Lucie, the beta board I have at home is 9.5 * 6 cm. It's 2 cm high without anything mounted on top or bottom connectors.
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to pencilnose2 +3
    You could use a powerbank. For low energy designs I use the one I got from my employer...
  • e14phil
    e14phil over 9 years ago

    Dear All
    Please note:
    Due to an issue with getting challenge Kit out to some of our challengers the Safe & Sound Wearables Challenge project submission date has been extended further to Monday, 10th July 2017 at 09:00 GMT.

    Thank you to all our Challengers, we hope this gives you enough time to really sink your teeth into this challenge, finish your projects and hit the 10 updates finishing line.


    Good Luck!

    e14Phil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago

    For anyone looking for a quick Pin-out reference for the LaunchPad and BoosterPacks, the TI Energia page has a link for the the pin-out for most of the devices.  These pin-out also include the Pin Number for the associate signal which certainly comes in handy.

     

    http://energia.nu/pin-maps/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago in reply to rscasny

    Randall,

    Thanks for the update.  Also, since I missed the opportunity in the previous post, I appreciate Element14 and Texas Instruments for providing such great tools to work with during this challenge.  I look forward to implementing these into my project and seeing what I can do with them. 

     

    You guys are awesome!

     

    Cheers,

     

    Jon

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to jomoenginer

    Jon,

     

    We are waiting on that board to be delivered. We decided to send you out the remaining boards so you can get started. We'll have to send you a follow up shipment when that board gets in.

     

    Randall

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago

    I noticed from the pics/videos as well as the kit that I recently received the BOOSTXL-SENSORS Sensors Booster Pack is not included as listed in the list of devices from the Challenge Kit list.  Is this no longer available?

     

    Cheers,

     

    Jon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jwatson
    jwatson over 9 years ago

    Hi All

     

    Want to learn more about the mandatory TI board in this Challenge Kit?

     

    Check out our NEW related ESSENTIALS Learning Modules: MCUs II - Wireless Microcontrollers too!

    element14 Essentials: MCUs II

     

    Take the quiz to test your knowledge, then read the module page, then retest yourselves and share the module link with your friends...a bit of fun & if you follow the criteria, you can earn a digital badge on your profile too!

     

    Become an expert image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch

    It uses a UART interface. I haven't checked if it's plug-in compatible, but certainly the protocol is a match.

    It would be nice to see this working!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago

    Any idea if something like the CC4000 GPS Module Kit would work with the MSP-EXP432P401R MCU? 

     

    I am not seeing it as a listed BoosterPack that is compatible.

     

     

    http://www.ti.com/tool/cc4000gpsem

     

    Thank you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • raffi3438
    raffi3438 over 9 years ago in reply to Jan Cumps

    Great, thanks!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to raffi3438

    Raffi,

    Yes, that's allowed. There is one component you have to use, the  MSP-EXP432P401R launchpad.

    You're free to add your own components.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>