Think ON Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Think ON Design Challenge
  • More
  • Cancel
Think ON Design Challenge
Blog Blog 4 - Think ON Design Challenge - Smart Pet Collar BLEx2
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
  • Author Author: rsc
  • Date Created: 9 Feb 2020 11:43 PM Date Created
  • Views 685 views
  • Likes 6 likes
  • Comments 1 comment
  • ble
  • arduino mkr 1010
  • think on design challenge
Related
Recommended

Blog 4 - Think ON Design Challenge - Smart Pet Collar BLEx2

rsc
rsc
9 Feb 2020

I'm finding out about BLE more and more each week.  I didn't realize RPi was BLE or Arduino MKR WIFI 1010 was BLE.

Updating the firmware on the Arduino MKR WIFI 1010, gave me a new platform to play with the RSL10.

I have a feature for the project where one BLE device recognizes another when in proximity.  The BLE device will periodically scan for other BLE devices in the area and act on the result.

Here's some modified code from the Arduino BLE examples.

  if (peripheral) {
    // discovered a peripheral
    Serial.println("Discovered a peripheral");
    Serial.println("-----------------------");


    // print address
    Serial.print("Address: ");
    Serial.println(peripheral.address());
    if (peripheral.address()=="60:c0:bf:29:ea:57"){ //address of the RSL10
      Serial.println("LED on");
      digitalWrite(ledPin, HIGH);
      // stop scanning
      BLE.stopScan();
      explorerPeripheral(peripheral);  //get RSL10 data
      }

If the BLE device recognizes the address of a "friend" device, then it reads the data from the new friend and responds to the server.

The arduino can activate GPIO for food/enter/egress/etc when a known friend enters the area.

  • Sign in to reply
  • dubbie
    dubbie over 6 years ago

    BLE is something that I would like to get to grips with at some point. It is interesting that the MKR 1010 is BLE. Regretfully I only have a MKR1000 which I am guessing is not BLE.

     

    Dubbie