Think ON Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Think ON Design Challenge
  • More
  • Cancel
Think ON Design Challenge
Blog RSL10-SENSE-GEVK Kit Unboxing!
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
  • Author Author: waihong113
  • Date Created: 11 Dec 2019 4:42 PM Date Created
  • Views 990 views
  • Likes 3 likes
  • Comments 2 comments
Related
Recommended

RSL10-SENSE-GEVK Kit Unboxing!

waihong113
waihong113
11 Dec 2019

After a long wait, I finally received my RSL10-SENSE-GEVK Kit, delivered to me by DHL Express

The kit is enclosed in a big box, and inside the box contains a smaller box that has the logo of On-Semiconductor

image

This box looks so elegant and eco-friendly. I am excited to see what is inside

image

This box contains the RSL10-SENSE-GEVK itself, a Segger debugger J−Link LITE CortexM and a USB cable, a Bluetooth connector, a flexible antenna, battery, and a 10 pin connector.

The RSL10-SENSE-GEVK is inserted in a charge insulation package. The products are well enclosed in polyform materials for shock proofing.

 

After unboxing, I immediately connect the battery to the RSL10-SENSE-GEVK to test the board.

before I play with the board, I read the tutorial from this PDF file https://www.onsemi.com/pub/Collateral/EVBUM2614-D.PDF

 

I downloaded RSL10 Sense and Control mobile application. The mobile application detects and connects to the board rapidly via Bluetooth(less than 1 second)

It is amazing that the application can read sensor readings from the board without any kind of setup needed.

This shows the convenience of plug-and-play

I have tried out some functions like gyroscope, accelerometer, and temperature sensors.

The interface is quick and easy

image

In overall, I am very excited that I am shortlisted to be the participant and given chance to work with this RSL10-SENSE-GEVK board. I will do my best to win this competition.

  • Sign in to reply

Top Comments

  • cstanton
    cstanton over 6 years ago +2
    That is pretty compact!
  • e14phil
    e14phil over 6 years ago +1
    teeny tiny!
  • e14phil
    e14phil over 6 years ago

    teeny tiny!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 6 years ago

    That is pretty compact!