Twist, Turn and Move Design Challenge with TE Robotics
  • Challenges & Projects
  • Design Challenges
  • Twist, Turn and Move Design Challenge with TE Robotics
  • More
  • Cancel
Twist, Turn and Move Design Challenge with TE Robotics
Blog Teleoperation Robot - Blog #2 - Twist, Turn and Move Design Challenge with TE Robotics
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: nilutpol_kashyap
  • Date Created: 29 Aug 2022 5:08 PM Date Created
  • Views 915 views
  • Likes 6 likes
  • Comments 1 comment
  • robots
  • te connectivity
  • Twist Turn and Move Robotics Design Challenge
  • terobotics
  • designchallenge
  • Turn and Move Design Challenge with TE Robotics
Related
Recommended

Teleoperation Robot - Blog #2 - Twist, Turn and Move Design Challenge with TE Robotics

nilutpol_kashyap
nilutpol_kashyap
29 Aug 2022

1. The Official Challenger Kit

the_kit

Contents

    - Arduino UNO R3 Board

    - DFRobot 2x2A Motor Shield for Arduino Twin

    - DFRobot Gravity: IO Expansion & Motor Driver Shield

    - TE Connectors (so many, can't even name them all)

I really like the Italy Made Arduino UNO R3 board. I have been working on these cheap Arduino UNO clones for such a long time.

image

2. Testing the 2x2A Motor Shield for Arduino Twin

2.1 Components

    - Arduino UNO R3 Board

    - DFRobot 2x2A Motor Shield for Arduino Twin

    - DC Geared Motor x 2

    - Power Source

2.2 Connection

imageWe need to change the Power Selection Jumper according to our power source. The motors can be powered by external power supply(PWMIN) or VIN from Arduino control board(e.g., UNO). 

* The two parallel jumper pins are by default, in VIN. So, if we want to use external power, we need to remove them both from VIN and put them over PWRIN.

In my case, I am using external power source in the Shield, so I had to change two parallel jumpers and put them onto PWRIN as show in the above connection diagram.

The shield uses 4 Pins in total for controlling two motors (2 pins per motor). Pins 10 and 12 for motor M1 and Pins 11 and 13 for motor M2. Pins 10 and 11 are PWM pins and used for controlling the speed of motors.

2.3 Arduino Code for Controlling two motors

Github Code - l298n_motor_control.ino

The code is written so as to control 2 DC Geared motors using the pins 10 and 12 for motor M1 and pins 11 and 13 for motor M2.

2.4 Output

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

3. Testing the Gravity IO Expansion Shield With Arduino Uno

3.1 Components

    - Arduino UNO R3 Board

    - DFRobot Gravity: IO Expansion & Motor Driver Shield

    - SG90 Servo motor x 2

    - MG995 Servo motor x 1

3.2 Connections

Two SG90 servo motor are connected to the pins A0 and A1.

1 MG995 servo motor is connected to pin A5.

image

The Analog pins on the shield are attached along with 5V and GND pins in the same order as the Servo motors. It made easier for me to directly put the servo motor connectors into the pins.

image

image

3.3 Arduino Code

Github Code - gravity_shield_servo_control.ino

3.4 Output

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
Parents
  • DAB
    DAB over 4 years ago

    The motors look small, are you going to have enough torque to move it once everything is assembled?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 4 years ago

    The motors look small, are you going to have enough torque to move it once everything is assembled?