Join us in Congratulating the Official Challengers of Twist & Turn Design challenge:
Internet Controlled Teleoperation Robot
nilutpol_kashyap
Unlimited CNC Robot
dwinhold
The Robo Cat
jwr50
Pool Butler
robogary
ARDUMOBO: Arduino mobile robot
a33333
PV Cleaning System
amgalbu
Robotic Yoga Instructor
hitesh.boghani
Sammy Semaphore - Semaphore Robot
dougw
R-Arm
GustavoMorales
Autonomous Navigation Robot
ajayvishaal
The Dates
To make sure challengers get their kit on time we have pushed back the end dates of this challenge and will be updating the site copy and terms to correspond with this.
Project Phases | Dates |
---|---|
Challengers Announced | 6th July 2022 |
Build Period | 7th July - 12th September 2022 |
Projects Due | 12nd September 2022 |
Winners Announced | September 2022 |
Prizes Shipped | September 2022 |
The Challenge
Each participant will receive a Challenger’s Kit, with which they are challenged to design and build a robotic arm or mobile robot that performs a specific task.
These 10 successful applicants will get a Selection of TE Connectors, an Arduino Uno, and Robotics Shields, free of charge, to build and blog their project with.
For the chance to win one of the prizes below, participants must blog their build process, as well as the final outcome of their Robotic Movement Project.
Included in the Challenger's Kit are a Selection of TE-provided components, as well as an Arduino Uno; use these to create your Robotic Movement Project.
Good integration of the TE components and interesting uses of movement will be graded more favorably.
Example tasks that can be performed include, but are not limited to:
- Building a robot arm that can pick up and set down an object
- Building a robot arm that moves in all degrees of freedom
- Building a mobile robot that follows a line
- Building a mobile robot that can avoid an object in its path
Challenger's Kit The Kit | Product Name |
---|---|
Dynamic Connectors Parts: 1-2366515-4 Connector Housing More Items: AXICOM IM Signal Relay |
|
Arduino Uno |
|
DRI0017 2x2A Motor Shield for Arduino Twin (Product Image may differ) |
|
DFR0502 Gravity: IO Expansion & Motor Driver Shield (Product Image may differ) |
*Or local equivalent
**Grand Prize and Runner Up winners also earn the finisher prize.