Ultimate RoadTest
  • Challenges & Projects
  • Design Challenges
  • Ultimate RoadTest
  • More
  • Cancel
Ultimate RoadTest
Blog Project "code name" Part 011
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 20 May 2012 12:33 AM Date Created
  • Views 861 views
  • Likes 1 like
  • Comments 1 comment
  • ultimate_roadtest
Related
Recommended

Project "code name" Part 011

COMPACT
COMPACT
20 May 2012
20th May

"But there are alternatives.."

As not to encroach on Nick's work with load cell interfaces, I have interfaced a set of digital scales in a completely different way to retain its original functionality and appearance.

image

 

My scale has an ASIC with I2C ROM that does all the work and I'm letting it do all the load cell management.

 

Like my previously mentioned mystery device I have reverse engineered the digital scales to find suitable interface points to tap.

At this moment I am purely using the scales as a pressure switch.

When a preset threshold pressure is reached (either in a positive or negative sense) it will assert a digital signal which the SimpleLink Wi-FI C3300 can process such as send a twitter message or SMS.

 

This is accomplished using just 3 wires;

     Ground

     On/Off and Zero Function

     "minus" LCD signal

 

Depending upon the circumstance, an additional actuator may be necessary to reset the threshold pressure setting or prevent the unit from automatically turning off.

This is to lift or place a calibration weight on the scales to either zero the setting or present signs of activity.

 

All that is going on is under program control, setting the Zero point to the threshold setting and checking the display for a positive or negative reading. 

image

 

The On/OFF LCD signal is used to turn the scales on and if necessary reset the desired threshold setting.

The "minus" LCD signal is not a digital logic level signal but an AC multi level LCD drive signal.

With a bit of decoding of this signal can be interpreted as either "minus" segment on or off.

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    When you get the project done, you might want to do some more explaining on the scale tap.

     

    I know I am interested and I am sure that others will be interested as well.  You know how us tinkerers think. image

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    When you get the project done, you might want to do some more explaining on the scale tap.

     

    I know I am interested and I am sure that others will be interested as well.  You know how us tinkerers think. image

     

    Thanks

    DAB