Upcycle IoT Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Upcycle IoT Design Challenge
  • More
  • Cancel
Upcycle IoT Design Challenge
Blog Curiosity Nano Programming
  • Blog
  • Forum
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Upcycle IoT Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 8 Feb 2024 5:01 AM Date Created
  • Views 2671 views
  • Likes 4 likes
  • Comments 5 comments
  • dougw
  • Microchip Curiosity Nano
  • Curiosity Nano with Arduino compiler
Related
Recommended

Curiosity Nano Programming

dougw
dougw
8 Feb 2024

Intro

The design kit has finally arrived, so this is a belated push to get something built and working before the project deadline this week. I have been able to get the kit system running some preliminary software but unfortunately I need to break off at this point and work on the final project blog. The plan for the Microchip Curiosity Nano was to build a file management system for my old Rockwell AIM 65, which used a cassette tape recorder for non-volatile storage. The Curiosity Nano can provide solid state storage and file management to rejuvenate the AIM 65.

Originally I was going to use the Curiosity Nano to simply act like a tape recorder, just recording and playing audio files which store digital data as modulated audio tones. However I think it will be better to store files as text via the AIM 65 ability to interface to a Teletype.

This blog is about how the Curiosity Nano can utilize Arduino libraries. To facilitate this Niraldri has created a Curiosity Nano board package for the Arduino IDE. (Link below) This board package allows the Arduino libraries and IDE to be used to create programs for the Curiosity Nano, but the Arduino IDE can't yet flash a program to the Curiosity Nano. However it can create a binary file that can easily be flashed to the Curiosity Nano by Microchip's MPLAB X IDE.

image

The AIM 65 File System Concept

The file system will be a simple approach. The system will have a fixed set of files that can be overwritten as needed. Suppose it is just 20 files - 2 buttons will allow scrolling through the 20 file names - forwards and backwards. One other button allows any data coming through the serial port to be saved in the currently selected file, which gets closed when any button is pushed. The last button sends the currently selected file to the serial port.

Programming the Curiosity Nano

This is the process I followed:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

To determine which pins were controlled by the buttons, I had to write a separate program to test each pin.

Here is the json message to install the board in the Arduino ISE:

" https://raw.githubusercontent.com/niladridmgit/CuriosityNiladriSAME51/master/package_curiosityniladri_same_index.json "

This is a good start but there is still work to do. The good news is that the unknowns have been eliminated and completion is mainly a matter of finding some time to work on it.

Here is the Software such as it is - very preliminary:

Firmware

/* File Management System for an AIM65 using a Microchip Curiosity Nano Eval Kit
 *  LCD1.ino
 *  by Doug Wong 2024
 *   20 character 4 line I2C Display
 *   Uses Bill Perry's HD44780 Library, which can be installed from the Arduino Library Manager
 *   See Bills documentation: https://github.com/duinoWitchery/hd44780
 *   
 *   Uses Curiosity Nano board package by Niladri installed with this json message:
 *   https://raw.githubusercontent.com/niladridmgit/CuriosityNiladriSAME51/master/package_curiosityniladri_same_index.json
 *   see his docs here: https://github.com/niladridmgit/CuriosityNiladriSAME51
 */
 // ----------------------------------------------------------------------------

/*-----( Import needed libraries )-----*/
#include <Wire.h>
#include <hd44780.h>                       // main hd44780 header
#include <hd44780ioClass/hd44780_I2Cexp.h> // i2c expander i/o class header


/*-----( Declare Constants )-----*/
// LCD geometry
const int LCD_COLS = 20;
const int LCD_ROWS = 4;
const int bp1 = 23;  // the number of the Up pushbutton pin
const int bp2 = 33;  // the number of the Down pushbutton pin
const int bp3 = 29;  // the number of the Left pushbutton pin
const int bp4 = 32;  // the number of the Right pushbutton pin

const int ledPin = 4;    // the number of the LED pin

/*-----( Declare objects )-----*/
hd44780_I2Cexp lcd; // declare lcd object: auto locate & auto config expander chip  
/*-----( Declare Variables )-----*/
int status;
int Upin, Dpin, Lpin, Rpin;

void setup()   /*----( SETUP: RUNS ONCE )----*/
{
    // initialize the LED pin as an output:
  pinMode(ledPin, OUTPUT);
  // initialize the pushbutton pin as an input:
  pinMode(bp1, INPUT);
  pinMode(bp2, INPUT);
  pinMode(bp3, INPUT);
  pinMode(bp4, INPUT);

  status = lcd.begin(LCD_COLS, LCD_ROWS);
  if(status) // non zero status means it was unsuccesful
  {
    // hd44780 has a fatalError() routine that blinks an led if possible
    // begin() failed so blink error code using the onboard LED if possible
    hd44780::fatalError(status); // does not return
  }  
  Serial.begin(9600);

  // Print a message to the LCD.
  lcd.setCursor(0, 0);
  lcd.print("     element14");
  delay(1500);
  lcd.setCursor(0, 1);
  lcd.print(" Upcycling Project"); 
    lcd.setCursor(0, 2);
  lcd.print("     Utilizing      "); 
    lcd.setCursor(0, 3);
  lcd.print("   Curiosity Nano   "); 
  
  delay(5000);
  lcd.clear();
  lcd.print("AIM65 File 1        ");
}/*--(end setup )---*/


void loop()
{
  lcd.setCursor(0, 0);
  // read all buttons
  Upin = digitalRead(bp1);
  if (Upin == 0) {
    lcd.print("AIM65 File 1        ");
  }

  lcd.setCursor(0, 0);
  Dpin = digitalRead(bp2);
  if (Dpin == 0) {
    lcd.print("AIM65 File 2        ");
  }

  lcd.setCursor(0, 2);
    Lpin = digitalRead(bp3);
  if (Lpin == 0) {
    lcd.print("<<   Receiving   <<");
    delay(3000);
    lcd.setCursor(0, 2);
    lcd.print("                    ");
  }
  else {
    lcd.print(" ");
  }
  lcd.setCursor(0, 2);
    Rpin = digitalRead(bp4);
  if (Rpin == 0) {
    lcd.print(">>>    Sending   >>>");
    delay(3000);
    lcd.setCursor(0, 2);
    lcd.print("                    ");
  }
  else {
    lcd.print(" ");
  }

  delay(50);
 // clear the screen
 // lcd.clear();

}

Just to provide some insight into what the AIM 65 is I made a descriptive video:

The AIM 65

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

It is a bit disappointing that the kit arrived so late in the design challenge, but it is a nice kit and it is at least up and running preliminary firmware.

I am pretty happy that I now have a workflow that allows development of the final application.

I now have one day left to pivot and put together the final project blog, which is not a lot of time, but it was important to spend the time to get the challenge kit up and running.

Links:

Upcycle The Beast - Blog 1

Serendipitous Salvage - Blog 2

What is on those old disks?

Mr. Pentium

PC based bench supply

Curiosity Nano Unboxing

Curiosity Programming

 Super-cycle Design Challenge 

 Upcycle IoT Design Challenge 

Upcycle IoT Design Challenge Info

https://github.com/niladridmgit/CuriosityNiladriSAME51

  • Sign in to reply
Parents
  • JWx
    JWx over 2 years ago

    Interesting project! If I manage to revive my CA80 I could possibly make something like this also (but the tape-recorder emulating version  - my computer doesn't have text based program loading method AFAIK)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to JWx

    You can see the green audio card with its 3.5mm jacks at the lower portion of the above images. I have not loaded libraries for it yet since this application will not use that method. However, eventually it can be used as a fully functional MP3 player with a 4 line display, so it won't be wasted. The other Click board is a micro SD card interface which can store files or music.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 2 years ago in reply to JWx

    You can see the green audio card with its 3.5mm jacks at the lower portion of the above images. I have not loaded libraries for it yet since this application will not use that method. However, eventually it can be used as a fully functional MP3 player with a 4 line display, so it won't be wasted. The other Click board is a micro SD card interface which can store files or music.