Upcycle IoT Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Upcycle IoT Design Challenge
  • More
  • Cancel
Upcycle IoT Design Challenge
Blog Using (obsolete) home appliances to optimize energy consumption - blog 1, why
  • Blog
  • Forum
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Upcycle IoT Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: JWx
  • Date Created: 29 Jan 2024 9:49 PM Date Created
  • Views 732 views
  • Likes 10 likes
  • Comments 2 comments
  • Upcycle IoT Design Challenge
Related
Recommended

Using (obsolete) home appliances to optimize energy consumption - blog 1, why

JWx
JWx
29 Jan 2024

Intro

If by some crazy accident you happen to analyze your customer agreement with the grid utility, you can probably find a paragraph about energy parameters and penalties when they are exceeded. It usually includes parameters like availability, voltage, base frequency and harmonics levels. This blog will be mainly about voltage level.

In the old, good times everything was simpler. Energy was produced in a few big, predictable power stations and the main concern was daily consumption variation, creating peaks and times of lesser demand. As some (types of) power stations were difficult/slow to control, some balancing methods were devised: different types of power stations at the production side (activated only at peak demand) and some incentives for consumers to move their demand off-peak (usually in form of tariff plans, when off-peak energy consumption was less expensive).

And here enters distributed renewable energy generation, with many small producers of hard to predict energy generation curves, which in turn  can lead to events of massive overproduction. In the rest of this blog I will concentrate on photovoltaic installations but the same can be usually said about wind turbines.

Economy of PV installation 

There are probably areas where photovoltaic energy production closely fits the desired consumption curve - I can imagine some warm, sunny, dry territories, with infrequent clouds and most of the energy consumed by A/C systems. In those cases, most of the energy produced can be consumed locally and instantly, limiting grid-wide influence.

But PV installations - as the cheapest, simplest to install and thus most available, are installed also in other places. For example, in central Europe, monthly PV production can be like this (source: https://re.jrc.ec.europa.eu/pvg_tools/en/)

Central Europe PV energy production

Even worse, in the northern Europe it can be like that:

monthly PV production - Sweden

As can be seen, production during the winter can be well below 1/4 of the level of the summer. To make things worse, energy consumption curve would be an opposite: during the winter more energy will be consumed not only for lighting but in some cases also for heating. This means that else:

  • one scales the installation for summer's energy consumption of the household (and still needs to buy most of the energy from the grid during the winter),
  • or installation is scaled to provide for most of the energy needs during the winter, thus being greatly over sized during the summer

One can ask - what's a big deal? I can sell the excess energy during the summer and be independent (energy-wise) during the winter. Not so fast - energy can be sold only if there is somebody who will consume it. Considering that private PV installations can be installed in every (other) home, overproduction problem will be only greater, especially when there is no energy-hungry industry nearby that can consume it. Some energy can be transferred deeper into the grid through low-to-middle voltage transformers, but usually energy overproduction can be experienced in all the area. And before that, local energy overproduction effects will be felt.

What is the main effect of energy overproduction? Grid voltage will raise and the frequency will increase - in both cases there are limits set that cannot be crossed. In the case ot the voltage, when it increases above (usually) 10% of nominal grid voltage, production has to cease and properly configured PV inverters (others are hunted by the utility crews and owners are fined and/or disconnected for breaching of agreements) will power down. 

Possible optimizations

As we can see, there is a possibility of great waste of resources - generation would be prohibited during the best times for it. What can be done in this case? Some producers resort to wasteful local consumption methods - using electricity to (for example) heat the water, when heating using direct solar energy is much more efficient (considering PV panel effectiveness of < 25%). Some are employing some energy storage systems (that can be expensive and short-lived).

Another approach could be the same as when utilizing off-peak tariffs - to move energy-hungry processes to the times of excess energy production. And if it means it will reduce energy consumption in other times, all the better.

In this project I would like to concentrate on possibility of storing excess energy as a cold in the typical household - technique employed by the operators of large industrial freezers, when they are over-freezed during energy production peaks in hope that it will conserve energy during the rest of the day.

  • Sign in to reply
  • JWx
    JWx over 2 years ago in reply to Andrew J

    Same here (Poland) - up to last year there was a system of using grid as a battery: excess energy produced was supposed to go to the grid with the promise to be able to retrieve some percent of it later at no cost, with balancing period of even several months (so one theoretically could produce at summer and retrieve at winter). It was too good it seems and they have switched to net metering (excess energy is simply sold at wholesale prices). But - you can only sell if the grid accepts it.

    New inverters have to obey some (I think EU - so you may be not subject of it) regulation about remote shutdown possibility and even old installations must shut down if grid voltage is too high (one disillusioned PV installer/owner have hinted me to measure socket voltage during sunny day). You can test it also - if voltage in the socket is about 10% higher than nominal (253V for example - depending on the utility's policy) inverter will have to turn offline. Some say that then you can write to your utility to rework the local energy grid and/or lower secondary voltage on medium to low voltage transformer (I don't know the correct English term: transformer between 15kV and 400V levels).

    And about batteries - I had a link somewhere about batteries being sulfurized in sort time because of being constantly kept undercharged, but maybe technology have matured in the meantime (it was about lead acid batteries used in off-grid installations and from several years in the past)

    This link was probably something like this one:

    https://www.solarpaneltalk.com/forum/off-grid-solar/batteries-energy-storage/351396-are-you-killing-your-batteries-part-2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 2 years ago

    Interesting, I’d not given much thought to over-production.  In fact, in the UK, selling back to the grid is part of the “payback” plan, despite rates being very low.  You say storage solutions, presumably batteries in a domestic setting, may be short lived, how so?  Again, I had thought that a PV installation, with batteries would have been the best solution for the owner who then avoids more pull from the grid.  In more northern climes, such as the UK I would expect there to still be more take from. The grid as per your images of course.

    I would like to invest in PV and batteries as we have a large roof space.  My best calculations are a payback period of around 14 years given current high electricity prices.  My wife and I aren’t sure we would still be living here for that long as we could well downsize.  Perhaps we would be, who knows??  Also if, by some miracle, electricity prices come down, then the payback period extends.

    On a related note, she does want a chest freezer installing so maybe we could take advantage of your experiment to bring the payback down Grinning