• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog A DIY Vertical and Horizontal Farming Solution with IoT
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
  • Author Author: ipv1
  • Date Created: 12 Nov 2015 5:12 AM Date Created
  • Views 1573 views
  • Likes 5 likes
  • Comments 4 comments
  • ip_iot
  • vertical_farming
Related
Recommended

A DIY Vertical and Horizontal Farming Solution with IoT

ipv1
ipv1
12 Nov 2015

Hi guys,

Recently I got to design a project which was farming oriented. Due to lack of time for regular updates, I did not apply for the vertical farming challenge but I did get a lot of inspiration from the posts and have come up with a solution that works for my requirement. The details of the project are on the instructables website (and hackaday and hackster)and I am still filling in some blanks such as results and some LED lighting but here is a small demo video I have made. Take a look see and lemme know what you guys think. image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The core is the Intel Edison which has openhab running on it and does all the GUI stuff as well as the rules stuff. I wrote a service which allows to connect the Edison via MQTT and exposes the API to retrive data as well as control the lights and pumps etc. I could have done a rest API or a TCP connection but this seemed easier when working with proxies. The OpenHAB rules engine is responsible for controlling the pumps, manage the lights etc and connects to the internet to get weather forecasts to modify the irrigation cycles. It also manages alerts for failed lights etc but I forgot to include that in the demo video.

 

The system is at Mark 1 stage and with the LED roadtest plus, I am hoping to add some lighting to the mix as well as report back some indoor growing results. Again thanks for taking the time out to read and comment.

Sincerely,

IP

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Nice post. I liked the control features you highlighted and showed how they could be extended or modified as needed. Great job, DAB
  • m.ratcliffe
    m.ratcliffe over 10 years ago +1
    Great Project, Could you keep us updated on the long term results of weather forecast irrigation control. I have something similar in mind and it would be great to have your project as a base to start…
Parents
  • m.ratcliffe
    m.ratcliffe over 10 years ago

    Great Project, Could you keep us updated on the long term results of weather forecast irrigation control. I have something similar in mind and it would be great to have your project as a base to start from.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 10 years ago

    Great Project, Could you keep us updated on the long term results of weather forecast irrigation control. I have something similar in mind and it would be great to have your project as a base to start from.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ipv1
    ipv1 over 10 years ago in reply to m.ratcliffe

    Sure will. I am working to improve some other aspects and will be creating a dedicated page for the project. Will link it here once done. image