Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green  Blog:25 - Growing: Planting Seeds and Experimentation
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
  • Author Author: m.ratcliffe
  • Date Created: 20 Oct 2015 9:31 PM Date Created
  • Views 1225 views
  • Likes 1 like
  • Comments 2 comments
  • adapted_greenhouse
Related
Recommended

Automated Green  Blog:25 - Growing: Planting Seeds and Experimentation

m.ratcliffe
m.ratcliffe
20 Oct 2015

Well we all got the go ahead to plant off Dave. This is great news because here in England the temperature is dropping and the sunlight intensity is dropping with it.

 

Most of my systems are soi less, to keep things simple I use Rockwool starter cubes, to plant in rockwool we need to:

>Soak the cubes for half a hour in a solution of EC=1 PH=5.5 [Just what works for me]

>Place Seeds on Top of Cubed and press them in with a pen/prodder

>Place in a heated propagator [Too cold here for natural Germination]

>Water them daily with a weak nutrient solution [I have an automated system doing this that I might write up sometime]

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Experiment:

We are testing the germination success rate of cubes:

>Soaked in EC and PH adjusted fluid

>Soaked in just EC adjusted fluid

 

Glad this competition is rolling onto the growing stage,

Mike

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    Nice germination technique.

     

    It will be interesting to see how good your germination rate will be.

    Do you need to add more light due to the reduced sunlight or are you using cool weather plants that work with less sunlight?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    I usually get a high germination rate with the heated propagator [90%+], So I'm hoping for something similar this time around.

    It would be great to add more light, but not really an option for my at the moment. We will just have to see how it goes, mid November usually marks the end of my growing season without added heat at night.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    I usually get a high germination rate with the heated propagator [90%+], So I'm hoping for something similar this time around.

    It would be great to add more light, but not really an option for my at the moment. We will just have to see how it goes, mid November usually marks the end of my growing season without added heat at night.