Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:3 - Fish Feeding of the Future
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
  • Author Author: m.ratcliffe
  • Date Created: 13 Aug 2015 9:21 PM Date Created
  • Views 2844 views
  • Likes 3 likes
  • Comments 11 comments
  • adapted_greenhouse
  • raspberypi
  • arduino
Related
Recommended

Automated Green House Blog:3 - Fish Feeding of the Future

m.ratcliffe
m.ratcliffe
13 Aug 2015

With not having the Competition Kit arrive yet, this blog will be about some of the other projects I am working on relating to automation.

 

See the main Blog for updates:

 

Automated Green House Blog's Home Page

 

Some Basic Information:

 

>156 Billion KG of fish reared annual [thats more than beef!] [1]

>Optimum feeding regimes can increase productivity by 40%, food efficiency by 20% compared to conventional once per day feeding [2]

>There are many variables to consider when feeding fish [3]

 

Feeding Fish Is a very time consuming task, takes skilled operators to visit sites multiple times a day and is prone to human error. A computer could perform this task day in day out repeatable, efficiently and without human interaction, saving time food and increasing yields from a system drastically.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Note: On Video I say FeedForwards, I mean Open-Loop Control [It had been a Long day]

 

I have thought of two solutions to this problem, a open loop controller and a vision based feedback controller.

 

Open Loop:

[Wiring Diagrams and Code to Implement this on a arduino Unu will be included soon]


Human input to the controller

>Fish Breed

>Fish age

>Number of Fish

 

This Controller will then take measurements of the environmental variables [mainly temperature] and adjust:

>Feeding Spacing

>Feed type [what mechanical feeder to feed from]

 

 

Closed Loop

The benefit of implementing a controller this way is we no longer need to define the system in as much detail. it is fully aware of the eating habits of the fish.

[Implemented on RaspberyPI using opencv and usb webcam]

 

The Final unit will be able to:

>Estimate the size of the fish

>Feed the fish at the correct intervals and feed until the food demands of the fish decrease [it means their stomach is almost full]

>Feeding amount per serving

>Alert the farmer to any problems

     -Change in eating habbits

     -Bloated

     -disease

 

 

Work Done So far:

>Built temperature compensated open loop controller

>Built the basic vision part of the camera control [it can detect number of food pellets]

 

Here is a video of the camera gui and explication of how it works:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

 

Work To Do:

>Improve Blob Detection Techniques used

>See if we can get the camera to read the fish size when they come to feed + check for bloating /disease

>Code in the rate of food consumption [Blobs disappearing every seconds lets say]

>Put the control units in a better housing with a GUI

 

 

 

The Systems in the video prove the basic concept will work, they need a lot more work to get them to do the best job they can.

 

What I am Stuck on right now:

 

I have written another basic vision code that I want to implement onto a arduino based MCU. These units cannot do any heavy image processing [blob detection etc] the plan is to combine a camera with a arduino over serial, asses the incoming serial data on a pixel by pixel level. Something like this below:

 

[r=red competent of pixel, g=green component,b=blue component] where r,b,g will be at locations in the data packet I hope.

 

          If (r>2*g && r>2*b) {

               PixelCount = ++;

                                            };

 

What this does is assesses if a pixel is very red [the food pellets are red] and adds the total number of pixels in the picture up. Run the scrip at the beginning of the day to remove any red pixels from random red objects in the camera view that are not food. [lets call this count StaticSystemPixels].

 

        FoodPixels=(PixelCount-StaticSystmPixels)

 

And then add the correct amount of food to keep the FoodPixelCount at a predetermined  value, we can tell by the duty cycle of the mechanical feeder what the demand is and watch out for it decreasing as a sign that the fish have eaten the right amount of food.

 

I have written this sketch in Processing on a linux desktop and the theory works well, but I know nothing about the arduino and camera integration. I want to do this in real time without saving the image. So What I would like to do is asses the incoming serial data as it reaches the arduino

 

Is this possible? Am I right in thinking that the camera will transmit over serial whole pixel data sets , ie packet one contains information for pixel 1,2,3,4 or will it transmit in a way that each pixel will be spread across different packets? and can I do some quick assessment of this packet before the next one comes in?

 

Any help on this would be great!

 

 

 

I will be uploading the codes and tutorials about how to make everything to:

 

www.michaelratcliffe.com/projects    [Give me a few days to comment the codes and upload them]

 

I cant wait to get the competition kit,

Michael

 

References:

[1] FAO Fisheries and Aquaculture Department “THE STATE OF WORLD FISHERIES AND AQUACULTURE” 2012

[2]  Steven Craig “Understanding Fish Nutrition, Feeds, and Feeding”    2002

[3] S. J. Yeoh, F. S. Taip  “Development of Automatic Feeding Machine for Aquaculture Industry” 2010

  • Sign in to reply

Top Comments

  • m.ratcliffe
    m.ratcliffe over 11 years ago +1
    RWReynolds To reply to Rick [I didnt realise the video goes live before I publish the Blog] "Amazing Michael! This is a system you've used in production, correct? Did you build and write the software for…
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds +1
    It works ok, but like most things it takes a couple of revisions to perfect it. The Temperature controller is Arduino Uno based because it is easy for anyone to understand and I want to see this information…
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds +1
    Doc Brown as in back to the future, ive been called worse lol What is it that made the connection? Ray Mears is my usual nickname. I did a degree in mechanical engineering and then a research one in electronic…
Parents
  • RWReynolds
    RWReynolds over 11 years ago

    OK, just watched the second video. Verry impressive indeed. You've done a lot of really great work Michael.

     

    I've nicknamed you Doc Brown. lol...

     

    You are totally self-taught, correct? Me too. I've been playing with and working on electronics, computers and programming a little over 40 years. It is one of my hobbies and my sole, and soul, career. I got out of the hobby side for some years, life gets in the way, but have recently jumped back in. Mainly because I got a job in electronics R&D and embedded programming. After 30 years, I've come back home. image

     

    The work you've done is amazing. I really like the lab. Currently, I only have a small area to work in but I will remedy that soon.

     

    On your questions concerning USB camera to Arduino interface... It is USB so technically it is a serial interface. Check out the link below. It may make the work a little easier as there is a camera shield available.

    http://www.arducam.com/tutorial/

     

    I think you have most of this under control but if eve need any help with the work I am willing to do what I can. I fully intend to start exoerimenting with aquaponics once I'm on my feet again.

     

    Keep the videos and blogs coming. And I'm following the Hackaday site as well. Thinking about setting one up myself. image

     

    Cheers,

    Rick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds

    Doc Brown as in back to the future, ive been called worse lol What is it that made the connection?  Ray Mears is my usual nickname. I did a degree in mechanical engineering and then a research one in electronic engineering [mainly simulation of electrical motor drives] but most of the stuff I use day to day for these projects is self taught and based on gut feelings or simple post-it note type calculations.

     

    The "LAB" is a bed I made for the dog next to my desk, with her bedding removed. I'm hoping to set up a full lab in a shipping container on the yard in the near future, but I don't have a lot of equipment to work with electronics wise. I'm hopping element14Dave  considers my application for road testing a DMM and ads an oscilloscope to the road tests, then I will be set to do some more interesting stuff.

     

    As far as help I think I can do most of the stuff, I would appreciate you trying the build tutorials once they are up if you want to use something similar in your aquaponics and giving me feedback on what was easy to follow and what needs more explanation. I'm watching your blog on the rotating system, it looks interesting! Just a bit of advice, put the distribution pump on a relay so you can reduce the duty cycle at night or just turn it off to let the system get air if you ever need to, I cant see if you are relying on a flood and drain set-up of just water running down the system, but if it is a flood and drain it is easier to cut the water flow every so often than fine tune a mechanical siphon to stop siphoning.

     

    The Hackaday competition is great, build something cool and see what people think. I made it in the hope of getting some free parts to make more project happen, I doubt I will make it to winning the competition [Fish is a pretty boring subject for most] but you never know.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to m.ratcliffe

    Had not heard of Ray Mears, but that fits as well. lol...

     

    Ok, you do have some formal ed. Cool, you are certainly putting the "learning how to learn" aspect to great use.

     

    I will definitely be talking to you concerning the Aquaponics systems. Seems you have done a great deal of research and work in this area.

     

    I am going to start hitting the Raod Tests as well. I see some good stuff come across there. And I love the shipping container idea. I have designs on the same thing here. I have about 13 acres so plenty of room to install one. And I've seen some incredible dwellings created for shipping containers online. Seems it would be very easy t build a fine lab in one. I'm also a musician and one 40' container could easily support a nice electronics lab and a small studio I think.

     

    Yeah, I have plans to implement a control system for the nutrient solution. I will get it into the design document before long. I would like to implement some feedback as well, if nothing but pH and an automatic pH up and pH down mechanism. The cultivation side is not my strong point. So I'm not sure what other sensing would be relevant in the nutrient feedforward/feedback loop. It's a bit of a ebb and flow system but not really. The plan is to deliver nutrient solution to the top and let it gravity feed to the bottom, feeding each successive planter. There will be a flow detector in the drain back to the reservoir. If I leave the pump on for some bit of time after the drainage starts that should effectively flood all plants. Then cut it off and wait for the next feeding cycle. I've seen it done successfully online and I wanted to try it. Seems well suited for the vertical and small footprint aspects of the challenge.

     

    I'm going to take a deeper look at the hackaday site. And I'm sure there are other engineering and hacking competitions going on all the time. This may become a thing for me. It's quite fun. And making new contacts with folks who have similar interests is always a good thing. Makes the ideas flow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds

    I was never that good in uni tbh, I spent most of my time making other things than working for the tests. I was thinking of a 20' container for the electronics lab, but a 40' would make an epic room for a bit of everything. I's an american acre the same as a British, if so that is a decent size for playing around on.

     

    I always find I need to PH down and never up in aquaponics so you could cut your number of pumps in half if you have the same situation, I'm working on a PPM meter now using an american plug as the sensor [they are cheap, corrosion resistance and always the same spec] If it works i'll upload it to the Blog. What other projects are you working on?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds

    I was never that good in uni tbh, I spent most of my time making other things than working for the tests. I was thinking of a 20' container for the electronics lab, but a 40' would make an epic room for a bit of everything. I's an american acre the same as a British, if so that is a decent size for playing around on.

     

    I always find I need to PH down and never up in aquaponics so you could cut your number of pumps in half if you have the same situation, I'm working on a PPM meter now using an american plug as the sensor [they are cheap, corrosion resistance and always the same spec] If it works i'll upload it to the Blog. What other projects are you working on?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • RWReynolds
    RWReynolds over 11 years ago in reply to m.ratcliffe

    You need one of these.

    http://gizmodo.com/the-laser-guided-robo-milker-is-the-future-of-dairy-1183979314

     

    Best I can tell is that a US and UK acre are the same.

     

    We have well water and it tends to be very acidic. So I will implement only the pH up system and save some effort and money. I'll have to do some testing and research.

     

    Let me know in the TDS sensor. I've been looking at some and the price range is pretty wide. Would be good to know if some of the less expensive models work well enough.

     

    Right now the challenge is my only project. That and recovering from the ankle surgery. I also do this at work and have several interesting projects there. Mostly utilizing the Raspberry Pi. But they are all under NDA agreements and I can't really talk about them. I do have one coming up that should be very cool. Working with cryogenic storage systems. I'm looking forward to that. On a personal level, I've just really gotten back into it all so I have lots of stuff in my head and not much in the works. And before the surgery I couldn't get around very well and the pain just kind of saps your motivation. It's amazing how much we take for granted the simple act of walking. This challenge has been very motivating.  I can see doing a lot once I can get back on my feet. First things would be some automation around here to help with our horses and chickens and such. And more work on the hydroponics/aquaponics stuff.