Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:3 - Fish Feeding of the Future
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
  • Author Author: m.ratcliffe
  • Date Created: 13 Aug 2015 9:21 PM Date Created
  • Views 2843 views
  • Likes 3 likes
  • Comments 11 comments
  • adapted_greenhouse
  • raspberypi
  • arduino
Related
Recommended

Automated Green House Blog:3 - Fish Feeding of the Future

m.ratcliffe
m.ratcliffe
13 Aug 2015

With not having the Competition Kit arrive yet, this blog will be about some of the other projects I am working on relating to automation.

 

See the main Blog for updates:

 

Automated Green House Blog's Home Page

 

Some Basic Information:

 

>156 Billion KG of fish reared annual [thats more than beef!] [1]

>Optimum feeding regimes can increase productivity by 40%, food efficiency by 20% compared to conventional once per day feeding [2]

>There are many variables to consider when feeding fish [3]

 

Feeding Fish Is a very time consuming task, takes skilled operators to visit sites multiple times a day and is prone to human error. A computer could perform this task day in day out repeatable, efficiently and without human interaction, saving time food and increasing yields from a system drastically.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Note: On Video I say FeedForwards, I mean Open-Loop Control [It had been a Long day]

 

I have thought of two solutions to this problem, a open loop controller and a vision based feedback controller.

 

Open Loop:

[Wiring Diagrams and Code to Implement this on a arduino Unu will be included soon]


Human input to the controller

>Fish Breed

>Fish age

>Number of Fish

 

This Controller will then take measurements of the environmental variables [mainly temperature] and adjust:

>Feeding Spacing

>Feed type [what mechanical feeder to feed from]

 

 

Closed Loop

The benefit of implementing a controller this way is we no longer need to define the system in as much detail. it is fully aware of the eating habits of the fish.

[Implemented on RaspberyPI using opencv and usb webcam]

 

The Final unit will be able to:

>Estimate the size of the fish

>Feed the fish at the correct intervals and feed until the food demands of the fish decrease [it means their stomach is almost full]

>Feeding amount per serving

>Alert the farmer to any problems

     -Change in eating habbits

     -Bloated

     -disease

 

 

Work Done So far:

>Built temperature compensated open loop controller

>Built the basic vision part of the camera control [it can detect number of food pellets]

 

Here is a video of the camera gui and explication of how it works:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

 

Work To Do:

>Improve Blob Detection Techniques used

>See if we can get the camera to read the fish size when they come to feed + check for bloating /disease

>Code in the rate of food consumption [Blobs disappearing every seconds lets say]

>Put the control units in a better housing with a GUI

 

 

 

The Systems in the video prove the basic concept will work, they need a lot more work to get them to do the best job they can.

 

What I am Stuck on right now:

 

I have written another basic vision code that I want to implement onto a arduino based MCU. These units cannot do any heavy image processing [blob detection etc] the plan is to combine a camera with a arduino over serial, asses the incoming serial data on a pixel by pixel level. Something like this below:

 

[r=red competent of pixel, g=green component,b=blue component] where r,b,g will be at locations in the data packet I hope.

 

          If (r>2*g && r>2*b) {

               PixelCount = ++;

                                            };

 

What this does is assesses if a pixel is very red [the food pellets are red] and adds the total number of pixels in the picture up. Run the scrip at the beginning of the day to remove any red pixels from random red objects in the camera view that are not food. [lets call this count StaticSystemPixels].

 

        FoodPixels=(PixelCount-StaticSystmPixels)

 

And then add the correct amount of food to keep the FoodPixelCount at a predetermined  value, we can tell by the duty cycle of the mechanical feeder what the demand is and watch out for it decreasing as a sign that the fish have eaten the right amount of food.

 

I have written this sketch in Processing on a linux desktop and the theory works well, but I know nothing about the arduino and camera integration. I want to do this in real time without saving the image. So What I would like to do is asses the incoming serial data as it reaches the arduino

 

Is this possible? Am I right in thinking that the camera will transmit over serial whole pixel data sets , ie packet one contains information for pixel 1,2,3,4 or will it transmit in a way that each pixel will be spread across different packets? and can I do some quick assessment of this packet before the next one comes in?

 

Any help on this would be great!

 

 

 

I will be uploading the codes and tutorials about how to make everything to:

 

www.michaelratcliffe.com/projects    [Give me a few days to comment the codes and upload them]

 

I cant wait to get the competition kit,

Michael

 

References:

[1] FAO Fisheries and Aquaculture Department “THE STATE OF WORLD FISHERIES AND AQUACULTURE” 2012

[2]  Steven Craig “Understanding Fish Nutrition, Feeds, and Feeding”    2002

[3] S. J. Yeoh, F. S. Taip  “Development of Automatic Feeding Machine for Aquaculture Industry” 2010

  • Sign in to reply

Top Comments

  • m.ratcliffe
    m.ratcliffe over 11 years ago +1
    RWReynolds To reply to Rick [I didnt realise the video goes live before I publish the Blog] "Amazing Michael! This is a system you've used in production, correct? Did you build and write the software for…
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds +1
    It works ok, but like most things it takes a couple of revisions to perfect it. The Temperature controller is Arduino Uno based because it is easy for anyone to understand and I want to see this information…
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds +1
    Doc Brown as in back to the future, ive been called worse lol What is it that made the connection? Ray Mears is my usual nickname. I did a degree in mechanical engineering and then a research one in electronic…
Parents
  • DAB
    DAB over 11 years ago

    It has long been a tradition to use farm ponds to raise fish and to harvest fertilizer and fish as part of the overall farm production.

     

    It looks like you have done a great job of automating some of the process.  Now all you need to do is assess the scale you need to support your crop growing efforts.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to DAB

    Thanks for the feedback Dab, i'm hoping to automate the entire farming process eventually [well the cattle rotation, aquaponics production and irrigation of pastures] so that one man can farm 14 acres in a few hours on a weekly visit. I'm running a simulation to optimise this and work out some basic ratios [pasture to aquaponics etc] but the outlay to test the idea is very expensive here in the UK, land is a crazy price.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to DAB

    Thanks for the feedback Dab, i'm hoping to automate the entire farming process eventually [well the cattle rotation, aquaponics production and irrigation of pastures] so that one man can farm 14 acres in a few hours on a weekly visit. I'm running a simulation to optimise this and work out some basic ratios [pasture to aquaponics etc] but the outlay to test the idea is very expensive here in the UK, land is a crazy price.