Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:6 -  Raspbery Pi and OpenCv the Easy Way
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
  • Author Author: m.ratcliffe
  • Date Created: 20 Aug 2015 12:12 PM Date Created
  • Views 865 views
  • Likes 2 likes
  • Comments 0 comments
  • adapted_greenhouse
  • opencv
  • raspberry-pi
Related
Recommended

Automated Green House Blog:6 -  Raspbery Pi and OpenCv the Easy Way

m.ratcliffe
m.ratcliffe
20 Aug 2015

It it crazy Just How much miss information there is about opencv and the Raspberry pi, many tutorials will guide you thru a installation process that takes 12 hours+ and has library's linked complexly.

 

Opencv 2.4.1 [CV2] is available in the default Rasbian Reposttory.

To Install on Rasbian, type the following into the command terminal:

 

Type Into Terminal

Sudo apt-get update

sudo apt-get upgrade

 

 

sudo apt-get install libcv-dev

sudo apt-get install python-opencv

sudo apt-get install libopencv-dev

sudo apt-get install libcv2.3

sudo apt-get install opencv-doc

 

How To use:

>Open the File manager and go to your documents

>Right click>CreatNew>Empty File

>Add the line [#!/usr/bin/python] To the top of the file

>Save it as <FileName>.py

>Right Click on the File >Properties>Permissions and select everyone> OK

>Double click on the file and execute in terminal

 

Hints:

>Remember it is a python based install of openCV 2

>Execute the python script as root if you want access to the GPIO pins

>If the script doesnt work, Cd / into the directory and run python <Filename.py>

 

Useful Links:

 

Adaptive Threshold:  http://opencv-python-tutroals.readthedocs.org/en/latest/py_tutorials/py_imgproc/py_thresholding/py_thresholding.html

Other Threshold