Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:9.3 - Tip for trimming arduino If statement times
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: m.ratcliffe
  • Date Created: 12 Feb 2016 5:59 PM Date Created
  • Views 823 views
  • Likes 3 likes
  • Comments 1 comment
  • arduino:
  • adapted_greenhouse
Related
Recommended

Automated Green House Blog:9.3 - Tip for trimming arduino If statement times

m.ratcliffe
m.ratcliffe
12 Feb 2016

This will not be a very useful tip for 99% of your arduino projects, but if you are wanting to keep your code running as quick as possible without reverting to C its a handy tip to have.

 

Ive got a few arduino projects going now where I need to keep my main loops running fast, This is a test to verify that a multiple IF statement finished if the primary statement is false.

 

In example...  if(A= =false && B== true)  the arduino will move onto the next line of code if stament A is not true. Restructuring your code a little to make sure you ask a boolean statement first can give you a little quicker loop times.

 

The results from the below test code:

Structure 1 :

24 (ms)

Structure 2 :

16 (ms)

 

Not a massive increase but something to keep in mind if you have resource expensive stamen conditions.

 

 

The Test Code:

 

The Code

/*

Script to verify how the arduino habldes if routines with multiple statments. ABA test

 

 

   28/8/2015  Michael Ratcliffe  Mike@MichaelRatcliffe.com

  

  

          This program is free software: you can redistribute it and/or modify

    it under the terms of the GNU General Public License as published by

    the Free Software Foundation, either version 3 of the License, or

    (at your option) any later version.

 

 

    This program is distributed in the hope that it will be useful,

    but WITHOUT ANY WARRANTY; without even the implied warranty of

    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

    GNU General Public License for more details.

 

 

    You should have received a copy of the GNU General Public License

    along with this program.  If not, see <http://www.gnu.org/licenses/>.

*/

 

 

 

 

 

 

 

 

//Just some variables for the test

 

 

long start=0;

int i=0;

int flag=1;

 

 

void setup() {

  // put your setup code here, to run once:

Serial.begin(9600);

 

 

 

 

//Test A, a boolean comparison fisrt

//runs loop 10,000 times and makes a log of time to compute if statment, shoot results out to terminal

i=0;

start=millis();

while (i<10000) {

if(millis()%(6000)>10000000 && flag==0);

i++;

}

Serial.println("Structure 1 : ");

Serial.println(millis()-start);

 

 

//Test B, a heavier math based statment first

i=0;

start=millis();

while (i<10000) {

if( flag==0 && millis()%(6000)>10000000 );

i++;

}

Serial.println("Structure 2 : ");

Serial.println(millis()-start);

 

 

//Test A, a boolean comparison fisrt

i=0;

start=millis();

while (i<10000) {

if(millis()%(6000)>10000000 && flag==0);

i++;

}

Serial.println("Structure 1 : ");

Serial.println(millis()-start);

 

 

 

}

 

 

void loop() {

//We only need to run the test once

};

  • Sign in to reply

Top Comments

  • mhmayyan
    mhmayyan over 9 years ago +1
    Really nice test. It is new for me. This timing issue would be clear if I programmed in assembly but I have never thought in this way with programming in C/C++. Thanks,
Parents
  • mhmayyan
    mhmayyan over 9 years ago

    Really nice test. It is new for me.

     

    This timing issue would be clear if I programmed in assembly but I have never thought in this way with programming in C/C++.

     

    Thanks,

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mhmayyan
    mhmayyan over 9 years ago

    Really nice test. It is new for me.

     

    This timing issue would be clear if I programmed in assembly but I have never thought in this way with programming in C/C++.

     

    Thanks,