• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Found schematic for PH meter, initial design thoughts
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
  • Author Author: sftwrngnr
  • Date Created: 29 Jul 2015 5:30 AM Date Created
  • Views 813 views
  • Likes 5 likes
  • Comments 5 comments
  • vertical
  • ambient_growth
  • farming
Related
Recommended

Found schematic for PH meter, initial design thoughts

sftwrngnr
sftwrngnr
29 Jul 2015

I found a schematic for a Ph meter that I'm likely going to use with this project.  I'll be ordering the necessary parts for that on Friday, along with a few peristaltic pumps for dispensing nutrients.  My plan is to start sketching up the initial prototype with FreeCad (a 3D parametric CAD program).  I remember some work that was done by NASA with regard to utilizing high voltage as a means to enhance plant growth, so for at least one of the growing tracts, I plan on having an adjustable high voltage mesh that sits directly above the plants.  The high voltage will be generated by a simple cascade/ladder circuit using diodes and capacitors (ideally from the build kit).  I have a small keypad that I can utilize for direct user input into the system, but my current plan is to utilize one of the boards from the kit as the means to run the backend API.  I'll get my domain name registered and basic hosting set up later this week, along with the initial version of the database schema.

 

My current design will be predicated on purchasing low cost, readily available parts from the local hardware store (Home Depot/Lowes).  To my knowledge, we haven't been given the specifics on what types of plants we are growing.  To that end, I'll be designing a heat exchanger system that utilizes a Peltier device to put the nutrient bath at a constant temperature that is ideal for the plant root system.  A larger "mini-hvac" system will need to be developed as well to keep the grow chamber at optimal temperature and humidity as well.

 

In order to minimize the system's water utilization footprint, I will be developing a small solar still that will accept as input the expended nutrient bath, and will have as output, distilled water that can subsequently be used by the system.  I'm planning on having the grow chamber be covered with reflective mylar film so that  plants absorb as much ambient sunlight and room light as possible, while also capturing water that is transpired from the plants as they grow. 

 

I'm looking into a couple of different options for misting systems so that the humidity can be controlled appropriately, and the plant leaves can be misted if desired.  All facets of the operations of this system will be controlled by the microcontroller, and data will be logged to the website in real-time.

  • Sign in to reply

Top Comments

  • sftwrngnr
    sftwrngnr over 11 years ago in reply to jw0752 +1
    Basically my thoughts for recapturing the distilled water was to reuse it for the nutrient water. What I'm trying to build is a system that is efficient in its electrical and water usage footprint. The…
Parents
  • mrinalk
    mrinalk over 7 years ago

    Can u please provide  me the schematic. i am also pursuing a project on ph meter. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sftwrngnr
    sftwrngnr over 7 years ago in reply to mrinalk

    I apologize for not getting back to you sooner. Let me see if I can dig up the schematic if you're still interested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sftwrngnr
    sftwrngnr over 7 years ago in reply to mrinalk

    I apologize for not getting back to you sooner. Let me see if I can dig up the schematic if you're still interested.