• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Found schematic for PH meter, initial design thoughts
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
  • Author Author: sftwrngnr
  • Date Created: 29 Jul 2015 5:30 AM Date Created
  • Views 814 views
  • Likes 5 likes
  • Comments 5 comments
  • vertical
  • ambient_growth
  • farming
Related
Recommended

Found schematic for PH meter, initial design thoughts

sftwrngnr
sftwrngnr
29 Jul 2015

I found a schematic for a Ph meter that I'm likely going to use with this project.  I'll be ordering the necessary parts for that on Friday, along with a few peristaltic pumps for dispensing nutrients.  My plan is to start sketching up the initial prototype with FreeCad (a 3D parametric CAD program).  I remember some work that was done by NASA with regard to utilizing high voltage as a means to enhance plant growth, so for at least one of the growing tracts, I plan on having an adjustable high voltage mesh that sits directly above the plants.  The high voltage will be generated by a simple cascade/ladder circuit using diodes and capacitors (ideally from the build kit).  I have a small keypad that I can utilize for direct user input into the system, but my current plan is to utilize one of the boards from the kit as the means to run the backend API.  I'll get my domain name registered and basic hosting set up later this week, along with the initial version of the database schema.

 

My current design will be predicated on purchasing low cost, readily available parts from the local hardware store (Home Depot/Lowes).  To my knowledge, we haven't been given the specifics on what types of plants we are growing.  To that end, I'll be designing a heat exchanger system that utilizes a Peltier device to put the nutrient bath at a constant temperature that is ideal for the plant root system.  A larger "mini-hvac" system will need to be developed as well to keep the grow chamber at optimal temperature and humidity as well.

 

In order to minimize the system's water utilization footprint, I will be developing a small solar still that will accept as input the expended nutrient bath, and will have as output, distilled water that can subsequently be used by the system.  I'm planning on having the grow chamber be covered with reflective mylar film so that  plants absorb as much ambient sunlight and room light as possible, while also capturing water that is transpired from the plants as they grow. 

 

I'm looking into a couple of different options for misting systems so that the humidity can be controlled appropriately, and the plant leaves can be misted if desired.  All facets of the operations of this system will be controlled by the microcontroller, and data will be logged to the website in real-time.

  • Sign in to reply

Top Comments

  • sftwrngnr
    sftwrngnr over 11 years ago in reply to jw0752 +1
    Basically my thoughts for recapturing the distilled water was to reuse it for the nutrient water. What I'm trying to build is a system that is efficient in its electrical and water usage footprint. The…
Parents
  • jw0752
    jw0752 over 11 years ago

    This sounds like a good plan. I am interested if you see any measurable difference in the plants in the high electric field. What voltage level will you be exploring? Also, can you elaborate a bit on the purpose for the still and the use for distilled water in the vertical farm?

    Thanks John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sftwrngnr
    sftwrngnr over 11 years ago in reply to jw0752

    Basically my thoughts for recapturing the distilled water was to reuse it for the nutrient water.  What I'm trying to build is a system that is efficient in its electrical and water usage footprint.  The nutrients need to be replenished/refreshed weekly, so I was thinking that I could consider developing a simple solar still so that the water could be purified and recaptured and reused by the system.  Clearly the used nutrients/salts would need to be cleaned out periodically, but a solar still would recapture the water. Hey... if I'm gonna build a prototype on my own time, I may as well over-engineer the thing and throw in as much geek-gadgetry as possible image.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to sftwrngnr

    Ok, Now I'm with the program. The nutrient levels must be rebalanced before the water can be used again. Over-engineer away, it will be cool to see the results.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 11 years ago in reply to sftwrngnr

    Ok, Now I'm with the program. The nutrient levels must be rebalanced before the water can be used again. Over-engineer away, it will be cool to see the results.

    John