Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Help needed with EZR32WG and EFM32
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
  • Author Author: ochikov
  • Date Created: 9 Sep 2015 2:28 PM Date Created
  • Views 966 views
  • Likes 3 likes
  • Comments 11 comments
Related
Recommended

Help needed with EZR32WG and EFM32

ochikov
ochikov
9 Sep 2015

Hello,

 

From about 3-4 days I have try to exlpore the kits. All I've done is this:

 

1. I managed to play example of Simplicity Studio tx-rx with EZR32WG 868 MHz kit with two nodes.

2. I managed to run Simplicity Studio energy monitoring with kit EZR32WG MHz kit

3. I managed to download the Android app and connect it with sensor-puck.

 

I managed to watch all about in youtube Silicon Lab's channel about our kit.

I'm not very good at C programming. I have experience only with web (PHP,MySQL).

Can somebody give me basic guideline how to deal with these kits and also how to connect sensors and etc. I will be very thankful. Also if somebody have additional documentation I will be very happy to share with me.

 

Thanks.

  • Sign in to reply

Top Comments

  • shanesissons
    shanesissons over 10 years ago +2
    I'm having the same issue I'm going to comment so I get email updates
  • e14 Contributor
    e14 Contributor over 10 years ago +2
    Hi All, I created a getting started guide in the vertical farming content to help you get off the ground (pun intended) and developing with EFM32, EZR32, and Simplicity Studio. Getting Started
  • ochikov
    ochikov over 10 years ago in reply to RWReynolds +1
    Hello Rick, Yes I have it. I only managed to run Demos on EZR32WG. I don't know where to start from. I don't have experience with C language. When I open software demos, I understand some of the written…
  • ochikov
    ochikov over 10 years ago in reply to michaelwylie

    I already made all demos and examples and still can't start develop anything image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago

    Usually firmware examples come with development kits to demonstrate their capability. These are loaded through simplicity studio. When you open Simpliciy studio look on the left. It should auto detect any kit attached. Then click software examples and you should be able to select from a few example projects for the kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 10 years ago in reply to ochikov

    Not sure how much help I can be on the radio code as I have not yet received the EZR32WG starter kit.

     

    How to attach the sensors depends on what type sensors you have. Some might be digital and use GPIO pins and some analog and use ADC pins. I am using one of the analog comparator pins on the EFM32ZG kit to read and control a timer/relay device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ochikov
    ochikov over 10 years ago in reply to RWReynolds

    Hello Rick,

    Yes I have it. I only managed to run Demos on EZR32WG. I don't know where to start from. I don't have experience with C language. When I open software demos, I understand some of the written lines, but is complicated at all. How can I attach sensors to EZR32WG. My idea is to use one part of the kit as Master (to collect data from sensors and the send it) and 2nd part as Slave (to recieve data through 868 Mhz interface) and then to export it through Ethernet interface to a web server.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 10 years ago

    Ognyan, you have the EZR32WG kit in hand now as well?

     

    Again, if I can help with getting you started on your software let me know. I'll do what I can.

     

    Cheers,

    Rick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>