Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Modular Farm Blog: Post 1 - Project Overview
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
  • Author Author: jmbranco76
  • Date Created: 5 Aug 2015 12:05 AM Date Created
  • Views 1178 views
  • Likes 5 likes
  • Comments 8 comments
  • modular_farm
  • net_zero_energy_farming
  • growsharp
Related
Recommended

Modular Farm Blog: Post 1 - Project Overview

jmbranco76
jmbranco76
5 Aug 2015

Hello vertical farmers!

 

This is our first post, so we would like to thank element14 and sponsors for starting this great challenge to inspire new ways of doing agriculture.

 

I heard somewhere that plants swim faster in water than fish! Faster than on land! And I assure you, much cleaner! So our goal is to develop a simple modular automated system to support indoor plant growing of fruits and vegetables based on hydroponics.

 

What we will need? Control the relevant variables of healthy growth in hydroponics (temperature, humidity, pH, light, nutrients, etc.). We will add to this a monitoring system based on a webcam, a web application for supervision and LED lighting to guarantee full time production. Concerning sustainability, we will implement a renewable energy system.

 

From this basic idea, the following scheme born on a piece of paper. It summarizes the components of the system.

 

image

 

The key features of the proposed system are:

  • Modular (horizontal and vertically)
  • Self-sufficient in terms of energy (“net-zero”)
  • All year production supported on artificial LED lighting
  • Renewable power sources
  • Highly efficient
  • Hydroponic
  • Automated
  • Artificial intelligence
  • Vision system for monitoring
  • True IoT solution
  • Low power consumption

 

Due to the time frame limitation, some components of the proposed system were identified as secondary in the scope of this challenge and will be implemented only after successful implementation of the remaining system. Those items are respectively the aerogenerator and the solar tracking implementation.

 

We designed the system as shown in the following photo. Ok, it's not a photo yet but we hope it will be soon ;-)

 

image

 

On the next post we'll guide you through our hydroponic system design and implementation.

 

Follow us on this journey to find new ways to feed the world and feel free to comment or ask any question.

 

See you in the next post :-)

  • Sign in to reply

Top Comments

  • jmbranco76
    jmbranco76 over 11 years ago in reply to m.ratcliffe +1
    Hi Michael, Thanks. The first image was generated by an online tool that you can fnd at www.coggle.it. Cheers, José
  • jmbranco76
    jmbranco76 over 11 years ago in reply to shanesissons +1
    Hi Shane, it will be a self contained unit outside with a footprint of 5x3m. The structure will be built on wood and the solar panel will be mounted on the roof. We´ll start with one solar panel of 250W…
Parents
  • shanesissons
    shanesissons over 11 years ago

    Great idea you say about using renewable energy is this going to be a self contained unit like a shipping container for example that will be outside or will it be a modular system inside a building?

     

    Shane

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jmbranco76
    jmbranco76 over 11 years ago in reply to shanesissons

    Hi Shane,

     

    it will be a self contained unit outside with a footprint of 5x3m. The structure will be built on wood and the solar panel will be mounted on the roof. We´ll start with one solar panel of 250W and a battery to be self sufficient energetically. The whole system will run on DC.

     

    Cheers,

    José

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jmbranco76
    jmbranco76 over 11 years ago in reply to shanesissons

    Hi Shane,

     

    it will be a self contained unit outside with a footprint of 5x3m. The structure will be built on wood and the solar panel will be mounted on the roof. We´ll start with one solar panel of 250W and a battery to be self sufficient energetically. The whole system will run on DC.

     

    Cheers,

    José

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shanesissons
    shanesissons over 11 years ago in reply to jmbranco76

    I though this might be the case and that is a great idea

     

    Shane